Arduino Forum Components needed for a barebones Arduino
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
  • State Not Answered
  • Replies 9 replies
  • Subscribers 405 subscribers
  • Views 638 views
  • Users 0 members are here
  • atmega328
  • microcontroller
  • arduino
Related

Components needed for a barebones Arduino

Former Member
Former Member over 10 years ago

Is there anything other than the crystal and the microcontroller that is necessary for this? I want to get as little as possible, as this is going somewhere and staying there, and doesn't need any shields or accessories. And also, if I wanted to program it just once, is there a way to ghetto-rig it up to a serial port with jumper wires? Thank You!

  • Sign in to reply
  • Cancel

Top Replies

  • 4ringfan
    4ringfan over 10 years ago in reply to Former Member +4
    Maybe I'm not following this. I'm not sure I understand the need to re-invent the wheel. If you are doing this as a DIY to prove to yourself that you can make a controller from ground up complete with…
  • mcb1
    mcb1 over 10 years ago +1
    Paul has given you some good advise .. and some searching on google will also find plenty ... http://cdn.shopify.com/s/files/1/0038/9582/files/RBBB_Instructions_06.pdf?1260749296 You don't need the resonator…
  • Problemchild
    Problemchild over 10 years ago in reply to mcb1 +1
    Other than the 8MHZ default clock. I believe they don't recommend the internal RC clock for serial due to instability...some even complain about the resonators...not that I've had a problem with those…
Parents
  • mcb1
    0 mcb1 over 10 years ago

    Paul has given you some good advise .. and some searching on google will also find plenty ...

    http://cdn.shopify.com/s/files/1/0038/9582/files/RBBB_Instructions_06.pdf?1260749296

     

    You don't need the resonator or the xtal BUT it will run at 8MHz and all the timing and libraries may change.

     

    You will need to laod the bootloader into the chip (search for loading the bootloader or buy a pre loaded chip)

    You don't need the serial after you load your program, so just unplug the USB to Serial device from pins D0, D1.

     

    Mark

    gadget.iom

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 10 years ago in reply to mcb1

    Other than the 8MHZ default clock. I believe they don't recommend the internal RC clock for serial due to instability...some even complain about the resonators...not that I've had a problem with those!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Problemchild

    Alright.  As soon as I get all the components I will build one and let you guys know.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 4ringfan
    0 4ringfan over 10 years ago in reply to Former Member

    Maybe I'm not following this.  I'm not sure I understand the need to re-invent the wheel.  If you are doing this as a DIY to prove to yourself that you can make a controller from ground up complete with a boot load, I would totally understand that, but if you are doing this just to save money, I doubt that you will.  You can probably score an aftermarket Arduino nano (for example) for less than $4-5 with free S&H.  Are you honestly going to be able to source the parts, pay for postage, construct it, and make your Arduino controller for much less than that?  I just find it hard to believe.

     

    If you don't want someone messing with the thing after the fact, desolder the USB port, or even cut that end of the PCB off.  Then your project is a set it and forget it.  I dunno, that is just my two cents.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 4ringfan
    0 4ringfan over 10 years ago in reply to Former Member

    Maybe I'm not following this.  I'm not sure I understand the need to re-invent the wheel.  If you are doing this as a DIY to prove to yourself that you can make a controller from ground up complete with a boot load, I would totally understand that, but if you are doing this just to save money, I doubt that you will.  You can probably score an aftermarket Arduino nano (for example) for less than $4-5 with free S&H.  Are you honestly going to be able to source the parts, pay for postage, construct it, and make your Arduino controller for much less than that?  I just find it hard to believe.

     

    If you don't want someone messing with the thing after the fact, desolder the USB port, or even cut that end of the PCB off.  Then your project is a set it and forget it.  I dunno, that is just my two cents.

    image

    • Cancel
    • Vote Up +4 Vote Down