Arduino Forum how to attach crystal?
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
  • State Not Answered
  • Replies 19 replies
  • Subscribers 406 subscribers
  • Views 1601 views
  • Users 0 members are here
  • crystal
  • oscillators
  • avr
  • atmega328p
Related

how to attach crystal?

rishi2628
rishi2628 over 10 years ago

i am making a custom board using atmega328p. i am programming the chip using a arduino uno board which works fine but when i attach the microcontroller to the development board, the delay function doesn't seem to work. I think there is a problem with the oscillator. I have simply connected a crystal at xtal pins. Is this the correct way??

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago +4
    Something like this... Google "arduino bare bones"
  • mcb1
    mcb1 over 10 years ago in reply to clem57 +3
    clem57 I see to recall we had a very similar discussion not that long ago. ... The Bare Bones project tend to use a resonator, although they talk about a xtal and neglect to say you need the capcitors…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to clem57 +3
    I tend to prefer a real xtal and a couple of caps, this gives a much more precise loop time. Either will work without issue and the cost is still measured in Pennies or Cents If your making thousands then…
Parents
  • rishi2628
    0 rishi2628 over 10 years ago

    suppose i want to select the internal oscillator of the microcontroller...............how will i do it on the arduino ide??..............what setting do i have to change.........or what is the code to select the internal oscillator?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to rishi2628

    rishi2628

         A good source of changing Arduino is through fuses. But if done incorrectly, can brick the microchip. http://forum.arduino.cc/index.php?topic=269448.0

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago in reply to rishi2628

    rishi2628

         A good source of changing Arduino is through fuses. But if done incorrectly, can brick the microchip. http://forum.arduino.cc/index.php?topic=269448.0

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to clem57

    I tend to prefer a real xtal and a couple of caps, this gives a much more precise loop time.

     

    Either will work without issue and the cost is still measured in Pennies or Cents

     

    If your making thousands then sure it makes a difference, but if your just building a few or need the precision then I would go for the Xtal and caps

     

    I also think you can get to 20Mhz only with a Xtal but I could be wrong there

     

    Regards

     

    Peter

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Robert Peter Oakes

    I have to agree with Peter. If you want to control external devices the timing can and will make a difference.

    Clem

    • Cancel
    • Vote Up +2 Vote Down