Arduino Forum Ann:$25 PCB to help novices/protect Arduino. Schools. Parents?
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
  • State Suggested Answer
  • Replies 20 replies
  • Answers 1 answer
  • Subscribers 392 subscribers
  • Views 910 views
  • Users 0 members are here
  • education
  • arduino
  • novice
Related

Ann:$25 PCB to help novices/protect Arduino. Schools. Parents?

Former Member
Former Member over 10 years ago

I hope it is okay that I marked this as a question? It IS an announcement... but also a question in that feedback on the item described is my main reason for posting! If experts find problems if they are kind enough to review the page offered below,their thoughts will be very welcome.

 

This is NOT "crowd sourced" vaporware! The boards exist. They work. But I am inviting Mr Murphy to the party, AND involving kids... I am not so egotistical to believe that there is nothing that could be improved. Before I put a lot more time into this, I want to be sure there are no fundamental flaws at the heart of the work to date!

 

I now have six copies of a PCB which, along with it's components, cost about $25 each.

 

NoviceGuard, as I call it, is an attempt to make an Arduino Pro Mini "novice friendly", and also novice SAFE... i.e., the user can't damage the Arduino, if just one basic rule is kept.

 

I hope it will make the Arduino something that can be used in schools with children as young as 10.

 

I have a general page about it, but also a page for teachers/ parents, and one written to tell "experts" what I've tried to do. I hope experts will look at their page, and write to me if they can see things that I've overlooked... is there a way to damage the board that I've overlooked?

 

Experts' page: Call for review: for experts, a plea for input: NoviceGuard (PCB261) ModGeeInt.htm

 

Parents', teachers' page: Introduction for teachers, parents: NoviceGuard (PCB261) ModTeaInt.htm

 

(There are links to the general page from both.)

 

I am looking for suitable people to LOAN a prototype to, for comment. Details in both pages.

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • Capper
    Capper over 10 years ago +2
    Here are my thoughts.... A PCB is not suitable for a 10 year old kid. They will only work with something in a big plastic box with large knobs and switches. loose parts like jumpers and LEDs will get immediately…
  • gadget.iom
    gadget.iom over 10 years ago +1
    I'm not sure I fully understand the concept. The approach sounds much like the ruggeduino: Rugged Circuits They mention 10 ways to destroy an arduino and then discuss preventive measures: https://andrew…
  • Former Member
    Former Member over 10 years ago in reply to gadget.iom +1
    Thank you! And yes, there is a clash of names. I can only protest that I was using "Rugguino" quite innocently for a time (started years ago) before becoming aware of Ruggeduino. (I have a note on my Rugguino…
Parents
  • Capper
    0 Capper over 10 years ago

    Here are my thoughts....

    A PCB is not suitable for a 10 year old kid. They will only work with something in a big plastic box with large knobs and switches.  loose parts like jumpers and LEDs will get immediately lost or swallowed by a younger sibling or pet.

    Why make a board for a micro or mini to make it bigger than an Uno? Just use an Uno.

    I think my son enjoyed burning up all my LEDs putting them on a 9V battery when he was about 10.

    10 year old kids have no interest in programming.  They like to push buttons and watch things happen immediately.

    Even 18-25 year olds in my classes have difficulty with programming, concepts like pull-up resistors, and current limiting.

    Good luck with your project, I would suggest going to a school and talking to teachers about what would be appropriate for the age group you are targeting.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to Capper

    10 year old kids have no interest in programming.  They like to push buttons and watch things happen immediately.

    Even 18-25 year olds in my classes have difficulty with programming, concepts like pull-up resistors, and current limiting.

    I'm not a full time teacher, but I am a mentor for two free programs we run at various schools.

    The first is assembling (inc soldering) and programming a picaxe based Xmas Tree, which they get to keep.

    These pupils are year 7 (11/12 yr olds)

    The second is a full day introducing pupils to Arduino programming and we target the year 8 (12/13 yrs old)

     

    From both of these I can assure you many of them are interested if they have good examples and are shown and helped.

     

    In some cases it is a matter of having different examples (we're unlucky to have so many roadworks here in Christchurch that the concept of limiting flow due to the roadwarks is easy to explain and compare to a resistor) and in some cases it might take a bit more until the "Ahh Haa" moment strikes.

     

    I have found that once you've captured them with changing the blink program, it's easy to introduce new bits and then it just snowballs and they are hooked.

    It does help that it is a full day, and I have done one with 2 hr sessions over 5 weeks and it was not as productive.

     

    So Scott I'm not sure my experience would support your comments.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 10 years ago in reply to Capper

    10 year old kids have no interest in programming.  They like to push buttons and watch things happen immediately.

    Even 18-25 year olds in my classes have difficulty with programming, concepts like pull-up resistors, and current limiting.

    I'm not a full time teacher, but I am a mentor for two free programs we run at various schools.

    The first is assembling (inc soldering) and programming a picaxe based Xmas Tree, which they get to keep.

    These pupils are year 7 (11/12 yr olds)

    The second is a full day introducing pupils to Arduino programming and we target the year 8 (12/13 yrs old)

     

    From both of these I can assure you many of them are interested if they have good examples and are shown and helped.

     

    In some cases it is a matter of having different examples (we're unlucky to have so many roadworks here in Christchurch that the concept of limiting flow due to the roadwarks is easy to explain and compare to a resistor) and in some cases it might take a bit more until the "Ahh Haa" moment strikes.

     

    I have found that once you've captured them with changing the blink program, it's easy to introduce new bits and then it just snowballs and they are hooked.

    It does help that it is a full day, and I have done one with 2 hr sessions over 5 weeks and it was not as productive.

     

    So Scott I'm not sure my experience would support your comments.

     

    Mark