Arduino Forum Will any capacitor work?
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
  • State Verified Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 395 subscribers
  • Views 667 views
  • Users 0 members are here
  • ceramic
  • capacitors
  • fm
  • make
  • transmitter
  • radio
  • disks
Related

Will any capacitor work?

Former Member
Former Member over 10 years ago

So I'm working on this project, well more like buying parts for it: https://www.youtube.com/watch?v=MMgzUGBfXiE

 

And I have a bunch of these capacitors:

 

image

101 Suntan ceramic disk capacitors that is.

 

And in the video he has two ceramic disk capacitors and two little blue capacitors. My question is, can I build this build without the other type of capacitor or would I need to buy both? If so what is the name for those little blue dudes?

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to clem57 +3
    Only the big blue one is an electrolytic, the two small "Dudes" are ceramic caps, an electrolytic would never get to that small a value or work at the frequency required Peter
  • lokkytron
    lokkytron over 10 years ago +1 suggested
    Hello Jacob Pickens I do not think you can get it done with any type of capacitor... in the video that you linked you can hear that the blue one is a electrolitic capacitor and it is mandatory observe…
  • clem57
    clem57 over 10 years ago +1 verified
    Electrolytic capacitor is the blue dudes. Unless you design electronics on the side, I recommend you to follow the instructions especially the coil. Neat idea btw. Enjoy the project, Clem
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    So it looks like you need

    2* 10nF Ceramic Cap (Brown ones)

    2* 10pF Ceramic cap (Little Blue ones)

    1 Electrolytic Cap (Big Blue one), this one is for AC coupling the audio so probably any value from 4.7uF to over 47uF will do

     

    None of these can be substituted with other values  except the Electrolytic as I have mentioned

     

    Hope this helps

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    So it looks like you need

    2* 10nF Ceramic Cap (Brown ones)

    2* 10pF Ceramic cap (Little Blue ones)

    1 Electrolytic Cap (Big Blue one), this one is for AC coupling the audio so probably any value from 4.7uF to over 47uF will do

     

    None of these can be substituted with other values  except the Electrolytic as I have mentioned

     

    Hope this helps

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer