Arduino Forum Will any capacitor work?
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
  • State Verified Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 395 subscribers
  • Views 667 views
  • Users 0 members are here
  • ceramic
  • capacitors
  • fm
  • make
  • transmitter
  • radio
  • disks
Related

Will any capacitor work?

Former Member
Former Member over 10 years ago

So I'm working on this project, well more like buying parts for it: https://www.youtube.com/watch?v=MMgzUGBfXiE

 

And I have a bunch of these capacitors:

 

image

101 Suntan ceramic disk capacitors that is.

 

And in the video he has two ceramic disk capacitors and two little blue capacitors. My question is, can I build this build without the other type of capacitor or would I need to buy both? If so what is the name for those little blue dudes?

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to clem57 +3
    Only the big blue one is an electrolytic, the two small "Dudes" are ceramic caps, an electrolytic would never get to that small a value or work at the frequency required Peter
  • lokkytron
    lokkytron over 10 years ago +1 suggested
    Hello Jacob Pickens I do not think you can get it done with any type of capacitor... in the video that you linked you can hear that the blue one is a electrolitic capacitor and it is mandatory observe…
  • clem57
    clem57 over 10 years ago +1 verified
    Electrolytic capacitor is the blue dudes. Unless you design electronics on the side, I recommend you to follow the instructions especially the coil. Neat idea btw. Enjoy the project, Clem
Parents
  • 4ringfan
    0 4ringfan over 10 years ago

    Their suggestion to use a machine screw to generate the coil is an excellent one and it works very very well.

     

    Awesome little FM transmitter!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 4ringfan
    0 4ringfan over 10 years ago

    Their suggestion to use a machine screw to generate the coil is an excellent one and it works very very well.

     

    Awesome little FM transmitter!