Arduino
  • Products
  • More
Arduino
Arduino Forum SAP
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Subscribers 421 subscribers
  • Views 1542 views
  • Users 0 members are here
Related

SAP

rishi2628
rishi2628 over 11 years ago

Can anyone suggest me a technique ?

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 11 years ago +2
    Sounds very much like a college project.
  • 4ringfan
    4ringfan over 11 years ago in reply to dougw +2 verified
    Your robot could have one ball in the center in contact with the ground and then X and Y counter wheels that pulse count its movement. Heck you could probably hack a computer mouse to do it. Then once…
  • clem57
    clem57 over 11 years ago +1
    http://www.robotshop.com/blog/en/how-to-make-a-robot-lesson-7-using-sensors-2-3683 shows almost any type of sensor you could use as well as a means to limit where it may go. Clem
Parents
  • dougw
    0 dougw over 11 years ago

    You could use an infrared strobe to trigger an ultrasonic ping on the robot.

    The strobe would also start a timer on each of 2 ultrasonic receivers - when they receive the ping, the time of arrival will indicate exactly how far the robot is from that receiver. 2 known distances will uniquely locate the robot on a flat surface.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 4ringfan
    0 4ringfan over 11 years ago in reply to dougw

    Your robot could have one ball in the center in contact with the ground and then X and Y counter wheels that pulse count its movement.  Heck you could probably hack a computer mouse to do it.  Then once you set it's home position, you can locate the robot using an X and Y position from the 0,0 home position.  Realize that if the robot gets lifted or sufficiently bumped that all bets are off.  You could consider a combination of methods, to keep your accuracy.

     

    A top down view will probably be the most accurate method though.

     

    Good luck!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • 4ringfan
    0 4ringfan over 11 years ago in reply to dougw

    Your robot could have one ball in the center in contact with the ground and then X and Y counter wheels that pulse count its movement.  Heck you could probably hack a computer mouse to do it.  Then once you set it's home position, you can locate the robot using an X and Y position from the 0,0 home position.  Realize that if the robot gets lifted or sufficiently bumped that all bets are off.  You could consider a combination of methods, to keep your accuracy.

     

    A top down view will probably be the most accurate method though.

     

    Good luck!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer