Arduino Forum problem with if else to run different sequences
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
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 391 subscribers
  • Views 322 views
  • Users 0 members are here
Related

problem with if else to run different sequences

peteypieca
peteypieca over 10 years ago

I am new to Arduino. I have a GE Fanuc PLC that controls the LEDs on my motorcycle. It runs through six different sequences. The problem is it only has six outputs. I want to replace it with an Arduino UNO. I have the Knight rider sketch which I am building off of. I have added two other flashing sequences and have each selected by different combinations of two switches. My problem is the first ( Knight rider) sequence works, but when I change the switches all sequences seem to run instead of only the one which is selected. The IF / ELSE statements do not seem to be working.

Here is a copy of my code. Thanks for any help that you can give.

 

//LED Sequencer with variable speed and program/sequence select

 

int prog1=13;

int prog2=12;

int speedpot0 = 0;

int speedpot1 = 1;

int pinArray[] = {1, 2, 3, 4, 5, 6, 7, 8,9,10,11};

int count = 0;

int timer = 30;

int timer2 = 1000;

int timer3 = 50;

int timer4 = 250;

int led1=1;

int led2=2;

int led3=3;

int led4=4;

int led5=5;

int led6=6;

int led7=7;

int led8=8;

int led9=9;

int led10=10;

int led11=11;

 

 

 

 

 

 

 

 

void setup(){

pinMode (prog1, INPUT);

pinMode (prog2, INPUT);

 

   for (count=0;count<11;count++) {

    pinMode(pinArray[count], OUTPUT);

      }

}

 

 

void loop() {

 

if (digitalRead(prog1)==HIGH && digitalRead(prog2)==LOW)

  {

  int val0 = analogRead(speedpot0);

  val0 = constrain(val0, 100,900);

  int timer = map(val0,100, 900, 0, 50);

 

   analogWrite(speedpot0, timer);

 

  for (count=0;count<10;count++) {

   digitalWrite(pinArray[count], HIGH);

   delay(timer);

   digitalWrite(pinArray[count + 1], HIGH);

   delay(timer);

   digitalWrite(pinArray[count], LOW);

   delay(timer*2);

  }

  for (count=10;count>0;count--) {

   digitalWrite(pinArray[count], HIGH);

   delay(timer);

   digitalWrite(pinArray[count - 1], HIGH);

   delay(timer);

   digitalWrite(pinArray[count], LOW);

   delay(timer*2);

  }

}

 

 

else if (digitalRead(prog1)==LOW && digitalRead(prog2)== HIGH);

  {

      int val1 = analogRead(speedpot1);

      val1 = constrain(val1, 100,900);

      int timer3 = map(val1,100, 900, 0, 1000);

    analogWrite (speedpot1, timer3);

    digitalWrite (led1, HIGH);

    digitalWrite (led2, HIGH);

    digitalWrite (led3, HIGH);

    digitalWrite (led4, HIGH);

    digitalWrite (led5, HIGH);

    digitalWrite (led6, HIGH);

    digitalWrite (led7, HIGH);

    digitalWrite (led8, HIGH);

    digitalWrite (led9, HIGH);

    digitalWrite (led10, HIGH);

    digitalWrite (led11, HIGH);

 

 

  delay(timer3);

 

    digitalWrite (led1, LOW);

    digitalWrite (led2, LOW);

    digitalWrite (led3, LOW);

    digitalWrite (led4, LOW);

    digitalWrite (led5, LOW);

    digitalWrite (led6, LOW);

    digitalWrite (led7, LOW);

    digitalWrite (led8, LOW);

    digitalWrite (led9, LOW);

    digitalWrite (led10, LOW);

    digitalWrite (led11, LOW);

   

    delay(timer3); }

 

  

       if (digitalRead(prog1)==HIGH && digitalRead(prog2)== HIGH);

    {

     int val1 = analogRead(speedpot1);

      val1 = constrain(val1, 100,900);

      int timer3 = map(val1,100, 900, 0, 1000);

    analogWrite (speedpot1, timer3);

   

    digitalWrite (led1, HIGH);

    digitalWrite (led2, HIGH);

    digitalWrite (led3, HIGH);

    digitalWrite (led4, HIGH);

    digitalWrite (led5, HIGH);

    digitalWrite (led6, LOW);

    digitalWrite (led7, LOW);

    digitalWrite (led8, LOW);

    digitalWrite (led9, LOW);

    digitalWrite (led10, LOW);

   digitalWrite (led11, LOW);

 

 

delay(timer3);

 

   digitalWrite (led1, LOW);

   digitalWrite (led2, LOW);

   digitalWrite (led3, LOW);

   digitalWrite (led4, LOW);

   digitalWrite (led5, LOW);

   digitalWrite (led6, HIGH);

   digitalWrite (led7, HIGH);

   digitalWrite (led8, HIGH);

   digitalWrite (led9, HIGH);

   digitalWrite (led10, HIGH);

   digitalWrite (led11, HIGH);

   

   delay(timer3); }

 

 

   

      if (digitalRead(prog1)== LOW && digitalRead(prog2) == LOW);

  {  digitalWrite (led1, HIGH);

  digitalWrite (led2, HIGH);

    digitalWrite (led3, HIGH);

    digitalWrite (led4, HIGH);

    digitalWrite (led5, HIGH);

    digitalWrite (led6, HIGH);

    digitalWrite (led7, HIGH);

    digitalWrite (led8, HIGH);

    digitalWrite (led9, HIGH);

    digitalWrite (led10, HIGH);

    digitalWrite (led11, HIGH); }

 

 

}

  • Sign in to reply
  • Cancel
  • xever
    0 xever over 10 years ago

    Hi Robert,

     

    if/else block do work, however, your code has a trivial bug such that you put a semi-colon at the end of the else if block.  in one of your lines you have the following:


    else if (digitalRead(prog1)==LOW && digitalRead(prog2)== HIGH);


    as you can see you have semi-colon at the end of this line, this will be interpreted similarly as:


    else if (digitalRead(prog1)==LOW && digitalRead(prog2)== HIGH)

    {

        ;

    }


    which basically does nothing and so your code will flow onto the next line regardless the condition.


    Another issue would be your if-else blocks.  I would recommend though that you functionalise your code like:

    void loop() 
    {
        if (digitalRead(prog1) == HIGH && digitalRead(prog2) == LOW)
        {
            led_sequence1();
        }
        else if (digitalRead(prog1) == LOW && digitalRead(prog2) == HIGH)
        {
            led_sequence2();
        }
        else if (digitalRead(prog1) == HIGH && digitalRead(prog2) == HIGH)
        {
            led_sequence3();
        }
        else (digitalRead(prog1) == LOW && digitalRead(prog2) == LOW)
        {  
            led_sequence4();
        }
    }

     

    where each led_sequence is the block of code you have as above.  Having this code structure would make debugging easier and have your code a bit more readable. image  Hope this is helpful. 

     

    Also, I think it would also be helpful if you read/learn the basics of C or C++, as that would accelerate your understanding on how code flows. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • peteypieca
    0 peteypieca over 10 years ago

    Thanks so much for the help. The program is running well. I have a question about your code structure suggestion.

    Does the " led_sequence1();" have to be declared at the beginning then called or is it just a comment to Identify each part of the program?

    I am sorry for the dumb questions. I do want to take a course in C when I get home. I haven't programmed in thirty years and that was assembly language for the Z-80 microprocessor.

    1. if (digitalRead(prog1) == HIGH && digitalRead(prog2) == LOW) 
    2.     { 
    3.         led_sequence1(); 
    4.     }