Arduino Forum A sneaky problem
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
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 392 subscribers
  • Views 625 views
  • Users 0 members are here
  • signal
  • status
  • digital
  • tactile_switch
  • tactile
  • arduino
  • relay
Related

A sneaky problem

balearicdynamics
balearicdynamics over 10 years ago

Hi to all.

 

I have a sneaky problem with Arduino initial pin settings. When the program starts, it should put a pin to 0 accordingly with the initial program flag status. This signal will change the on/off status (i.e. powered status) of a micro relay activated by a NPN 2222 transistor. The circuit part works perfectly and the initialisation code is the following:

 

int powerStatus;

 

void setup() { 

  pinMode(8, OUTPUT); // Relay ON/OFF

  pinMode(7, INPUT);  // Power Button

 

  powerStatus = 0; // Initial power status relay

    // Power OFF the relay

    digitalWrite(8, 0);


}

 

What I expect is that the relay is intially in the OFF state.

Then in the loop function every time that a pushbutton is pressed the state is changed from ON to OFF and vice versa. This works without problems but when the Arduino board is powered and the program starts, the relay is powered.

The loop test program is the following:

 

void loop() {

  // Check if the button is pressed  

  if( (digitalRead(7) == 0) {

     // Invert the power status of the relay

     if(powerStatus == 0)

       powerStatus = 1;

     else

       powerStatus = 0;

    // Power ON or OFF the relay

    digitalWrite(8, powerStatus);

    delay(500);

  }

}

 

Some ideas where I have done mistakes ?

 

Thanks in advance. Enrico

 

FOUND THE MISTAKE

The relais works in negative logic driver by the NPN 2222 transistor controlled by pin  8: means that as a matter of fact, when the pin has the logical value 1 there is no activity on the transistor, there is no GND to the relay and it is OFF. The following is the working code including a serial monitor to see how the operation works.

 

#include <Streaming.h>

 

int powerStatus;

 

#define RELAY_ON 0

#define RELAY_OFF 1

 

void setup() {

  pinMode(8, OUTPUT); // Relay ON/OFF

  pinMode(7, INPUT);  // Power Button

 

  // First, setup the relay 

  powerStatus = RELAY_OFF; // Initial power status realis

  digitalWrite(8, powerStatus);

 

  // Init serial and dump setup status

  Serial.begin(19200);

  Serial << "setup() - START" << endl;

  Serial << "powerStatus = " << powerStatus << " - written to pin 8 (relay)" << endl;

  Serial << "setup() - END" << endl << endl;

}

 

void loop() {

 

  if(digitalRead(7) == 0) {

     if(powerStatus == RELAY_ON)

       powerStatus = RELAY_OFF;

     else

       powerStatus = RELAY_ON;

      

    digitalWrite(8, powerStatus);

    Serial << "powerStatus = " << powerStatus << " wrtieen on pin 8 (relay)" << endl;

 

 

    delay(1000);

  } // button pressed

 

} // loop

 

 

Message was edited by: Enrico Miglino

  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 10 years ago in reply to lokkytron +1
    Thank you for the support. As the code had to be correct, there was a problem in the logic. I have updated the question with the right code and the serial debug information. Thank you, lokkytron
Parents
  • terryking
    0 terryking over 10 years ago

    Hi,

    Sometimes you need to have a pin always be 1 or 0 at the time the pin is set to output. Like in your case, you want to be sure the pin is at 1 (relay inactive) when Setup sets the pin to output. You can do that in setup by FIRST writing the pin to 1 and THEN doing pinMode. Then when you reset the Arduino the pin is never actively driven to 0, even for a very short time.

     

    See example code of this on the http://ArduinoInfo.Info wiki HERE:  http://arduino-info.wikispaces.com/ArduinoPower#4-8http://

     

    Regards, Terry King

    ...In The Woods in Vermont, USA

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to terryking

    terryking , you are right. The last minor - but meaningful - change I have done to the relais connection is to move the transistor output to the other point of the relais. Also with the right initial pin setting (1 instead 0) there was anyway the problem that immediately at power-on the status of the pin was not the same as what I set in the setup() function. At this point, I have moved the power-off) status to the relay on and vice-versa the normal condition of relay-on is when the relay is off. Now at power-on the ping goes high, the transistor is excited and the relay is powered. The result is that the external device power is switched off. At this point, I initialise the pin value to 0 and all remain powered off without the disturbing initial on-off.

     

    I hope I had explained correctly this concept image

     

    Cheers, Enrico

    ...From the sunny seaside of Ibiza

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to terryking

    terryking , you are right. The last minor - but meaningful - change I have done to the relais connection is to move the transistor output to the other point of the relais. Also with the right initial pin setting (1 instead 0) there was anyway the problem that immediately at power-on the status of the pin was not the same as what I set in the setup() function. At this point, I have moved the power-off) status to the relay on and vice-versa the normal condition of relay-on is when the relay is off. Now at power-on the ping goes high, the transistor is excited and the relay is powered. The result is that the external device power is switched off. At this point, I initialise the pin value to 0 and all remain powered off without the disturbing initial on-off.

     

    I hope I had explained correctly this concept image

     

    Cheers, Enrico

    ...From the sunny seaside of Ibiza