Arduino
  • Products
  • More
Arduino
Arduino Forum Need a hand, reading temperature from a NTC thermistor 10k (calibration)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 416 subscribers
  • Views 1183 views
  • Users 0 members are here
  • ntc
  • temperature
  • thermistor
  • reading
  • arduino
Related

Need a hand, reading temperature from a NTC thermistor 10k (calibration)

e14 Contributor
e14 Contributor over 11 years ago

Hi,

 

I'm trying to get a reading of a NTC thermistor, because i want to measure and log water temperature from a garden pond.

I have tryed reading trough the different tutorials on the arduino playground and i can conclude they only work for PTC thermistors.

Same problem with adafruit tutorials.

 

Arduino Playground - Thermistor2

 

And guess what, I'm stuck with some NTC thermistors, which is kinda annoying because the initial base value checks out ok.

But when I either increase or decrease the temperature, the value sendt to the arduino is the "inverse"

 

Meaning, my base value reading is usually  "-22.00" degrees,  well it's sorta correct, it's really +22.00

Well if that was the only problem, then i would just multiply with -1,

 

However, as the thermistor heats up, the value drops, well that is also ok i guess.  from -22 to -16 is a heat increase of 6 degrees..

So..  how would you suggest i go about reading the temperature correctly ?

 

Hardware :

 

NTC thermistor 10k , (I'm worried the seller might have sold me a 100k set)

10k pull down resistor

 

//Schematic:

// [Ground] ---- [10k-Resistor] -------|------- [Thermistor] ---- [+5v]

//                                                |

//                                          Analog Pin 0



My favorite code is the one from Arduino Playground - Thermistor2


The last one called "The Elaborate, cleaned up a bit"  image 


But I'm getting annoyed to switched to something far simpler



************************************** [code] or

dosent work, anyway code starts here.

#include <math.h>

 

void setup() {

Serial.begin(9600);

}

 

double Thermister(int RawADC) {

  double Temp;

  // See http://en.wikipedia.org/wiki/Thermistor for explanation of formula

  Temp = log(((10240000/RawADC) - 10000));

  Temp = 1 / (0.001129148 + (0.000234125 * Temp) + (0.0000000876741 * Temp * Temp * Temp));

  Temp = Temp - 273.15;           // Convert Kelvin to Celcius

  return Temp;

}

 

void loop() {

   double temp = Thermister(analogRead(0));

   Serial.println(temp);

   delay(2000);

}

 



Any help would be greatly appriciated

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Well of course my wife (vera) came and said, why don't you just add some degrees to the base value..

     

    So i changed the line

     

    Temp = Temp - 273.15;

     

    to

     

    Temp = Temp - 273.15 + 44;  // Adding the Vera Factor..


    And i guess that works. image  still very strange... 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Well of course my wife (vera) came and said, why don't you just add some degrees to the base value..

     

    So i changed the line

     

    Temp = Temp - 273.15;

     

    to

     

    Temp = Temp - 273.15 + 44;  // Adding the Vera Factor..


    And i guess that works. image  still very strange... 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer