Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum tesla turbine
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 417 subscribers
  • Views 1701 views
  • Users 0 members are here
  • question
Related

tesla turbine

e14 Contributor
e14 Contributor over 11 years ago

Hello,

Can anyone please guide me on how to make a tesla turbine from scratch.

I am actually a under-grad student of mechanical engineering right now with just enough knowledge so please make it simple if possible.

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago +1
    Hi Safeer, You can get raw disk from Hard Disk, I'd recomment desktop hardisk since they tends to be bigger (3.747") and made in aluminium most of the time, you can still use old server HDD, however, they…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Workshopshed +1
    thanks but looks like i will be able to get by somehow now i some how solved it but thanks any ways
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Safeer,

     

    You can get raw disk from Hard Disk, I'd recomment desktop hardisk since they tends to be bigger (3.747") and made in aluminium most of the time, you can still use old server HDD, however, they tends to be in glass/ceramic which shatters when you attempt to drill them, or the disk size is too small. So you need to check and make sure if they are in aluminium only.

     

    Further, considering you are an undergraduate student in the mech department, short answer, it behaves like an impulse turbine. If you attempt to put high pressure without nozzle, then you're turbine won't turn.

     

    Here is an outdated video of my tesla turbine using HDD. It has to use 100 PSI with massive pressure lost due to set up, in order to achieve 20k rpm with no load. Our current configuration allows to feed a pressure of 9-11 PSI and running above 25k RPM with actual load.

     

    https://www.youtube.com/watch?v=1jxzXSF5ons

     

    But yea, and don't be cheap when you will be choosing the bearing, because they gets really hot.... and you need to pick some good quality.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Safeer,

     

    You can get raw disk from Hard Disk, I'd recomment desktop hardisk since they tends to be bigger (3.747") and made in aluminium most of the time, you can still use old server HDD, however, they tends to be in glass/ceramic which shatters when you attempt to drill them, or the disk size is too small. So you need to check and make sure if they are in aluminium only.

     

    Further, considering you are an undergraduate student in the mech department, short answer, it behaves like an impulse turbine. If you attempt to put high pressure without nozzle, then you're turbine won't turn.

     

    Here is an outdated video of my tesla turbine using HDD. It has to use 100 PSI with massive pressure lost due to set up, in order to achieve 20k rpm with no load. Our current configuration allows to feed a pressure of 9-11 PSI and running above 25k RPM with actual load.

     

    https://www.youtube.com/watch?v=1jxzXSF5ons

     

    But yea, and don't be cheap when you will be choosing the bearing, because they gets really hot.... and you need to pick some good quality.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Thanks man it was really helpful.

    I was wondering if you had any data on the tesla turbine.

    I was thinking of making a small testing setup which might be used as a testing bed in the future.

    Thanks once again.