Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Yun: rest calls over internet?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 410 subscribers
  • Views 1147 views
  • Users 0 members are here
  • internet
  • yun
  • rest
  • api
  • arduino
Related

Arduino Yun: rest calls over internet?

Former Member
Former Member over 10 years ago

Hello everyone,

I've used my Arduino Yùn to control pins, to set and read variables from my browser through local area network using REST api.

The goal is to do the same thing from a remote PC over internet. I've got a Public and STATIC IP Address of the Yùn to localize it over the network, but how can I accomplish this task?

There are some examples for CC3000 chip (aREST api), but not written for the Yùn.

Any ideas? Thanks...

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago in reply to Former Member +1 suggested
    Yes alexmawashi If the IP address is public and static (not 192.168 because that is not public or rout-able). Or you have to use IP forwarding/NAT to a valid internet address... Oh you want to use security…
Parents
  • clem57
    0 clem57 over 10 years ago

    If you wish to use the REST api, any browser that has network access to the Yun can control the Yun. Maybe I do not understand your question.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    With rest.h libraries you can control a Yun and connect to it only if your computer is connected at the same Local Area Network of the Yun.

    So you have Computer, Your Modem and the Yun connected in a LAN.

    INSTEAD, I need to control and connect to the Yun via internet. So I have my computer here in Italy, and the Yun in America for istance. Is that possible in a practical way?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    With rest.h libraries you can control a Yun and connect to it only if your computer is connected at the same Local Area Network of the Yun.

    So you have Computer, Your Modem and the Yun connected in a LAN.

    INSTEAD, I need to control and connect to the Yun via internet. So I have my computer here in Italy, and the Yun in America for istance. Is that possible in a practical way?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    Yes alexmawashi If the IP address is public and static (not 192.168 because that is not public or rout-able). Or you have to use IP forwarding/NAT to a valid internet address... Oh you want to use security or you may get someone else controlling it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    Thanks very much Clem for helping out.

     

    Very much appreciated.