Arduino Forum RA8875 + 7'' TFT + ARDUINO UNO = WORKING having issues with images loading slow
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
  • State Not Answered
  • Replies 18 replies
  • Subscribers 402 subscribers
  • Views 1280 views
  • Users 0 members are here
Related

RA8875 + 7'' TFT + ARDUINO UNO = WORKING having issues with images loading slow

Former Member
Former Member over 10 years ago

hello I managed to run audio and imaging into my Arduino Uno project.

the project consist off:

 

- RA8875

- Arduino Uno

- MP3 with SD Card

- 7'' TFT Screen

 

Pixels are 800 X 480

the only issue that i am encountering is that the images are taking 1 minute and 30 seconds to fully load up.

images are in bmp format. i was wondering if there is any solution to this problem. 

any feedbacks will be grateful. if images can be done in any other format that can potentially be faster i would gladly take it into consideration as well considering its an arduino.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    Are the images slow when running the MP3? Or without? also what is the clock speed for the SPI interface? It may be the Arduino is 8 Mhz trying to drive the SPI fast and MP3... A video could help here...

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    no the image was not slow when running the mp3. I did not set any clock speed, its in its standard clock speed. thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    no the image was not slow when running the mp3. I did not set any clock speed, its in its standard clock speed. thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    Can you drop the sketch here? It may need some optimization.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    i mean it always been slow. I haven't been able to make it run any faster. i will give you the sketch to have a look at. is it possible to email it to you ?