Arduino Forum Multiple I2C connections, best way?
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 392 subscribers
  • Views 322 views
  • Users 0 members are here
  • multiple
  • i2c
  • connections
  • arduino
Related

Multiple I2C connections, best way?

screamingtiger
screamingtiger over 10 years ago

If I need to connect multiple slaves to a master, whats a good way to do that without a PCB?

The master has a pin header but the slaves do not, requiring soldering.

 

I've though of splicing wires but wondered if there is something out there to aid in this.

 

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 10 years ago +2
    Why not a breadboard? Get some male-male jumper cables and you should be good to go! If you're looking for a permanent solution, I don't think there are any options that don't require soldering...
  • johnbeetem
    johnbeetem over 10 years ago in reply to Former Member +1
    Francesco Truzzi wrote: If you're looking for a permanent solution, I don't think there are any options that don't require soldering... If you can get components as DIPs you can use wire-wrap. However…
  • screamingtiger
    screamingtiger over 10 years ago +1
    Thanks for the information. What I mean is the physical connection between multiple slaves. If I had 10 slaves, all of then would be connected to 2 pins on the Master. I'll probably end up using one of…
Parents
  • Former Member
    0 Former Member over 10 years ago

    Why not a breadboard? Get some male-male jumper cables and you should be good to go!

     

    If you're looking for a permanent solution, I don't think there are any options that don't require soldering...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 10 years ago in reply to Former Member

    Francesco Truzzi wrote:

     

    If you're looking for a permanent solution, I don't think there are any options that don't require soldering...

    If you can get components as DIPs you can use wire-wrap.  However, even with wire-wrap, you'll probably want to solder at least power and ground, and may need to solder discrete components onto a plug-in header.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 10 years ago in reply to Former Member

    Francesco Truzzi wrote:

     

    If you're looking for a permanent solution, I don't think there are any options that don't require soldering...

    If you can get components as DIPs you can use wire-wrap.  However, even with wire-wrap, you'll probably want to solder at least power and ground, and may need to solder discrete components onto a plug-in header.