Arduino Forum Arduino - Two Inputs Using the Keypad.
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
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 403 subscribers
  • Views 1841 views
  • Users 0 members are here
Related

Arduino - Two Inputs Using the Keypad.

Former Member
Former Member over 10 years ago

Hey guys,

i am new to arduino. i am currently working on a small project. basically i am using the 4 x 4 keypad for the input and LCD for display. so once the program runs the user enters two value. so first input is 2 digit input which arduino saves in an array and similarly the second input is a four digit input that is saved into the second array. The program runs successfully and reads the first input correctly though the second input does not work.

 

if (int(key1) != 0 and currentState == 1) {

 

switch (key1) {

case '*':

// sets the first array to zero

currentState = 1;

break;

 

case '#':

//saves the value into the first array

//sets the currentState to 2

currentState = 2;

if (currentState = 2){

switch (key1){

case '*':

//sets the second array to zero

currentState = 2;

break;

case '#':

//saves the value into the second array

currentState = 1;

break;

 

case 'A':

//goes back to the menu

break;

 

default:

currentTValue[0] = currentTValue[1];

currentTValue[1] = key1;

break;

}

}

break;

 

case 'A':

//goes back to the menu

break;

 

default:

currentT2Value[0] = currentT2Value[1];

currentT2Value[1] = currentT2Value[2];

currentT2Value[2] = currentT2Value[3];

currentT2Value[3] = key1;

break;

}

}

}

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    You have the classic beginner mistake of using an assignment where you want to perform a comparison currentState = 2 is an assignment not a compare currentState == 2 is a comparison and will return a true…
  • mcb1
    mcb1 over 10 years ago +1 verified
    if (currentState = 2) needs to be if (currentState == 2) Although I'm unsure why you check when you set it the line above and several lines later. Do you really need line 12 and 13 ? if (int(key1) !…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to mcb1 +1
    A very good and valid point Mark, I was not intending to deminish your valued input, just focus on the lesser issue of the use of comparison vs assignment operators to help Terry along. And yes, it is…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    You have the classic beginner mistake of using an assignment where you want to perform a comparison

     

    currentState = 2 is an assignment not a compare

    currentState == 2 is a comparison and will return a true or false that is needed by an "if" statement of other commands like "while and do"

     

    the comparison operators extend to != (Not equal), <= Less than or equal, >= Greater than or equal, || Logical OR of the two values, && Logical AND of two values

     

    so a logical or could be " if (currentValue >= 5) && (currentValue <= 10)"

    in this case if the current value is between 5 and 10 including 5 and 10 then a true would be returned

     

    If the expression was this  " if (currentValue >= 10) || (currentValue <= 5)" then anything between 5 and 10 would return true

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to Robert Peter Oakes

    Peter

    While the incorrect operator has been used, there is the question of why check when you set it in the line above.

     

    It's possible the case statement is missing an ending, or similar.

     

     

    I suspect some cutting and pasting went wrong.

    Since the code is not complete, I left it at that issue.

     

    Terry will come back with some clues as to what it should do.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 10 years ago in reply to Robert Peter Oakes

    Peter

    While the incorrect operator has been used, there is the question of why check when you set it in the line above.

     

    It's possible the case statement is missing an ending, or similar.

     

     

    I suspect some cutting and pasting went wrong.

    Since the code is not complete, I left it at that issue.

     

    Terry will come back with some clues as to what it should do.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to mcb1

    A very good and valid point Mark, I was not intending to deminish your valued input, just focus on the lesser issue of the use of comparison vs assignment operators to help Terry along.

     

    And yes, it is probably a copy paste issue.  Terrry... Your turn image