Arduino
  • Products
  • More
Arduino
Arduino Forum wire transfer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 401 subscribers
  • Views 228 views
  • Users 0 members are here
Related

wire transfer

Former Member
Former Member over 10 years ago

i am trying to get the voice shield to play the pre recorded sound when the keypad is pushed on the sender. the voice shield is on the receiver, and i am also having issues getting the info to display on the LCD screen, the only thing i see on the LCD screen is -1 and i dont know why.

 

sender code

//Sender

#include <Wire.h>

#include <SoftwareSerial.h>

#include <Keypad.h>                  //This is the library for the key pad

#include <TinyGPS.h>

//#include<VoiceShield.h>

const int inPin=A0;

float temp;

int tempPin = A0;

const int heartratePin = A1;

int difference;

int newHeartReading = 0;

int lastHeartReading = 0;

int measurements[5] = {0,0,0,0,0};

int historySize = 5;

int recenttotal = 0;

int Index = 0;

boolean highChange = false;

int minimumdifference = 2;

int num[5];

int average=0;

SoftwareSerial GPS(11,12); // configure software serial port

TinyGPS shield;

// Heart rate timing

long lastHeartbeatTime = 0;

long debounceDelay = 150;      // the debounce time; increase if the output flickers

int currentHeartrate = 0;

int lastHeartrate = 0;

int slope = ((newHeartReading-lastHeartReading)/(debounceDelay-lastHeartrate));

// Debugging string

String debugOutput = "";

const byte ROWS = 4; //four rows

const byte COLS = 3; //three columns

char keys[ROWS][COLS] = {

        {'1','2','3'},

        {'4','5','6'},

        {'7','8','9'},

        {'*','0','#'}

        };

byte rowPins[ROWS] = {5, 4, 3, 2}; //connect to the row pinouts of the keypad

//byte rowPins[ROWS] = {38, 39, 40, 41}; //connect to the row pinouts of the keypad

byte colPins[COLS] = {8, 7, 6}; //connect to the column pinouts of the keypad

//byte colPins[COLS] = {42, 43, 44}; //connect to the column pinouts of the keypad

 

 

Keypad keypad = Keypad( makeKeymap(keys), rowPins, colPins, ROWS, COLS );

byte ledPin = 13;

//VoiceShield vs(80);              // Create a instance of the Voice Shield called "vs" with 80 sound slots

 

 

/*int i = 1;

int Sentence[16];

int Phs1[] = {

  33, 78, 72, 255};    // "I am cold"

int Phs2[] = {

  33, 78, 16};            // "I am sick"

int Phs3[] = {

    33, 44, 69};        // "I want food"

  */

void setup()

{

  Wire.begin(); // join i2c bus (address optional for master)

  GPS.begin(9600);

    Serial.begin(9600);

}

 

 

void getgps(TinyGPS &gps)

  {

    // Define the variables that will be used

    float latitude, longitude;

    // Then call this function

    shield.f_get_position(&latitude, &longitude);

  }

 

 

 

 

void loop()

{

  int value = analogRead(inPin);

  Wire.beginTransmission(4); // transmit to device #4

  float millivolts = (value/1024.0)*5000;

  float celsius = millivolts/10-50;

  //temp = analogRead(tempPin);

  //temp = temp * 0.48828125;

  Wire.println("TEMPRATURE = ");

  Wire.println(celsius);

  Wire.println("*C");

  Wire.println();

// lcd.setCursor(0,1);

  Wire.println((celsius * 9)/5 +32);

  Wire.println("*F");

  Wire.println();

  newHeartReading = analogRead(heartratePin);

  // Wire.beginTransmission(1); // transmit to device #4

  //calculation

  difference = newHeartReading - lastHeartReading;

  lastHeartReading = newHeartReading;

 

  // Find new recent total

  recenttotal = recenttotal - measurements[Index] + difference;

  // replace indexed recent value

  measurements[Index] = difference;

  //index + 1 index = (index + 1) % historySize;

    for (int i=0; i<5; i=i+1){

              num[i]=0;

  }

 

              if (Index>=5)

              Index=0;

              //calculating the average

              average=recenttotal/5;

              Wire.println(average);

              //delay(100);

  if (recenttotal >= minimumdifference)

  {

    // possible heart rate check timing

    if (millis() - lastHeartbeatTime >= debounceDelay)  // whatever the reading is at, it's been there for longer

    // than the debounce delay, so take it as the actual current state:

 

 

    {

  // Heart rate

 

  currentHeartrate = 60000 / (millis() - lastHeartbeatTime);

    lastHeartbeatTime = millis();

    if (currentHeartrate <= 200)// && currentHeartrate > 20)

    {

  

                  Wire.println("Heart Rate =" + String(currentHeartrate) + "  ");

                // delay(100);

    }

            if (currentHeartrate <= 39 and currentHeartrate >= 0){

    

                  Wire.println("I Am Sick");

                }

              //  delay(100);

          if (currentHeartrate<= 79 and currentHeartrate >= 70){

    

                  Wire.println("Night Mare");

                }

              //  delay(100);

            if (currentHeartrate <= 69 and currentHeartrate >= 40){

    

                  Wire.println("kid Is At Sleep");

          }

              //delay(100);

              if (currentHeartrate <= 99 and currentHeartrate >= 80){

    

                  Wire.println("Kid Is Resting");

            }

                //delay(100);

                if (currentHeartrate <= 119 and currentHeartrate >= 100){

    

                  Wire.println("Kid Is Playing");

              }

 

                  if(currentHeartrate > 120){

      

                    Wire.println(" The Kid Is Having ");

                    //lcd.setCursor(0,1);

                    //lcd.println(" A Heart Attack");

                }

 

    Wire.endTransmission();    // stop transmitting*/

 

 

  Wire.beginTransmission(4); // transmit to device #4

    byte a;

  if ( GPS.available() > 0 ) // if there is data coming from the GPS shield

  {

    a = GPS.read(); // get the byte of data

    if(shield.encode(a)) // if there is valid GPS data...

    {

      getgps(shield); // then grab the data and display it on the LCD

    }

  float latitude, longitude;

      // Then call this function

      shield.f_get_position(&latitude, &longitude);

 

      Wire.println("Lat: ");

      Wire.println(latitude,5);

      Wire.println("  ");

      Wire.println("Long: ");

      Wire.println(longitude,5);

      Wire.println(" ");

 

  }

  Wire.endTransmission();    // stop transmitting

 

Wire.beginTransmission(4); // transmit to device #4

char key = keypad.getKey();  //This calls the keypad its self

 

 

  if (key) {

    Wire.println(key);      //This will print which ever key is pressed

    }

// int phrase;

  //int loca=0;

  //{

  // for(i =1; i < 4; i++)

// {

  //SayPhrase(i);

  //delay(1000);                  // Wait 1 secounds

// }

 

 

switch (key)              // Switching the keypad numbers to a message

      {

 

      case '1':      //This calls keypad number 1

      // lcd.clear();  //This clears previous message on the screen

      //lcd.setCursor(0,1);  //This set the cursor on line 1 on the LCD screen

      Wire.println("I AM Sick");    //This will display the message

 

      break;        //Ends witch for PRESSED

 

      case '2':      //This calls keypad number 2

      //lcd.clear();    //This clears previous message on the screen

      //lcd.setCursor(0,1);    ////This set the cursor on line 1 on the LCD screen

      Wire.println("I Want Food");  //This will display the message

 

      break;        //Ends witch for PRESSED

 

      case '3':      //This calls keypad number 3

      //lcd.clear();    //This clears previous message on the screen

      //lcd.setCursor(0,1);  //This set the cursor on line 1 on the LCD screen

      Wire.println("I Am Cold");  //This will display the message

 

      break;        //Ends witch for PRESSED

 

      case '4':  //This calls keypad number 4

      //lcd.clear();  //This clears previous message on the screen

      //lcd.setCursor(0,1);    //This set the cursor on line 1 on the LCD screen

      Wire.println("RECCA");  //This will display the message

      break;        //Ends witch for PRESSED

 

      case '5':  ////This calls keypad number 5

      //lcd.clear();    //This clears previous message on the screen

      //lcd.setCursor(0,1);  //This set the cursor on line 1 on the LCD screen

      Wire.println("REVON");  //This will display the message

      break;        //Ends witch for PRESSED

 

      case '6':  ////This calls keypad number 6

      //lcd.clear();      ////This clears previous message on the screen

      //lcd.setCursor(0,1);  //This set the cursor on line 1 on the LCD screen

      Wire.println("JEAN PAUL");  //This will display the message

      break;        //Ends witch for PRESSED

 

      case '7':  ////This calls keypad number 7

      //lcd.clear();  //This clears previous message on the screen

      //lcd.setCursor(0,1);  ////This set the cursor on line 1 on the LCD screen

      Wire.println("MONIA");    //This will display the message

      break;        //Ends witch for PRESSED

 

      case '8':  ////This calls keypad number 8

      //lcd.clear();    //This clears previous message on the screen

      //lcd.setCursor(0,1);  //This set the cursor on line 1 on the LCD screen

      Wire.println("DREAD HAIR");  //This will display the message

      break;        //Ends witch for PRESSED

 

 

  }

 

 

 

}

 

 

  Wire.endTransmission();    // stop transmitting

 

 

 

delay(2000);

}

  }

 

 

receiver code

 

//Reciever

#include<SPI.h>

#include <Wire.h>

#include <LiquidCrystal.h>

#include<VoiceShield.h>

LiquidCrystal lcd(30,31,32,33,34,35);

//#include <Keypad.h>

int key;

const byte ROWS = 4; //four rows

const byte COLS = 3; //three columns

/*char keys[ROWS][COLS] = {

        {'1','2','3'},

        {'4','5','6'},

        {'7','8','9'},

        {'*','0','#'}

        };

byte rowPins[ROWS] = {5, 4, 3, 2}; //connect to the row pinouts of the keypad

//byte rowPins[ROWS] = {38, 39, 40, 41}; //connect to the row pinouts of the keypad

byte colPins[COLS] = {8, 7, 6}; //connect to the column pinouts of the keypad

//byte colPins[COLS] = {42, 43, 44}; //connect to the column pinouts of the keypad

 

 

Keypad keypad = Keypad( makeKeymap(keys), rowPins, colPins, ROWS, COLS );*/

byte ledPin = 13;

VoiceShield vs(80);              // Create a instance of the Voice Shield called "vs" with 80 sound slots

 

 

int i = 1;

int Sentence[16];

int Phs1[] = {

   33, 78, 72, 255};     // "I am cold"

int Phs2[] = {

   33, 78, 16};            // "I am sick"      

int Phs3[] = {

    33, 44, 69};        // "I want food" 

void setup()

{

  Wire.begin(4);                // join i2c bus with address #4

  Wire.onReceive(receiveEvent); // register event

  Serial.begin(9600);           // start serial for output

    lcd.begin(16,2);

}

 

 

void loop()

{//char key = keypad.getKey();   //This calls the keypad its self

 

 

  if (key) {

    Wire.println(key);      //This will print which ever key is pressed

    }

int phrase;    

  int loca=0;

  {

   for(i =1; i < 4; i++)

  {

  //SayPhrase(i);

// delay(1000);                   // Wait 1 secounds

  }

 

 

switch (key)               // Switching the keypad numbers to a message

      {

      

       case '1':      //This calls keypad number 1

      // lcd.clear();   //This clears previous message on the screen

       //lcd.setCursor(0,1);  //This set the cursor on line 1 on the LCD screen

      // Wire.println("I AM Sick");    //This will display the message

       for(loca =0; loca < (sizeof(Phs2)/sizeof(int)); loca++)

    {

      Sentence[loca] = Phs2[loca];

    }

       break;        //Ends witch for PRESSED

      

       case '2':      //This calls keypad number 2

       //lcd.clear();     //This clears previous message on the screen

       //lcd.setCursor(0,1);    ////This set the cursor on line 1 on the LCD screen

       //Wire.println("I Want Food");   //This will display the message

        for(loca =0; loca < (sizeof(Phs3)/sizeof(int)); loca++)

    {

      Sentence[loca] = Phs3[loca];

    }

       break;        //Ends witch for PRESSED

      

       case '3':       //This calls keypad number 3

       //lcd.clear();     //This clears previous message on the screen

       //lcd.setCursor(0,1);  //This set the cursor on line 1 on the LCD screen

       //Wire.println("I Am Cold");   //This will display the message

        for(loca =0; loca < (sizeof(Phs1)/sizeof(int)); loca++)

        {

          Sentence[loca] = Phs1[loca];

        }

       break;        //Ends witch for PRESSED

      

     //  case '4':   //This calls keypad number 4

       //lcd.clear();   //This clears previous message on the screen

       //lcd.setCursor(0,1);    //This set the cursor on line 1 on the LCD screen

     //  Wire.println("RECCA");   //This will display the message

     //  break;        //Ends witch for PRESSED

      

      // case '5':   ////This calls keypad number 5

       //lcd.clear();    //This clears previous message on the screen

       //lcd.setCursor(0,1);  //This set the cursor on line 1 on the LCD screen

     //  Wire.println("REVON");  //This will display the message

     //  break;        //Ends witch for PRESSED

  

      // case '6':  ////This calls keypad number 6

       //lcd.clear();      ////This clears previous message on the screen

       //lcd.setCursor(0,1);  //This set the cursor on line 1 on the LCD screen

    //   Wire.println("JEAN PAUL");   //This will display the message

    //   break;         //Ends witch for PRESSED

      

     //  case '7':   ////This calls keypad number 7

       //lcd.clear();   //This clears previous message on the screen

       //lcd.setCursor(0,1);  ////This set the cursor on line 1 on the LCD screen

    //   Wire.println("MONIA");    //This will display the message

     //  break;        //Ends witch for PRESSED

      

     //  case '8':   ////This calls keypad number 8

       //lcd.clear();    //This clears previous message on the screen

       //lcd.setCursor(0,1);  //This set the cursor on line 1 on the LCD screen

    //   Wire.println("DREAD HAIR");   //This will display the message

     //  break;         //Ends witch for PRESSED

      

         default:

    Sentence[0] = 255;

  }

  for(loca=0; loca < 15; loca = loca +1)

  {

    if(Sentence[loca] == 255)

    {

      loca = 15;

    }

    else

    {

        vs.ISDPLAY_to_EOM(Sentence[loca]);

      }

}

 

 

}

 

 

// Wire.endTransmission();    // stop transmitting

 

 

  // when characters arrive over the serial port...

    if (Serial.available()) {

      // wait a bit for the entire message to arrive

      delay(100);

      // clear the screen

      lcd.clear();

      // read all the available characters

      while (Serial.available() > 0) {

        // display each character to the LCD

        lcd.write(Serial.read());

      }

delay(20);

}

}

 

 

void receiveEvent(int howMany)

{

  while(1 < Wire.available()) // loop through all but the last

  {

    char c = Wire.read(); // receive byte as a character

    //Serial.print(c);         // print the character

    lcd.setCursor(1,0);

     lcd.print(c);

  }

int x = Wire.read();    // receive byte as an integer

//Serial.print(x);

lcd.setCursor(0,1);

lcd.print(x);

}

 

 

 

pls i would really appreciate any help.

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 10 years ago

    This needs hardware to figure out. But if I was to attack this, I would build one function at a time and test it. adding next one and then test it. smaller the step the easier to fix.

    Clem
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.