I've recently been working with home automation stuff using Arduino and Raspberry Pi. I only got into electronics just a few months ago and I need some help on this design I'm working on. The idea is to be able to remotely trigger lights that are already hooked up to a wall switch, I'd like to still be able to use the switch though as well. I created a schematic in Fritzing as it is the most user friendly software I know of, there is also a visual diagram and a PCB layout. To be able to control the arduino wirelessly I use the HopeRFM69HW module, I didn't include this in the layout because it is not important and not what this is really about. The circuit works (at least in theory) by triggering a relay using an Arduino Pro Mini, when tripped the 110V flows through the relay and into the light. Hopefully some of you can give me some pointers on whether or not this will work and if it does not how I could fix it. Thanks!
I've included several PDF's all named accordingly to what they are, keep in mind on the PCB with components file things like the button and light would not actually be mounted on the board but attached with wires leading off the board.