Arduino Forum Arduino serial moniter
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 392 subscribers
  • Views 378 views
  • Users 0 members are here
Related

Arduino serial moniter

gabyhass
gabyhass over 10 years ago

Im trying to build a button martix keyboard (need help with that) and I decided to go my own way and make it use the arduinos serial moniter to detect if a certain row and column was pulled high or low and have a pre assigned value like if i press this button it detects and says oh! thats an f and displays it in the serial moniter

 

-Thanks,Gabriel wells

  • Sign in to reply
  • Cancel
Parents
  • gabyhass
    0 gabyhass over 10 years ago

    well good news is i figured out how to make it and make it work i have 2 buttons wired right now pushing one gives a 1 and pushing other gives 5 or 2 or whatever i want them to be,

    layout:

    row 1 "1"

    row 2  "2"

    now i want to make it so if i press 1 i get the arduino to print in serial moniter something like Serial.println("wrong")

    and pressing 2 will give "right" i will of course change this later but its a starting point

    code:

    #include <Keypad.h>

     

     

     

     

     

    char keys[2][1]={

    {'1'},

    {'5'}};

     

     

     

     

     

     

    byte rowPin[2]={5,8};

    byte colPin[1]={6};

     

    Keypad keypad=Keypad(makeKeymap(keys),rowPin,colPin,2,1);

     

    void setup()

    {

    Serial.begin(9600);

    }

     

    void loop()

    {

    char pressed=keypad.getKey();

    if(pressed)

    {

       Serial.println(pressed);

    }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gabyhass
    0 gabyhass over 10 years ago

    well good news is i figured out how to make it and make it work i have 2 buttons wired right now pushing one gives a 1 and pushing other gives 5 or 2 or whatever i want them to be,

    layout:

    row 1 "1"

    row 2  "2"

    now i want to make it so if i press 1 i get the arduino to print in serial moniter something like Serial.println("wrong")

    and pressing 2 will give "right" i will of course change this later but its a starting point

    code:

    #include <Keypad.h>

     

     

     

     

     

    char keys[2][1]={

    {'1'},

    {'5'}};

     

     

     

     

     

     

    byte rowPin[2]={5,8};

    byte colPin[1]={6};

     

    Keypad keypad=Keypad(makeKeymap(keys),rowPin,colPin,2,1);

     

    void setup()

    {

    Serial.begin(9600);

    }

     

    void loop()

    {

    char pressed=keypad.getKey();

    if(pressed)

    {

       Serial.println(pressed);

    }

    }