Arduino Forum Help with 3v dc motor
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
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 393 subscribers
  • Views 1137 views
  • Users 0 members are here
Related

Help with 3v dc motor

Former Member
Former Member over 10 years ago

Hi, I have been attempting to get a 3v DC motor to work with my ardiuno with no luck. Im pretty new to arduino so its probably something stupid simple im missing. I have tried other tutorials on the inter-webs to see if maybe the book i was using had something wrong in it.

http://exploringarduino.com/wp-content/uploads/2013/05/549360-c04f003callouts-copy-150x150.jpg

The link above is the diagram provided by the book.

http://exploringarduino.com/content/ch4/

This link is the online material of the book im using.

arduino 3v dc motor setup - Album on Imgur

This link is of what i have done.

code is below.

-----------------------------------------------------------

const int motor = 9;

void setup() {

pinMode(motor, OUTPUT);

}

 

void loop() {

  for(int i = 0; i < 256; i++){

  analogWrite(motor, i);

  delay(10);

  }

  delay(2000);

  for(int i = 255; i>=0; i--){

   analogWrite(motor, i);

  delay(10);

  }

delay (2000);

}

---------------------------------------------------

 

Alright so everything i have tried so far is switching both the transistor (pn2222a) and the diode around in case i had them the wrong way and that is not the case.

I have measured the output of the transistor thinking that maybe it a was a faulty part and i get ~7 volts which i feel seems high. the transistor also gets really hot to the touch. If i put the multimeter up to any other part(diode, capacitor. motor) I get no volts. If I hook the motor directly to the ground then the motor will run at full speed.

Im pretty lost on what else to do any help will be greatly appreciated if you need better pictures or for me to test something just ask. Thank you in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • ipv1
    ipv1 over 10 years ago +3
    Hello Nathan, I think you might have damaged the 2n2222 in your case which is why there are issues. I have a few recommendations for you to try out if you could. 1. Replace the 2n2222 with a new one and…
  • jw0752
    jw0752 over 10 years ago +1 suggested
    Hi Nathan, I have made this circuit when I went through Jeremy's book so the circuit design is correct. One thing to check is to make sure that you have identified the leads of the 2N2222 correctly. Here…
  • Anonymous-237891
    Anonymous-237891 over 10 years ago in reply to Former Member +1
    Hi, I think you may have fried your transistor. Since your circuit seems right to me I would suggest to do the simple led check. You need: One 1K resistor on the gate which goes to Vcc One led and a 330R…
Parents
  • clem57
    0 clem57 over 10 years ago

    If the transistor is hot, you are over driving it and it will pop at some point. Check voltage requirements on data sheet.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    If the transistor is hot, you are over driving it and it will pop at some point. Check voltage requirements on data sheet.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer