Arduino Forum Arduino with LabView and flex sensors
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
  • State Not Answered
  • Replies 2 replies
  • Subscribers 402 subscribers
  • Views 723 views
  • Users 0 members are here
  • hand;
  • sensors
  • arduino;
  • robot
  • flex
  • labview;
Related

Arduino with LabView and flex sensors

Former Member
Former Member over 10 years ago

Hello, first time in this forum.

I am having problems with Arduino Mega which is connected to a pc with LabView from which i control the board in real time. I also connected some flex sensors. The idea is to control robot hand and fingers with my own hand and fingers. I have written the code in labview and it kind of work but it is very unstable and slow. In the code I wanted to map the voltage changes from flex sensors and get the changes in degrees so the servos can understand it. I could map it properly because the flex sensors are hooked up with a voltage divider and the values i get are between 2.5 and 1.9 volts approximately. So i just put 9 points with limitations for voltage (ex. from 2.15 to 2.2 equals to 160 degrees and when i get values in that range the servo goes to 160 degree).  I know that I could map this using arduino coding because of the libraries for servos but can someone help me map it in  LabView or maybe suggest a better way to do it. And also i have to figure out a way to move the rest of the hand i 3 dimensions. I am thinking of 3d accelerometer but maybe there is a better way?

Thank you

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 10 years ago

    If you need a fast sampling rate for a close loop system you should do all of the processing on an Arduino board and just use Labview as a graphical interface for supervisory control. Why? because the interaction from PC to Mega is much slower than a real time can handle. The PC may get lost handling other tasks too. Just my two cents worth

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago

    Hello dear friend. You solve the problem with maping? I have same problem with same project..... how i can transform value analogic from sensor in degree of rotation for servo? image