Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino USB powering Arduino and 3.3v device
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 19 replies
  • Subscribers 421 subscribers
  • Views 2287 views
  • Users 0 members are here
  • arduino
Related

Arduino USB powering Arduino and 3.3v device

alexbee13
alexbee13 over 11 years ago

Hi. Im a newbie when it comes to this stuff but i recently bought an arduino and i was wondering if i could use the arduino cable and splice into it and connect the arduino using standard 5v then add a zener diode on another wire attatched to the 5v wire. Can i do this? I need a 3.3v power source and 5v for the arduino without using 2 usb cables. I know its probably the bad way of doing it. Im just curious to see if i can do it. Its the arduino uno.

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 11 years ago in reply to alexbee13 +1
    No worries. I have annotated your drawing with my suggested approach. Forget about anything within the greyed out box area and consider adding the two wires I have added in:
  • screamingtiger
    screamingtiger over 11 years ago +1
    One thing being left out, the device you are powering. How much current will it draw? The 3.3 output o the arduino is rated for 50ma. If you need more I can see why you want to use the USB. I don't recommend…
  • clem57
    0 clem57 over 11 years ago in reply to alexbee13

    A fly back diode would be a safe bet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alexbee13
    0 alexbee13 over 11 years ago in reply to clem57

    whats a flyback diode? ive never heard of one or seen one before.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to alexbee13

    http://en.wikipedia.org/wiki/Flyback_diode

    Google is your friend.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to alexbee13

    That is the name of the function the diode does in

    wont i need any diode on the 3.3v on the one to the RF module to prevent the current going back into the 3.3v line? the RF module is bi-directional or something

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alexbee13
    0 alexbee13 over 11 years ago in reply to gadget.iom

    so what type of flyback diode would i need or is there only 1 type?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • pettitda
    0 pettitda over 11 years ago in reply to alexbee13

    If the USB is the only source of power in your circuit then there won't be any reverse current on the 3.3V line from the Arduino to the Xbox 360 RF board.  In the original circuit, the guy was using two diodes to drop the 5V to near 3.3V (3.6V assuming 0.7V drop across each diode).

     

    However, as Robert Peter Oakes said, you'll most likely need to convert the 5V I/O voltage to 3.3V using one of the methods he listed. That is assuming that the Xbox 360 RF board is using 3.3V logic and not regulating down to 2.5V or 1.8V, etc..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alexbee13
    0 alexbee13 over 11 years ago in reply to pettitda

    so even though the RF module can sent the flow of current back to the arduino, its not going to damage it?. the reason for the diodes is to bring it to 3.3v but also to prevent the voltage drop that would burn out the RF module and the USB controller.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • chrisdracko
    0 chrisdracko over 11 years ago

    if you only need power for the zener diode and rf modular why not connect it to a standalone power suppy?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • screamingtiger
    0 screamingtiger over 11 years ago

    One thing being left out, the device you are powering.  How much current will it draw?  The 3.3 output o the arduino is rated for 50ma.  If you need more I can see why you want to use the USB.

     

    I don't recommend splicing into a USB cable, they aren't very easy to work with, all the shielding, the tiny wires etc.  The approach suggested is the best IF you are within the current tolerances of the 3.3V output of the Arduino.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<