Arduino Forum Circuit Issue with MOSFET
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
  • State Verified Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 405 subscribers
  • Views 2686 views
  • Users 0 members are here
  • irf540
  • 2N7000
  • arduino
Related

Circuit Issue with MOSFET

wallarug
wallarug over 10 years ago

Hey,

 

I am having issues with this circuit:

 

image

 

Background:  This circuit is to control an RGB LED strip (so three of the above would achieve this).  The reason for this particular design is: IRF540 to drive load (large current) and the two 2N7000 drive the MOSFET, reducing current drain from Controller (possibly a 3v3 Arduino).  The double 2N7000 allows the IRF540 to be active when logic high.

 

Can someone please tell me if there is a problem with the above schematic, otherwise I think it would be my breadboard layout is not correct. (too hard to post that right now).

 

Any comments would be much appreciated.

 

Many thanks,

 

wallarug

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 10 years ago +2
    How is it (mis)behaving? Just some ideas: 1. In general, don't hook up your actual output device until you're sure the circuits controlling it work with a voltmeter. Put a resistor in place of the LED…
  • wallarug
    wallarug over 10 years ago in reply to johnbeetem +1
    Thanks John, I will take everything above into consideration.
  • mcb1
    mcb1 over 10 years ago +1
    @wallarug I'm having feeling of dejavue with a similar circuit some time back to do a similar task. The first FET is right on the limit for conducting, so you could reduce the resistor to 1k or similar…
Parents
  • johnbeetem
    0 johnbeetem over 10 years ago

    How is it (mis)behaving?

     

    Just some ideas:

     

    1.  In general, don't hook up your actual output device until you're sure the circuits controlling it work with a voltmeter.  Put a resistor in place of the LED strip to see if the transistors are switching properly.

     

    2.  Are the transistors switching properly?  What voltages are you seeing at the transistor drains for each control input voltage?

     

    3.  I saw from the 2N7000 spec sheet that it has a typical gate threshold voltage of 2.1 V, though it could go as high as 3V.  You might have trouble controlling it from a 3.3V Arduino.  You might want to replace it with an NFET with a lower gate threshold or use a good old 2N2222 bipolar NPN transistor.

     

    4.  You haven't biased the first transistor's gate, so when you first turn on power the transistor may or may not switch on, depending on what's driving it and whether that driver is floating.  You may want to have a pull-down resistor so it's guaranteed off when you first power up.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wallarug
    0 wallarug over 10 years ago in reply to johnbeetem

    Thanks John,

     

    I will take everything above into consideration.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • wallarug
    0 wallarug over 10 years ago in reply to johnbeetem

    Thanks John,

     

    I will take everything above into consideration.