Arduino Forum Atmega328P-PU (arduino uno) from breadboard to pcb
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
  • State Not Answered
  • Replies 22 replies
  • Subscribers 397 subscribers
  • Views 1886 views
  • Users 0 members are here
  • atmega328
  • arduino
Related

Atmega328P-PU (arduino uno) from breadboard to pcb

bobj6
bobj6 over 10 years ago

Hello everybody.

 

I been working with an arduino uno for a few years now and i decide to make them standalone.

So i bought some Atmega328P-PU and start putting them on a breadboard with a Crystal and a few capacitors

I have loaded the BLINK example onto my Atmega chip and this works fine, The led blinks with an interval of aproximilly a 1/2 second.

 

Now this works i have solderd one onto a PCB.

I used a Voltage regulator (L7805ABV) to make 5 volts out of 12 volts.

the Atmega does get power and ground and the Crystal is also correct installed.

But when i start it up the led on pin 13 doesn't light up.

When I touch the plastic of the Atmega chip the led does ligt up, But flashes way to fast (Not the 1/2 a second it should).

 

does anyone have an idea what is going wrong here?

I thank you in advance.

 

Yours sincerly,

Bob

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago +3
    It sounds like a couple of things; probably a floating reset pin (that would explain why a finger near it makes a difference) and also probably the config reg fuse values have an incorrect prescaler value…
  • bobj6
    bobj6 over 10 years ago in reply to clem57 +2
    I am using ic sockets so i dont solder with the chip on the board.
  • kidiccurus
    kidiccurus over 10 years ago +2
    I have been doing this recently and have had an issue with a dead crystal after a short. The chip didn't work at all in my board but was fine in the original arduino. I'm waiting for some replacements…
Parents
  • deepankarmaithani
    0 deepankarmaithani over 10 years ago

    Did you get a solution? After reading all the comments i think all the possibilities are covered, one thing that once i face was that i connected the crystal too far from the chip and my controller dint worked well. Hope u dont have done this too. Also sometimes dry soldering is the culprit. I had this problem at times by viewing it might seem that the connection is perfect but actually sometimes when the temperature of solder is not correctly set the connection is just not good enough . try heating your soldered points. A good soldering should have shiny surface and not dull surface

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • deepankarmaithani
    0 deepankarmaithani over 10 years ago

    Did you get a solution? After reading all the comments i think all the possibilities are covered, one thing that once i face was that i connected the crystal too far from the chip and my controller dint worked well. Hope u dont have done this too. Also sometimes dry soldering is the culprit. I had this problem at times by viewing it might seem that the connection is perfect but actually sometimes when the temperature of solder is not correctly set the connection is just not good enough . try heating your soldered points. A good soldering should have shiny surface and not dull surface