Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Sending serial data from Arduino to Android via Bluetooth - NOT ANSWERED Yet
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 23 replies
  • Answers 7 answers
  • Subscribers 420 subscribers
  • Views 8027 views
  • Users 0 members are here
  • bluetooth
  • arduino
Related

Sending serial data from Arduino to Android via Bluetooth - NOT ANSWERED Yet

e14 Contributor
e14 Contributor over 11 years ago

Hi all,

 

I've been working on my Arduino project for quite a while now, managed to process the incoming data in the Arduino and display it on LCD (data is coming from a simulation on the laptop). But I cannot manage to view this data on my Android App (used MIT App Inventor) via Bluetooth (HC-06). I have managed to do this but after a week I tested it again and found some errors (I think problem was with my hardware) therefore (silly me) I didnt save the sketch, therefore blocks in MIT App Inventor are 100% working.

 

Also, I am connecting RX pin of Bluetooth through a voltage divider with pin 7.  Any ideas pls?

 

Arduino sketch:

 

#include <SoftwareSerial.h>

#include <LiquidCrystal.h>

 

byte myByte; // Storing the incoming data from serial port

int txPin = 7;

int rxPin =6;

 

lcd(12,11,5,4,3,2) //pin of lcd   ****I know this is not the exact command

SoftwareSerial BlueToothConnect(txPin, rxPin);

 

pinMode(rxPin, INPUT);

pinMode(txPin, OUTPUT);

 

void setup(){

lcd.begin(16,2);

Serial.begin(9600);  //Serial communication

 

}

void loop(){

if(Serial.available(){

lcd.clear();

while(Serial.available()>0){       //Until data is being found in Serial, turn on serial on Bluetooth

BlueToothConnect.begin(9600);

myByte = Serial.read(); //reading the myByte data

lcd.write(myByte);  //showing data on LCD

Serial.write(myByte) ; //Showing data on serial monitor

 

txPin = digitalWrite(myByte);   //writing myByte content on pin 7 (txPin)

BlueToothConnect.write(txPin);   //  BlueToothConnect.print(txPin);  //displaying content of txPin to be view on Android display

 

}

 

Message was edited by: Lor B

  • Sign in to reply
  • Cancel

Top Replies

  • neilk
    neilk over 11 years ago in reply to e14 Contributor +2 verified
    Hi lorrainebarbara I've never used SoftwareSerial successfully, although I've been trying to recently to reprogram an HC05 (Master/Slave Bluetooth). This requires the use of SoftWare serial ad so far I…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to neilk +2 suggested
    Hi neilk , Thank you so much I have managed to incorporate (and change) some of the program you ve published, worked Here is my whole sketch. Thanks alot for your help!! //Sending data serially to Android…
  • gadget.iom
    gadget.iom over 8 years ago in reply to happyforever +2 suggested
    Are you trying to send sensor values or text typed into the serial monitor? All of the other references to bluetooth.print are commented out. Try putting: bluetooth.print("Sending Init String"); // Test…
Parents
  • happyforever
    0 happyforever over 8 years ago

    I can receive data from android but cant send data to android, please help me to solve. The below is my code.

    #include <SoftwareSerial.h>

     

     

    int bluetoothTx = 13;  // TX-O pin of bluetooth mate, Arduino D2

    int bluetoothRx = 14;  // RX-I pin of bluetooth mate, Arduino D3

     

     

    char incomingByte; // incoming data

    int sensorPin = A0;   

    int ledPin = 11;      // select the pin for the LED

    int ledPin2 = 12;

    int sensorValue = 0;  // variable to store the value coming from the sensor

    int rTrigPin = 6;

    int rEchoPin = 7;

    int trigPin = 9;

    int echoPin = 10;

    int lTrigPin = 4;

    int lEchoPin = 5;

     

     

    // defines variables

    long rDuration;

    int rDistance;

    long duration;

    int distance;

    long lDuration;

    int lDistance;

     

     

     

     

    SoftwareSerial bluetooth(bluetoothTx, bluetoothRx);

     

     

    void setup() {

     

     

      Serial.begin(115200);

     

      bluetooth.begin(115200);  // The Bluetooth Mate defaults to 115200bps

      //bluetooth.print("$");  // Print three times individually

      //bluetooth.print("$");

      //bluetooth.print("$");  // Enter command mode

      //delay(100);  // Short delay, wait for the Mate to send back CMD

      //bluetooth.println("U,9600,N");  // Temporarily Change the baudrate to 9600, no parity

      // 115200 can be too fast at times for NewSoftSerial to relay the data reliably

      bluetooth.begin(9600);  // Start bluetooth serial at 9600

     

      pinMode(rTrigPin, OUTPUT); // Sets the rTrigPin as an Output

      pinMode(rEchoPin, INPUT); // Sets the rEchoPin as an Input

      pinMode(trigPin, OUTPUT); // Sets the trigPin as an Output

      pinMode(echoPin, INPUT); // Sets the echoPin as an Input

      pinMode(lTrigPin, OUTPUT); // Sets the lTrigPin as an Output

      pinMode(lEchoPin, INPUT); // Sets the lEchoPin as an Input

     

     

      // declare the ledPin as an OUTPUT:

      pinMode(ledPin, OUTPUT);

      pinMode(ledPin2, OUTPUT);

     

     

    }

     

    /*void loop() {

      // read the value from the sensor:

      sensorValue = analogRead(sensorPin);

      // turn the ledPin on

      digitalWrite(ledPin, LOW);

      // stop the program for <sensorValue> milliseconds:

      delay(sensorValue);

      // turn the ledPin off:

      digitalWrite(ledPin, HIGH);

      // stop the program for for <sensorValue> milliseconds:

      delay(sensorValue);

      }*/

     

     

    void loop()

    {   

            digitalWrite(rTrigPin, LOW);

            delayMicroseconds(2);

            digitalWrite(rTrigPin, HIGH);

            delayMicroseconds(10);

            digitalWrite(rTrigPin, LOW);

            rDuration = pulseIn(rEchoPin, HIGH);

            rDistance = (rDuration / 2) / 29.1;

         

            digitalWrite(trigPin, LOW);

            delayMicroseconds(2);

            digitalWrite(trigPin, HIGH);

            delayMicroseconds(10);

            digitalWrite(trigPin, LOW);

            duration = pulseIn(echoPin, HIGH);

            distance = (duration / 2) / 29.1;

         

            digitalWrite(lTrigPin, LOW);

            delayMicroseconds(2);

            digitalWrite(lTrigPin, HIGH);

            delayMicroseconds(10);

            digitalWrite(lTrigPin, LOW);

            lDuration = pulseIn(lEchoPin, HIGH);

            lDistance = (lDuration / 2) / 29.1;

         

            sensorValue = analogRead(sensorPin); 

     

     

              if (rDistance <= 221 || distance <= 221 || lDistance <= 221)

            {

              if (sensorValue <= 140)

              {

                digitalWrite(ledPin, LOW);

                digitalWrite(ledPin2, LOW);

              }

              else

              {

                digitalWrite(ledPin, HIGH);

                digitalWrite(ledPin2, HIGH);

              }

               

            }

            else if (rDistance > 221 || distance > 221 || lDistance > 221)

            {

              if (sensorValue <= 140)

              {

                digitalWrite(ledPin, LOW);

                digitalWrite(ledPin2, LOW);

              }

              else

              {

                digitalWrite(ledPin, HIGH);

                digitalWrite(ledPin2, HIGH);

              }

            }

     

      if (bluetooth.available()) // If the bluetooth sent any characters

      {

        // Send any characters the bluetooth prints to the serial monitor

       

        Serial.println((char)bluetooth.read());

        incomingByte = bluetooth.read();

     

     

       

        if(incomingByte == '1') { 

     

     

             Serial.println("Music is pause and now you are in dangerous situation.");  // print message

             //bluetooth.print("1");

            

             //delay(1000);

        }

     

     

     

        if(incomingByte == '0') {

         

              digitalWrite(ledPin, HIGH);

              digitalWrite(ledPin2, HIGH);

              Serial.println("Alert signal OFF and music would not pause when in dangerous situation.");  // print message

              //bluetooth.print("0");

              //delay(1000);

              //break;

             

        }

      }

     

     

      if (Serial.available()>0) // If stuff was typed in the serial monitor

      {

        int bytes=Serial.available();

        //Serial.readBytes(buffer, startPosition, bytes);

     

        bluetooth.print((char)Serial.read());

       

      }

     

     

     

    }









    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • happyforever
    0 happyforever over 8 years ago

    I can receive data from android but cant send data to android, please help me to solve. The below is my code.

    #include <SoftwareSerial.h>

     

     

    int bluetoothTx = 13;  // TX-O pin of bluetooth mate, Arduino D2

    int bluetoothRx = 14;  // RX-I pin of bluetooth mate, Arduino D3

     

     

    char incomingByte; // incoming data

    int sensorPin = A0;   

    int ledPin = 11;      // select the pin for the LED

    int ledPin2 = 12;

    int sensorValue = 0;  // variable to store the value coming from the sensor

    int rTrigPin = 6;

    int rEchoPin = 7;

    int trigPin = 9;

    int echoPin = 10;

    int lTrigPin = 4;

    int lEchoPin = 5;

     

     

    // defines variables

    long rDuration;

    int rDistance;

    long duration;

    int distance;

    long lDuration;

    int lDistance;

     

     

     

     

    SoftwareSerial bluetooth(bluetoothTx, bluetoothRx);

     

     

    void setup() {

     

     

      Serial.begin(115200);

     

      bluetooth.begin(115200);  // The Bluetooth Mate defaults to 115200bps

      //bluetooth.print("$");  // Print three times individually

      //bluetooth.print("$");

      //bluetooth.print("$");  // Enter command mode

      //delay(100);  // Short delay, wait for the Mate to send back CMD

      //bluetooth.println("U,9600,N");  // Temporarily Change the baudrate to 9600, no parity

      // 115200 can be too fast at times for NewSoftSerial to relay the data reliably

      bluetooth.begin(9600);  // Start bluetooth serial at 9600

     

      pinMode(rTrigPin, OUTPUT); // Sets the rTrigPin as an Output

      pinMode(rEchoPin, INPUT); // Sets the rEchoPin as an Input

      pinMode(trigPin, OUTPUT); // Sets the trigPin as an Output

      pinMode(echoPin, INPUT); // Sets the echoPin as an Input

      pinMode(lTrigPin, OUTPUT); // Sets the lTrigPin as an Output

      pinMode(lEchoPin, INPUT); // Sets the lEchoPin as an Input

     

     

      // declare the ledPin as an OUTPUT:

      pinMode(ledPin, OUTPUT);

      pinMode(ledPin2, OUTPUT);

     

     

    }

     

    /*void loop() {

      // read the value from the sensor:

      sensorValue = analogRead(sensorPin);

      // turn the ledPin on

      digitalWrite(ledPin, LOW);

      // stop the program for <sensorValue> milliseconds:

      delay(sensorValue);

      // turn the ledPin off:

      digitalWrite(ledPin, HIGH);

      // stop the program for for <sensorValue> milliseconds:

      delay(sensorValue);

      }*/

     

     

    void loop()

    {   

            digitalWrite(rTrigPin, LOW);

            delayMicroseconds(2);

            digitalWrite(rTrigPin, HIGH);

            delayMicroseconds(10);

            digitalWrite(rTrigPin, LOW);

            rDuration = pulseIn(rEchoPin, HIGH);

            rDistance = (rDuration / 2) / 29.1;

         

            digitalWrite(trigPin, LOW);

            delayMicroseconds(2);

            digitalWrite(trigPin, HIGH);

            delayMicroseconds(10);

            digitalWrite(trigPin, LOW);

            duration = pulseIn(echoPin, HIGH);

            distance = (duration / 2) / 29.1;

         

            digitalWrite(lTrigPin, LOW);

            delayMicroseconds(2);

            digitalWrite(lTrigPin, HIGH);

            delayMicroseconds(10);

            digitalWrite(lTrigPin, LOW);

            lDuration = pulseIn(lEchoPin, HIGH);

            lDistance = (lDuration / 2) / 29.1;

         

            sensorValue = analogRead(sensorPin); 

     

     

              if (rDistance <= 221 || distance <= 221 || lDistance <= 221)

            {

              if (sensorValue <= 140)

              {

                digitalWrite(ledPin, LOW);

                digitalWrite(ledPin2, LOW);

              }

              else

              {

                digitalWrite(ledPin, HIGH);

                digitalWrite(ledPin2, HIGH);

              }

               

            }

            else if (rDistance > 221 || distance > 221 || lDistance > 221)

            {

              if (sensorValue <= 140)

              {

                digitalWrite(ledPin, LOW);

                digitalWrite(ledPin2, LOW);

              }

              else

              {

                digitalWrite(ledPin, HIGH);

                digitalWrite(ledPin2, HIGH);

              }

            }

     

      if (bluetooth.available()) // If the bluetooth sent any characters

      {

        // Send any characters the bluetooth prints to the serial monitor

       

        Serial.println((char)bluetooth.read());

        incomingByte = bluetooth.read();

     

     

       

        if(incomingByte == '1') { 

     

     

             Serial.println("Music is pause and now you are in dangerous situation.");  // print message

             //bluetooth.print("1");

            

             //delay(1000);

        }

     

     

     

        if(incomingByte == '0') {

         

              digitalWrite(ledPin, HIGH);

              digitalWrite(ledPin2, HIGH);

              Serial.println("Alert signal OFF and music would not pause when in dangerous situation.");  // print message

              //bluetooth.print("0");

              //delay(1000);

              //break;

             

        }

      }

     

     

      if (Serial.available()>0) // If stuff was typed in the serial monitor

      {

        int bytes=Serial.available();

        //Serial.readBytes(buffer, startPosition, bytes);

     

        bluetooth.print((char)Serial.read());

       

      }

     

     

     

    }









    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • gadget.iom
    0 gadget.iom over 8 years ago in reply to happyforever

    Are you trying to send sensor values or text typed into the serial monitor?

    All of the other references to bluetooth.print are commented out.

     

    Try putting:

    bluetooth.print("Sending Init String"); // Test bluetooth TX

    after the line:

    bluetooth.begin(9600);  // Start bluetooth serial at 9600

    and see if you get any output when you reset the Arduino.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • neilk
    0 neilk over 8 years ago in reply to happyforever

    Hi happyforever I have replied to you as well, but at the other location. I was already composing my reply there when mcb1 replied here.

     

    Neil

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • happyforever
    0 happyforever over 8 years ago in reply to gadget.iom

    Thanks for reply my answer, but i try add the [ bluetooth.print("Sending Init String"); ] but the error still there. Besides that, serial monitor also do not display this message.

    Is because android part got problem? Below is my android code(MainActivity.java)

     

    package com.example.helloworld.ninjatechsmartheadphone;

    import java.io.IOException;
    import java.io.InputStream;
    import java.io.OutputStream;
    import java.lang.reflect.Method;
    import java.util.UUID;

    import android.support.v7.app.AppCompatActivity;
    import android.bluetooth.BluetoothAdapter;
    import android.bluetooth.BluetoothDevice;
    import android.bluetooth.BluetoothSocket;
    import android.content.Intent;
    import android.os.Bundle;
    import android.os.Handler;
    import android.util.Log;
    import android.view.View;
    import android.view.View.OnClickListener;
    import android.widget.Button;
    import android.widget.TextView;
    import android.media.MediaPlayer;
    import android.widget.Toast;


    public class MainActivity extends AppCompatActivity {

       private static final String TAG = "bluetooth";

       Button on;
       Button off;
       Button button;
       TextView txtArduino;
       Handler h;

      final int RECIEVE_MESSAGE = 1;  // Status for Handler
       private BluetoothAdapter btAdapter = null;
      private BluetoothSocket btSocket = null;
      private StringBuilder sb = new StringBuilder();

      private ConnectedThread mConnectedThread;

       // SPP UUID service
       private static final UUID MY_UUID = UUID.fromString("00001101-0000-1000-8000-00805F9B34FB");


      private static String address = "98:D3:31:FD:21:00";

       @Override
       public void onCreate(Bundle savedInstanceState) {

       super.onCreate(savedInstanceState);

       setContentView(R.layout.activity_main);

      final MediaPlayer catSoundMediaPlayer = MediaPlayer.create(this, R.raw.afi);

       button = (Button) findViewById(R.id.play);
       on = (Button) findViewById(R.id.on);
       off = (Button) findViewById(R.id.off);
       txtArduino = (TextView) findViewById(R.id.txtArduino);  // for display the received data from the Arduino

       h = new Handler() {

       public void handleMessage(android.os.Message msg) {

      Log.d("msg", "msg.what is " + msg.what);
      switch (msg.what) {

       case RECIEVE_MESSAGE:  // if receive massage
       byte[] readBuf = (byte[]) msg.obj;
       Toast.makeText(getBaseContext(), "I want try try try", Toast.LENGTH_SHORT).show();
       String strIncom = new String(readBuf, 0, msg.arg1);  // create string from bytes array
       sb.append(strIncom);  // append string
       int endOfLineIndex = sb.indexOf("\r\n");  // determine the end-of-line
       if (endOfLineIndex > 0) {  // if end-of-line,
       String sbprint = sb.substring(0, endOfLineIndex);  // extract string
       sb.delete(0, sb.length());  // and clear
       txtArduino.setText("Data from Arduino: " + sbprint);  // update TextView
      //off.setEnabled(true);
      // on.setEnabled(true);
       }

      Log.d(TAG, "...String:"+ sb.toString() +  "Byte:" + msg.arg1 + "...");
      break;

      default:

      Toast.makeText(getBaseContext(), "I want try", Toast.LENGTH_LONG).show();
       Log.d(TAG, "...String:"+ sb.toString() +  "Byte:" + msg.arg1 + "...");
       }

      }

     

       ;
       };

       btAdapter = BluetoothAdapter.getDefaultAdapter();  // get Bluetooth adapter
       checkBTState();

       button.setOnClickListener(new OnClickListener() {

       public void onClick(View v) {

     

       catSoundMediaPlayer.start();

       //Intent intent = new Intent("android.intent.action.MUSIC_PLAYER");
      //intent.addFlags(Intent.FLAG_ACTIVITY_NEW_TASK);
      //startActivity(intent);
       }

      });

       on.setOnClickListener(new OnClickListener() {

       public void onClick(View v) {

       //on.setEnabled(false);
       mConnectedThread.write("1");  // Send "1" via Bluetooth
       Toast.makeText(getBaseContext(), "Turn on Alert Signal", Toast.LENGTH_SHORT).show();
       }

      });

       off.setOnClickListener(new OnClickListener() {

       public void onClick(View v) {

       //off.setEnabled(false);
       mConnectedThread.write("0");  // Send "0" via Bluetooth
       Toast.makeText(getBaseContext(), "Turn off Alert Signal", Toast.LENGTH_SHORT).show();
       }

      });

       }

     

     

       private BluetoothSocket createBluetoothSocket(BluetoothDevice device) throws IOException {

     

       try {

       final Method m = device.getClass().getMethod("createInsecureRfcommSocketToServiceRecord", new Class[] { UUID.class });
      return (BluetoothSocket) m.invoke(device, MY_UUID);
       } catch (Exception e) {

      Log.e(TAG, "Could not create Insecure RFComm Connection",e);
       }

     

       return  device.createRfcommSocketToServiceRecord(MY_UUID);
       }

     

     

       @Override
       public void onResume() {

       super.onResume();

       Log.d(TAG, "...onResume - try connect...");

       // Set up a pointer to the remote node using it's address.
       BluetoothDevice device = btAdapter.getRemoteDevice(address);

       // Two things are needed to make a connection:
      // A MAC address, which we got above.
      // A Service ID or UUID. In this case we are using the
      // UUID for SPP.

       try {

       btSocket = createBluetoothSocket(device);
       } catch (IOException e) {

      errorExit("Fatal Error", "In onResume() and socket create failed: " + e.getMessage() + ".");
       }

     

       // Discovery is resource intensive. Make sure it isn't going on
      // when you attempt to connect and pass your message.
       btAdapter.cancelDiscovery();

       // Establish the connection. This will block until it connects.
       Log.d(TAG, "...Connecting...");
      try {

       btSocket.connect();
       Log.d(TAG, "....Connection ok...");
       Toast.makeText(getBaseContext(), "Connected", Toast.LENGTH_SHORT).show();
       } catch (IOException e) {

       try {

       //Log.d(TAG, "....111...");
      //Toast.makeText(getBaseContext(), "1", Toast.LENGTH_SHORT).show();
       btSocket.close();
       } catch (IOException e2) {

      errorExit("Fatal Error", "In onResume() and unable to close socket during connection failure" + e2.getMessage() + ".");
       //Toast.makeText(getBaseContext(), "2", Toast.LENGTH_SHORT).show();
       }

      }

     

       // Create a data stream so we can talk to server.
       Log.d(TAG, "...Create Socket...");

       mConnectedThread = new ConnectedThread(btSocket);
       mConnectedThread.start();
       }

     

       @Override
       public void onPause() {

       super.onPause();

       Log.d(TAG, "...In onPause()...");

      try  {

       btSocket.close();
       } catch (IOException e2) {

      errorExit("Fatal Error", "In onPause() and failed to close socket." + e2.getMessage() + ".");
       }

      }

     

       private void checkBTState() {

       // Check for Bluetooth support and then check to make sure it is turned on
      // Emulator doesn't support Bluetooth and will return null
       if(btAdapter==null) {

      errorExit("Fatal Error", "Bluetooth not support");
       } else {

       if (btAdapter.isEnabled()) {

      Log.d(TAG, "...Bluetooth ON...");
       } else {

       //Prompt user to turn on Bluetooth
       Intent enableBtIntent = new Intent(BluetoothAdapter.ACTION_REQUEST_ENABLE);
       startActivityForResult(enableBtIntent, 1);
       }

      }

      }

     

       private void errorExit(String title, String message){

      Toast.makeText(getBaseContext(), title + " - " + message, Toast.LENGTH_LONG).show();
       finish();
       }

     

       private class ConnectedThread extends Thread {

       private final InputStream mmInStream;
      private final OutputStream mmOutStream;

      public ConnectedThread(BluetoothSocket socket) {

      InputStream tmpIn = null;
       OutputStream tmpOut = null;

       // Get the input and output streams, using temp objects because
      // member streams are final
       try {

      tmpIn = socket.getInputStream();
       tmpOut = socket.getOutputStream();
       } catch (IOException e) { }

     

       mmInStream = tmpIn;
       mmOutStream = tmpOut;
       }

     

       public void run() {

       byte[] buffer = new byte[256];  // buffer store for the stream
       int bytes; // bytes returned from read()
      //Toast.makeText(getBaseContext(), "qqqqqqq", Toast.LENGTH_SHORT).show();

      // Keep listening to the InputStream until an exception occurs
       while (true) {

       try {

       // Read from the InputStream
       bytes = mmInStream.read(buffer);  // Get number of bytes and message in "buffer"
       h.obtainMessage(RECIEVE_MESSAGE, bytes, -1, buffer).sendToTarget();  // Send to message queue Handler
       Toast.makeText(getBaseContext(), "q111q", Toast.LENGTH_SHORT).show();
       } catch (IOException e) {

       //Toast.makeText(getBaseContext(), "qq222qq", Toast.LENGTH_SHORT).show();
       break;
       }

      }

      }

     

       /* Call this from the main activity to send data to the remote device */
       public void write(String message) {

      Log.d(TAG, "...Data to send: " + message + "...");
      byte[] msgBuffer = message.getBytes();
      try {

       mmOutStream.write(msgBuffer);
       } catch (IOException e) {

      Log.d(TAG, "...Error data send: " + e.getMessage() + "...");
       }

      }

      }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • happyforever
    0 happyforever over 8 years ago in reply to neilk

    Hi Neil, can you help me check my android code got any problem? I think maybe is android part cause this error.

     

    Below is my android code(MainActivity.java)

     

    package com.example.helloworld.ninjatechsmartheadphone;

    import java.io.IOException;
    import java.io.InputStream;
    import java.io.OutputStream;
    import java.lang.reflect.Method;
    import java.util.UUID;

    import android.support.v7.app.AppCompatActivity;
    import android.bluetooth.BluetoothAdapter;
    import android.bluetooth.BluetoothDevice;
    import android.bluetooth.BluetoothSocket;
    import android.content.Intent;
    import android.os.Bundle;
    import android.os.Handler;
    import android.util.Log;
    import android.view.View;
    import android.view.View.OnClickListener;
    import android.widget.Button;
    import android.widget.TextView;
    import android.media.MediaPlayer;
    import android.widget.Toast;


    public class MainActivity extends AppCompatActivity {

       private static final String TAG = "bluetooth";

       Button on;
       Button off;
       Button button;
       TextView txtArduino;
       Handler h;

      final int RECIEVE_MESSAGE = 1;  // Status for Handler
       private BluetoothAdapter btAdapter = null;
      private BluetoothSocket btSocket = null;
      private StringBuilder sb = new StringBuilder();

      private ConnectedThread mConnectedThread;

       // SPP UUID service
       private static final UUID MY_UUID = UUID.fromString("00001101-0000-1000-8000-00805F9B34FB");


      private static String address = "98:D3:31:FD:21:00";

       @Override
       public void onCreate(Bundle savedInstanceState) {

       super.onCreate(savedInstanceState);

       setContentView(R.layout.activity_main);

      final MediaPlayer catSoundMediaPlayer = MediaPlayer.create(this, R.raw.afi);

       button = (Button) findViewById(R.id.play);
       on = (Button) findViewById(R.id.on);
       off = (Button) findViewById(R.id.off);
       txtArduino = (TextView) findViewById(R.id.txtArduino);  // for display the received data from the Arduino

       h = new Handler() {

       public void handleMessage(android.os.Message msg) {

      Log.d("msg", "msg.what is " + msg.what);
      switch (msg.what) {

       case RECIEVE_MESSAGE:  // if receive massage
       byte[] readBuf = (byte[]) msg.obj;
       Toast.makeText(getBaseContext(), "I want try try try", Toast.LENGTH_SHORT).show();
       String strIncom = new String(readBuf, 0, msg.arg1);  // create string from bytes array
       sb.append(strIncom);  // append string
       int endOfLineIndex = sb.indexOf("\r\n");  // determine the end-of-line
       if (endOfLineIndex > 0) {  // if end-of-line,
       String sbprint = sb.substring(0, endOfLineIndex);  // extract string
       sb.delete(0, sb.length());  // and clear
       txtArduino.setText("Data from Arduino: " + sbprint);  // update TextView
      //off.setEnabled(true);
      // on.setEnabled(true);
       }

      Log.d(TAG, "...String:"+ sb.toString() +  "Byte:" + msg.arg1 + "...");
      break;

      default:

      Toast.makeText(getBaseContext(), "I want try", Toast.LENGTH_LONG).show();
       Log.d(TAG, "...String:"+ sb.toString() +  "Byte:" + msg.arg1 + "...");
       }

      }

     

       ;
       };

       btAdapter = BluetoothAdapter.getDefaultAdapter();  // get Bluetooth adapter
       checkBTState();

       button.setOnClickListener(new OnClickListener() {

       public void onClick(View v) {

     

       catSoundMediaPlayer.start();

       //Intent intent = new Intent("android.intent.action.MUSIC_PLAYER");
      //intent.addFlags(Intent.FLAG_ACTIVITY_NEW_TASK);
      //startActivity(intent);
       }

      });

       on.setOnClickListener(new OnClickListener() {

       public void onClick(View v) {

       //on.setEnabled(false);
       mConnectedThread.write("1");  // Send "1" via Bluetooth
       Toast.makeText(getBaseContext(), "Turn on Alert Signal", Toast.LENGTH_SHORT).show();
       }

      });

       off.setOnClickListener(new OnClickListener() {

       public void onClick(View v) {

       //off.setEnabled(false);
       mConnectedThread.write("0");  // Send "0" via Bluetooth
       Toast.makeText(getBaseContext(), "Turn off Alert Signal", Toast.LENGTH_SHORT).show();
       }

      });

       }

     

     

       private BluetoothSocket createBluetoothSocket(BluetoothDevice device) throws IOException {

     

       try {

       final Method m = device.getClass().getMethod("createInsecureRfcommSocketToServiceRecord", new Class[] { UUID.class });
      return (BluetoothSocket) m.invoke(device, MY_UUID);
       } catch (Exception e) {

      Log.e(TAG, "Could not create Insecure RFComm Connection",e);
       }

     

       return  device.createRfcommSocketToServiceRecord(MY_UUID);
       }

     

     

       @Override
       public void onResume() {

       super.onResume();

       Log.d(TAG, "...onResume - try connect...");

       // Set up a pointer to the remote node using it's address.
       BluetoothDevice device = btAdapter.getRemoteDevice(address);

       // Two things are needed to make a connection:
      // A MAC address, which we got above.
      // A Service ID or UUID. In this case we are using the
      // UUID for SPP.

       try {

       btSocket = createBluetoothSocket(device);
       } catch (IOException e) {

      errorExit("Fatal Error", "In onResume() and socket create failed: " + e.getMessage() + ".");
       }

     

       // Discovery is resource intensive. Make sure it isn't going on
      // when you attempt to connect and pass your message.
       btAdapter.cancelDiscovery();

       // Establish the connection. This will block until it connects.
       Log.d(TAG, "...Connecting...");
      try {

       btSocket.connect();
       Log.d(TAG, "....Connection ok...");
       Toast.makeText(getBaseContext(), "Connected", Toast.LENGTH_SHORT).show();
       } catch (IOException e) {

       try {

       //Log.d(TAG, "....111...");
      //Toast.makeText(getBaseContext(), "1", Toast.LENGTH_SHORT).show();
       btSocket.close();
       } catch (IOException e2) {

      errorExit("Fatal Error", "In onResume() and unable to close socket during connection failure" + e2.getMessage() + ".");
       //Toast.makeText(getBaseContext(), "2", Toast.LENGTH_SHORT).show();
       }

      }

     

       // Create a data stream so we can talk to server.
       Log.d(TAG, "...Create Socket...");

       mConnectedThread = new ConnectedThread(btSocket);
       mConnectedThread.start();
       }

     

       @Override
       public void onPause() {

       super.onPause();

       Log.d(TAG, "...In onPause()...");

      try  {

       btSocket.close();
       } catch (IOException e2) {

      errorExit("Fatal Error", "In onPause() and failed to close socket." + e2.getMessage() + ".");
       }

      }

     

       private void checkBTState() {

       // Check for Bluetooth support and then check to make sure it is turned on
      // Emulator doesn't support Bluetooth and will return null
       if(btAdapter==null) {

      errorExit("Fatal Error", "Bluetooth not support");
       } else {

       if (btAdapter.isEnabled()) {

      Log.d(TAG, "...Bluetooth ON...");
       } else {

       //Prompt user to turn on Bluetooth
       Intent enableBtIntent = new Intent(BluetoothAdapter.ACTION_REQUEST_ENABLE);
       startActivityForResult(enableBtIntent, 1);
       }

      }

      }

     

       private void errorExit(String title, String message){

      Toast.makeText(getBaseContext(), title + " - " + message, Toast.LENGTH_LONG).show();
       finish();
       }

     

       private class ConnectedThread extends Thread {

       private final InputStream mmInStream;
      private final OutputStream mmOutStream;

      public ConnectedThread(BluetoothSocket socket) {

      InputStream tmpIn = null;
       OutputStream tmpOut = null;

       // Get the input and output streams, using temp objects because
      // member streams are final
       try {

      tmpIn = socket.getInputStream();
       tmpOut = socket.getOutputStream();
       } catch (IOException e) { }

     

       mmInStream = tmpIn;
       mmOutStream = tmpOut;
       }

     

       public void run() {

       byte[] buffer = new byte[256];  // buffer store for the stream
       int bytes; // bytes returned from read()
      //Toast.makeText(getBaseContext(), "qqqqqqq", Toast.LENGTH_SHORT).show();

      // Keep listening to the InputStream until an exception occurs
       while (true) {

       try {

       // Read from the InputStream
       bytes = mmInStream.read(buffer);  // Get number of bytes and message in "buffer"
       h.obtainMessage(RECIEVE_MESSAGE, bytes, -1, buffer).sendToTarget();  // Send to message queue Handler
       Toast.makeText(getBaseContext(), "q111q", Toast.LENGTH_SHORT).show();
       } catch (IOException e) {

       //Toast.makeText(getBaseContext(), "qq222qq", Toast.LENGTH_SHORT).show();
       break;
       }

      }

      }

     

       /* Call this from the main activity to send data to the remote device */
       public void write(String message) {

      Log.d(TAG, "...Data to send: " + message + "...");
      byte[] msgBuffer = message.getBytes();
      try {

       mmOutStream.write(msgBuffer);
       } catch (IOException e) {

      Log.d(TAG, "...Error data send: " + e.getMessage() + "...");
       }

      }

      }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • happyforever
    0 happyforever over 8 years ago in reply to happyforever

    I had debug the android code, found that the I cant run into the switch case. Can anyone help me to correct it? Thanks

     

       h = new Handler() {

       public void handleMessage(android.os.Message msg) {

      Log.d("msg", "msg.what is " + msg.what);
      switch (msg.what) {

       case RECIEVE_MESSAGE:  // if receive massage
       byte[] readBuf = (byte[]) msg.obj;
       Toast.makeText(getBaseContext(), "I want try try try", Toast.LENGTH_SHORT).show();
       String strIncom = new String(readBuf, 0, msg.arg1);  // create string from bytes array
       sb.append(strIncom);  // append string
       int endOfLineIndex = sb.indexOf("\r\n");  // determine the end-of-line
       if (endOfLineIndex > 0) {  // if end-of-line,
       String sbprint = sb.substring(0, endOfLineIndex);  // extract string
       sb.delete(0, sb.length());  // and clear
       txtArduino.setText("Data from Arduino: " + sbprint);  // update TextView
      //off.setEnabled(true);
      // on.setEnabled(true);
       }

      Log.d(TAG, "...String:"+ sb.toString() +  "Byte:" + msg.arg1 + "...");
      break;

      default:

      Toast.makeText(getBaseContext(), "I want try", Toast.LENGTH_LONG).show();
       Log.d(TAG, "...String:"+ sb.toString() +  "Byte:" + msg.arg1 + "...");
       }

      }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • neilk
    0 neilk over 8 years ago in reply to happyforever

    Sorry - I develop my android Apps at a much higher level using MIT Appinventor