Arduino Forum How to Build RC Hovercraft!
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
  • State Not Answered
  • Replies 5 replies
  • Subscribers 393 subscribers
  • Views 558 views
  • Users 0 members are here
  • arduino
Related

How to Build RC Hovercraft!

Former Member
Former Member over 10 years ago

Dear All ,

I'm a Precision Engineering Student from Myanmar. I've to built a RC hovercraft for my university project.

But,I'm just a beginner for Electronic field.

I don't trouble for designing cover frame of hovercraft,but start difficulties in building Control System for this.

First , I don't know which radio Transmitter & Receiver use for this?

And then , I don't know how to connect this selected Control System to the motors that used in the hovercraft.

But before that, I had a little experience of Arduino , and so I hope if I use Arduino for Control System , I'll be OK.

So, I wanna request your advice for starting this project.

 

Thanks ...

  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 10 years ago +1
    Hello, I think that the best thing you should do before is to post for us more detailed information on the mechanic and construction of the system. The number of channels of the RC controller, for example…
  • clem57
    clem57 over 10 years ago +1
    A radio transmitter/receiver to control your motors, doesn't matter which transmitter you use . Just choose a frequency allowed in your country. For testing the motors, you first have to solder an electric…
Parents
  • clem57
    0 clem57 over 10 years ago

    imageA radio transmitter/receiver to control your motors, doesn't matter which transmitter you use. Just choose a frequency allowed in your country.


    For testing the motors, you first have to solder an electric circuit to connect the battery to the ESC's and motors.

    - Use the gold connectors for connections between ESC and motor, and between ESC and thick black/red wire. Cover the connectors with heat shrink to avoid them from touching other connectors.

    - The three-colored cable from the servo can be plugged directly into your receiver. (the servo runs on the receiver-battery. LiPo)

    - The three-colored cable from the ESC's can also be plugged directly into your receiver, but...

    image! Do not plug the red/power (probably the ones in the middle) wires from these cables into your receiver. The ESC's are already being powered by your LiPo-battery. Just fold the red wires back and cover them with heat shrink or tape.


    imageI used Arduino to control the motors with a potmeter, I've also controlled this hovercraft with a PlayStation3 controller.

    imageThese are suggestions since I do not know the motor you choose. Follow these with your mind engaged since I make no warranties here.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    imageA radio transmitter/receiver to control your motors, doesn't matter which transmitter you use. Just choose a frequency allowed in your country.


    For testing the motors, you first have to solder an electric circuit to connect the battery to the ESC's and motors.

    - Use the gold connectors for connections between ESC and motor, and between ESC and thick black/red wire. Cover the connectors with heat shrink to avoid them from touching other connectors.

    - The three-colored cable from the servo can be plugged directly into your receiver. (the servo runs on the receiver-battery. LiPo)

    - The three-colored cable from the ESC's can also be plugged directly into your receiver, but...

    image! Do not plug the red/power (probably the ones in the middle) wires from these cables into your receiver. The ESC's are already being powered by your LiPo-battery. Just fold the red wires back and cover them with heat shrink or tape.


    imageI used Arduino to control the motors with a potmeter, I've also controlled this hovercraft with a PlayStation3 controller.

    imageThese are suggestions since I do not know the motor you choose. Follow these with your mind engaged since I make no warranties here.

    Clem