I bought this relay system and it doesn't work
http://www.ebay.com/itm/231573073495?_trksid=p2057872.m2749.l2649&ssPageName=STRK%3AMEBIDX%3AIT
Its a 12V relay system so I have to use 12V into the VCC and the input pins are driven by 5V. So I connect 5V in, the relays trip. The code is simple, digital high and low with a 1 second delay. Pins are output.
The little LEDS turn off and on as expected but the relays do not trip. I don't have a load on them but should not matter. If I use 12V as required into the VCC, the leds only turn on, then go dimmer, never off.
I have a common ground between the arduino and relay board as well.
What is going on?
I went ahead and 2nd day aired a 5v version, I will just run it off the same regulator as the arduino. Anybody have any experience with these?