Arduino Forum MINI DVD ROM CNC
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
  • State Not Answered
  • Replies 0 replies
  • Subscribers 389 subscribers
  • Views 196 views
  • Users 0 members are here
Related

MINI DVD ROM CNC

Former Member
Former Member over 10 years ago

Hello, I have built all the hardware: physical structure, and have completed in entering the GRBLtoArduino and all the software. I have used the Universal GCodeSender and has successfully interpreted the software for is says " Grbl 0.8c ['$' for help] ". I've soldered the stepper motors (for I'm using steppers from dvd roms) to some salvages wire from a printer I took apart. I installed some female sockets in order to connect to the male pins on the CNC Shield ver. 2.01 . The orange light from the arduino flashes and in the Universal GCodeSender ver. 0.8 completes the operation b/c is says " ok " . I have no idea whats wrong. I know the steppers work b/c ive used a 9v battery to pulse the motors and they do indeed pulse. Ive used a multimeter to check its resistance and it works. I've checked the current on the motors once connected to the cnc shield and there's current. I have tested if the drivers are in fact getting power and they are. I've attempted the code " x=100 " , " $7=225 " but no motor movement.  Can ANYONE help me ?