Arduino Forum Arduino - Sink more than 6 volts
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
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 405 subscribers
  • Views 430 views
  • Users 0 members are here
  • arduino
Related

Arduino - Sink more than 6 volts

Former Member
Former Member over 10 years ago

Hi everyone,

 

I need to sink an active low line in a system to ground using an Arduino, the problem is that it's more than what the Arduino's pins can handle around 6v. I tried finding out if a mosfet would actually connect Drain to Source and drive the line low (ground) and just drive the gate with the arduino, but I couldn't find anything, or at least didn't understand it.

 

Thanks for any help! image

 

Regards

 

Theoneil

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1 suggested
    The goto IC for that kind of thing the low cost, available everywhere ULN2003 http://www.ti.com/lit/ds/symlink/uln2003a.pdf up to 50V and upto 1000mA peak, 500mA typical, you can combine pins if you need…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    The goto IC for that kind of thing

     

    the low cost, available everywhere ULN2003

     

    http://www.ti.com/lit/ds/symlink/uln2003a.pdf

     

    up to 50V and upto 1000mA peak, 500mA typical, you can combine pins if you need more

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    The goto IC for that kind of thing

     

    the low cost, available everywhere ULN2003

     

    http://www.ti.com/lit/ds/symlink/uln2003a.pdf

     

    up to 50V and upto 1000mA peak, 500mA typical, you can combine pins if you need more

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to Robert Peter Oakes

    Agree Peter, and if he needs to manage more power can user the ULN2004 instead of ULN2003 that us up to 3A. I used it for 2.3 motors and worked fine without problems. The chips only need a heat dissipator.