Arduino
  • Products
  • More
Arduino
Arduino Forum USART Trigger not working
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 407 subscribers
  • Views 1623 views
  • Users 0 members are here
  • usart
  • avr
  • trigger
  • atmega328
Related

USART Trigger not working

icongdo
icongdo over 10 years ago

I've been trying to debug this program. I am using an ATmega328p My USART trigger isn't getting called? Maybe I'm missing something?

Hardware using PuTTY to send message or simply echo 1> COM1

 

 

#include <avr/io.h>

#include <avr/interrupt.h>

#include <util/setbaud.h>

 

 

#ifndef BAUD                         

#define BAUD  9600                    

#endif

 

 

int main(void) {

 

  DDRB = 0x1;

 

 

  UCSR0B = (1 << TXEN0) | (1 << RXEN0) | ( 1 << RXCIE0 );

  UCSR0C = (1 << UCSZ01) | (1 << UCSZ00); 

 

 

  UBRR0H = UBRRH_VALUE;                      

  UBRR0L = UBRRL_VALUE;

 

  sei( );

          

  while (1) { }

  return (0);

}



 

ISR( USART_RX_vect ) {

  PORTB ^= 0x1;

}



  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to icongdo +1 verified
    OK, i did not look there so its good you have that covered one thought on the re-trigger is reading from the port in some way once the trigger has occured so that it will reset the trigger. without searching…
  • icongdo
    icongdo over 10 years ago in reply to Robert Peter Oakes +1
    Yes this is what I suspected. For future references. Writing directly to RCX0 flag will not stop the interrupt from reoccurring ADCSRA &= ~( 1 << RXC0 ); Taken from the data sheet: When interrupt-driven…
Parents
  • ipv1
    0 ipv1 over 10 years ago

    In order to test the UART, you should write a simple code to repeatedly send say a character after a fixed delay. Probe the TX pin on the Controller to see if the baudrate comes out right.

    That might help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ipv1
    0 ipv1 over 10 years ago

    In order to test the UART, you should write a simple code to repeatedly send say a character after a fixed delay. Probe the TX pin on the Controller to see if the baudrate comes out right.

    That might help.