Arduino Forum Deciding between Arduino UNO and Leonardo for interfacig an AFE with Serial.
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
  • State Suggested Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 403 subscribers
  • Views 604 views
  • Users 0 members are here
Related

Deciding between Arduino UNO and Leonardo for interfacig an AFE with Serial.

Former Member
Former Member over 10 years ago

Hello,

 

I have used Arduino in previous projects quite successfully. However, on this occasion, I would like to know the best way to interface an  Analogue Front End (AFE) with Arduino.

I want to have a LCD interface to a project which is meant to display internal register values of the AFE to the LCD. I want to use an Arduino to interface both of these.

 

The AFE is Cirrus Logic CS5490, which is an energy measurement IC. CS5490 has Tx/Rx interface to R/W internal registers.Must I wire the Tx/Rx of CS5490 with those of the Arduino (pin 0 and1 on UNO) or could they be connected to other Digital pins as well?

 

Should I use Arduino UNO (with one serial port) or Leonardo (2 UARTS). I have identified this as LCD shield on this website.

 

I will make a small PCB with CS5490.

Regards.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1 suggested
    your other choice culd be an Arduino MEGA, it has multiple serial ports and loads of RAM and FLASH A work of warning though, this is a MAINS power monitor, If you are not familuar with working on mains…
Parents
  • clem57
    0 clem57 over 10 years ago

    If you use other digital pins, you will need to use software to assemble the bits whereas the 0,1 are hardware based interrupts. The Uno shares the serial port with USB, so I would go with the Leonardo to use a non-shared port.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    If you use other digital pins, you will need to use software to assemble the bits whereas the 0,1 are hardware based interrupts. The Uno shares the serial port with USB, so I would go with the Leonardo to use a non-shared port.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer