Arduino Forum RFID 13.56 MHz / NFC Module for Arduino
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
  • Replies 3 replies
  • Subscribers 402 subscribers
  • Views 265 views
  • Users 0 members are here
Related

RFID 13.56 MHz / NFC Module for Arduino

ritamüller
ritamüller over 10 years ago

Hi,

Im in desperate need of some help for a project I am doing.

I have RFID 13.56 MHz / NFC Module for Arduino from Cooking Hacks (Cooking Hacks - RFID 13.56 MHz / NFC Module for Arduino)

and I try to reading tags according to the Programm in this website but I get the following error message in Arduino:


Der Sketch verwendet 3.772 Bytes (11%) des Programmspeicherplatzes. Das Maximum sind 32.256 Bytes.

Globale Variablen verwenden 481 Bytes (23%) des dynamischen Speichers, 1.567 Bytes für lokale Variablen verbleiben. Das Maximum sind 2.048 Bytes.

avrdude: stk500_getsync() attempt 1 of 10: not in sync: resp=0xff

avrdude: stk500_getsync() attempt 2 of 10: not in sync: resp=0x04

avrdude: stk500_getsync() attempt 3 of 10: not in sync: resp=0xfc

avrdude: stk500_getsync() attempt 4 of 10: not in sync: resp=0xf1

avrdude: stk500_getsync() attempt 5 of 10: not in sync: resp=0x04

avrdude: stk500_getsync() attempt 6 of 10: not in sync: resp=0xfc

avrdude: stk500_getsync() attempt 7 of 10: not in sync: resp=0xc4

avrdude: stk500_getsync() attempt 8 of 10: not in sync: resp=0x82

avrdude: stk500_getsync() attempt 9 of 10: not in sync: resp=0x18

avrdude: stk500_getsync() attempt 10 of 10: not in sync: resp=0x00

 

can someone help me ?

 

Thx

 

Rita

  • Sign in to reply
  • Cancel
Parents
  • clem57
    clem57 over 10 years ago

    Do you get anything like this. It would help if you print yours here to see where the errors are coming from.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • clem57
    clem57 over 10 years ago

    Do you get anything like this. It would help if you print yours here to see where the errors are coming from.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ritamüller
    ritamüller over 10 years ago in reply to clem57

    Thanks Martin I got the window and everything it's ok but I have not understood the progrmm !!
    is this program for one block ? because there are 64 blocks on an RFID card how can I read the other blocks ?

     

     

    Thx

     

     

    Rita