Arduino Forum RFID read / write Blocks
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
  • Replies 2 replies
  • Subscribers 389 subscribers
  • Views 443 views
  • Users 0 members are here
Related

RFID read / write Blocks

ritamüller
ritamüller over 10 years ago

Hallo,

I have RFID 13.56 MHz / NFC Module for Arduino from Cooking Hacks (Cooking Hacks - RFID 13.56 MHz / NFC Module for Arduino) .
I tried to read / write one block und i get this Error !

 

can someone help me ?

 

 

Error :

sketch_jun01a.ino:70:2: error: expected unqualified-id before 'if'

Fehler beim Kompilieren.

 

 

  *************************************************************************************

 

The Program:

 

/*
*  RFID/NFC Modul for Arduino.
*  one block read / write
*/

uint8_t dataRX[35];//Receive buffer
uint8_t dataTX[35];//Transmit buffer
uint8_t _UID[4]; // stores the UID (unique identifier) of a card
uint8_t blockData[] = {0x00,0x01,0x02,0x03,0x04,0x05,0x06,0x07,
    0x08,0x09,0x0A,0x0B,0x0C,0x0D,0x0E,0x0F};//Data to write (16 bytes)
uint8_t keyAccess[] = {0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF} ;// stores the key or password
uint8_t address = 0x04;//Address to read
uint8_t ATQ[2];//Answer to request
uint8_t state;//state of the process
uint8_t aux[16];//Auxiliar buffer

void setup()
{
//Start serial port 115200 bps:
Serial.begin(115200);
delay(100);
Serial.print("RFID/NFC @ 13.56 MHz module started");
delay(1000);

//! It is needed to launch a simple command to sycnchronize
getFirmware();
configureSAM();
}
void loop()
{
Serial.print("\n");
Serial.println("Ready to read...");
/////////////////////////////////////////////////////////////
//Get the Card Identifier
init(_UID, ATQ);
Serial.print("\n");
Serial.print( "The Card NUID : ");
print(_UID , 4);
/////////////////////////////////////////////////////////////
//Auntenticate a block with his keyAccess
state = authenticate(_UID, address, keyAccess);
Serial.print("\n");

if ( state == 0) {
  Serial.println("Authentication block OK");
} else {
  Serial.println("Authentication failed");
}
        /////////////////////////////////////////////////////////////
//Read from address after authentication
state = readData(address, aux);
Serial.print("\n");

if (state == 0) {
  Serial.println("Read block OK");
} else {
  Serial.println("Read failed");
}

Serial.print("\n");
Serial.print("Data readed : ");
print(aux , 16);
Serial.print("\n");
delay(2000);
}

         /////////////////////////////////////////////////////////////
//Write blockData in a address, after authentication.
if ( state == 0 ) {
  state = writeData(address, blockData);
  Serial.print("\n");
   if ( state == 0) {
    Serial.println("Write block OK");
   } else {
    Serial.println("Write failed");
   }
/////////////////////////////////////////////////////////////
//Read from address after authentication
  state = readData(address, aux);
  Serial.print("\n");

  if (state == 0) {
   Serial.println("Read block OK");
  } else {
   Serial.println("Read failed");
  }

  Serial.print("Data readed : ");
  print(aux , 16);
  Serial.print("\n");
}
   delay(2000);
}
//**********************************************************************
//!The goal of this command is to detect as many targets (maximum MaxTg)
// as possible in passive mode.
uint8_t init(uint8_t *UID , uint8_t *ATQ)   //! Request InListPassive
{
Serial.flush();

dataTX[0] = 0x04; // Length
lengthCheckSum(dataTX); // Length Checksum
dataTX[2] = 0xD4;
dataTX[3] = 0x4A; // Code
dataTX[4] = 0x01; //MaxTarget
dataTX[5] = 0x00; //BaudRate = 106Kbps
dataTX[6] = 0x00; // Clear checkSum position
checkSum(dataTX);

sendTX(dataTX , 7 ,23);

for (int i = 17; i < (21) ; i++){
  _UID[i-17] = dataRX[i];
  UID[i-17] = _UID[i-17];
}

ATQ[0] = dataRX[13];
ATQ[1] = dataRX[14];

if ((dataRX[9]== 0xD5) & (dataRX[10] == 0x4B) & (dataRX[11] == 0x01)) {
  return 0;
} else {
  return 1;
}
}
//**********************************************************************
//!A block must be authenticated before read and write operations
uint8_t authenticate(uint8_t *UID, uint8_t blockAddress, uint8_t *keyAccess)
{
dataTX[0] = 0x0F;
lengthCheckSum(dataTX);
dataTX[2] = 0xD4;
dataTX[3] = 0x40; // inDataEchange
dataTX[4] = 0x01; //Number of targets
dataTX[5] = 0x60; // Authentication code
dataTX[6] = blockAddress;

for (int i = 0; i < 6 ; i++) {
  dataTX[i + 7] = keyAccess[i];
}

dataTX[13] = UID[0];  dataTX[14] = UID[1];
dataTX[15] = UID[2];  dataTX[16] = UID[3];
dataTX[17] = 0x00;
checkSum(dataTX);
sendTX(dataTX , 18 ,14);

if ((dataRX[9]== 0xD5) & (dataRX[10] == 0x41) & (dataRX[11] == 0x00)) {
  return 0;
} else {
  return 1;
}
}
//**********************************************************************
//!Write 16 bytes in address .
uint8_t writeData(uint8_t address, uint8_t *blockData)  //!Writing
{
Serial.print("                ");
dataTX[0] = 0x15;
lengthCheckSum(dataTX); // Length Checksum
dataTX[2] = 0xD4;
dataTX[3] = 0x40;  //inDataEchange CODE
dataTX[4] = 0x01;  //Number of targets
dataTX[5] = 0xA0; //Write Command
dataTX[6] = address; //Address 

for (int i = 0; i < 16; i++) {
  dataTX[i+7] = blockData[i];
}

dataTX[23] = 0x00;
checkSum(dataTX);
sendTX(dataTX , 24 ,14);   

if ((dataRX[9]== 0xD5) & (dataRX[10] == 0x41) & (dataRX[11] == 0x00)) {
  return 0;
} else {
  return 1;
}
}
//**********************************************************************
//!Read 16 bytes from  address .
uint8_t readData(uint8_t address, uint8_t *readData) //!Reading
{
Serial.print("                "); 

dataTX[0] = 0x05;
lengthCheckSum(dataTX); // Length Checksum
dataTX[2] = 0xD4; // Code
dataTX[3] = 0x40; // Code
dataTX[4] = 0x01; // Number of targets
dataTX[5] = 0x30; //ReadCode
dataTX[6] = address;  //Read address
dataTX[7] = 0x00;
checkSum(dataTX);
sendTX(dataTX , 8, 30);
memset(readData, 0x00, 16);

if ((dataRX[9]== 0xD5) & (dataRX[10] == 0x41) & (dataRX[11] == 0x00)) {
  for (int i = 12; i < 28; i++) {
   readData[i-12] = dataRX[i];
  }
  return 0;
} else {
  return 1;
}
}
//**********************************************************************
//!The PN532 sends back the version of the embedded firmware.
bool getFirmware(void)  //! It is needed to launch a simple command to sycnchronize
{
Serial.print("                ");

memset(dataTX, 0x00, 35);
dataTX[0] = 0x02; // Length
lengthCheckSum(dataTX); // Length Checksum
dataTX[2] = 0xD4; // CODE
dataTX[3] = 0x02; //TFI
checkSum(dataTX); //0x2A; //Checksum 

sendTX(dataTX , 5 , 17);
Serial.print("\n");
Serial.print("Your Firmware version is : ");

for (int i = 11; i < (15) ; i++){
  Serial.print(dataRX[i], HEX);
  Serial.print(" ");
}
Serial.print("\n");
}

//**********************************************************************
//!Print data stored in vectors .
void print(uint8_t * _data, uint8_t length)
{
for (int i = 0; i < length ; i++){
  Serial.print(_data[i], HEX);
  Serial.print(" ");
}
Serial.print("\n");
}
//**********************************************************************
//!This command is used to set internal parameters of the PN532,
bool configureSAM(void)//! Configure the SAM
{
Serial.print("               ");

dataTX[0] = 0x05; //Length
lengthCheckSum(dataTX); // Length Checksum
dataTX[2] = 0xD4;
dataTX[3] = 0x14;
dataTX[4] = 0x01; //Normal mode
dataTX[5] = 0x14; // TimeOUT
dataTX[6] = 0x00; // IRQ
dataTX[7] = 0x00; // Clean checkSum position
checkSum(dataTX);

sendTX(dataTX , 8, 13);
}
//**********************************************************************
//!Send data stored in dataTX
void sendTX(uint8_t *dataTX, uint8_t length, uint8_t outLength)
{
Serial.print(char(0x00));
Serial.print(char(0x00));
Serial.print(char(0xFF));

for (int i = 0; i < length; i++) {
  Serial.print(char(dataTX[i]));
}

Serial.print(char(0x00));
getACK();
waitResponse();    // 1C - receive response
getData(outLength);
}
//**********************************************************************
//!Wait for ACK response and stores it in the dataRX buffer
void getACK(void)
{
delay(5);
waitResponse();
for (int i = 0; i < 5 ; i++) {
  dataRX[i] = Serial.read();
}
}
//**********************************************************************
//!Wait the response of the module
void waitResponse(void)
{
int val = 0xFF;
int cont = 0x00;
while(val != 0x00) {
  val = Serial.read();
  delay(5);
  cont ++;
}
}
//**********************************************************************
//!Get data from the module
void getData(uint8_t outLength)
{
for (int i=5; i < outLength; i++) {
  dataRX[i] = Serial.read(); // read data from the module.
}
}
//**********************************************************************
//!Calculates the checksum and stores it in dataTX buffer
void checkSum(uint8_t *dataTX)
{
for (int i = 0; i < dataTX[0] ; i++) {
  dataTX[dataTX[0] + 2] += dataTX[i + 2];
}
byte(dataTX[dataTX[0] + 2]= - dataTX[dataTX[0] + 2]);
}
//**********************************************************************
//!Calculates the length checksum and sotres it in the buffer.
uint8_t lengthCheckSum(uint8_t *dataTX)
{
dataTX[1] = byte(0x100 - dataTX[0]);
}

 

Thx

 

Rita

  • Sign in to reply
  • Cancel
Parents
  • gadget.iom
    gadget.iom over 10 years ago

    I managed to get the code to compile by removing the "}" at line 58.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gadget.iom
    gadget.iom over 10 years ago

    I managed to get the code to compile by removing the "}" at line 58.