Arduino Forum Read all blocks RFID card
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
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 403 subscribers
  • Views 1822 views
  • Users 0 members are here
Related

Read all blocks RFID card

ritamüller
ritamüller over 10 years ago

Hi,

I have RFID 13.56 MHz / NFC Module for Arduino from Cooking Hacks (Cooking Hacks - RFID 13.56 MHz / NFC Module for Arduino)

can I read all the blocks ? I tried but I get error, I just want to know if that's possible


/*
*  RFID/NFC module from Libelium for Arduino.
*  read all blocks in a RFID tag
*/


uint8_t dataRX[35];//Receive buffer.
uint8_t dataTX[35];//Transmit buffer.
uint8_t _UID[4];// stores the UID (unique identifier) of a card.
uint8_t keyAccess[] = {0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF } ;// stores the key or password.
uint8_t ATQ[2];//Answer to request
uint8_t state;//state of the process
uint8_t aux[16];//Auxiliar buffer.


void setup()
{
  //Start serial port 115200 bps:
  Serial.begin(115200);
  delay(100);
  Serial.print("RFID/NFC @ 13.56 MHz module started");
  delay(1000);
  //!It is needed to launch a simple command to sycnchronize
  getFirmware();
  configureSAM();
}


void loop()
{
  Serial.print("\n");
  Serial.println("Ready to read...");
  /////////////////////////////////////////////////////////////
  //Get the UID Identifier
  init(_UID, ATQ);
  Serial.print("\n");
  Serial.print( "The UID : ");
  print(_UID , 4);
   
      // we will do the same actions in blocks from 0 to 3 (which is sector 1)
      for (int n=0; n< 64; n++)
      {
      // **** authenticate the key A of each sector
      if (n % 4 == 0) // only one authentication per sector is needed
      {
        state = authenticate(_UID, n , keyAccess); // it is supposed all the blocks have the same key
        Serial.print("\r\nAuthentication block");
        Serial.print(n, DEC); // show the number of the block [n = 0..63 in a 1 kB RFID card]
        Serial.print(": ");
        Serial.print(state, HEX); // show the state of the executed authentication command
        //delay(1);
      }
      // **** if passed authentication in the sector, we will be able to read the data in its blocks
      Serial.read(n, aux);
      Serial.print("\r\nRead block ");
      Serial.print(n, DEC); // show the number of the block [n = 0..63]
      Serial.print(": ");
      Serial.print(state, HEX); // show the state of the executed read command
      Serial.print("  ");
   
      if (state == 0) // if the read command was successful, we show the data (16 bytes)
      {
        Serial.print(" | ");
        for (int i=0; i< 16; i++)
        {
          if (aux[i] <=  B01111)
          {
            Serial.print(" ");
          }
          Serial.print(aux[i], HEX); // print the 16 bytes of the block 'n'
          Serial.print(" ");
        }
        Serial.print("  ");
        if (n==0)
          Serial.print("<--UID(first 4 bytes)");
        else if (((n+1) % 4) == 0)
          Serial.print("<--Trailer block");
      }
    }
    Serial.println();
  }
  delay(2000); // wait 2 second in each loop
}
//**********************************************************************
//!The goal of this command is to detect as many targets (maximum MaxTg)
// as possible in passive mode.
uint8_t init(uint8_t *UID , uint8_t *ATQ)  //! Request InListPassive
{
  Serial.flush();


  dataTX[0] = 0x04; // Length
  lengthCheckSum(dataTX); // Length Checksum
  dataTX[2] = 0xD4;
  dataTX[3] = 0x4A; // Code
  dataTX[4] = 0x01; //MaxTarget
  dataTX[5] = 0x00; //BaudRate = 106Kbps
  dataTX[6] = 0x00; // Clear checkSum position
  checkSum(dataTX);


  sendTX(dataTX , 7 ,23);


  for (int i = 17; i < (21) ; i++){
  _UID[i-17] = dataRX[i];
  UID[i-17] = _UID[i-17];
  }


  ATQ[0] = dataRX[13];
  ATQ[1] = dataRX[14];


  if ((dataRX[9]== 0xD5) & (dataRX[10] == 0x4B) & (dataRX[11] == 0x01)) {
  return 0;
  } else {
  return 1;
  }
}
//**********************************************************************
//!A block must be authenticated before read and write operations
uint8_t authenticate(uint8_t *UID, uint8_t blockAddress, uint8_t *keyAccess)
{
  dataTX[0] = 0x0F;
  lengthCheckSum(dataTX);
  dataTX[2] = 0xD4;
  dataTX[3] = 0x40; // inDataEchange
  dataTX[4] = 0x01; //Number of targets
  dataTX[5] = 0x60; // Authentication code
  dataTX[6] = blockAddress;
  for (int i = 0; i < 6 ; i++) {
  dataTX[i + 7] = keyAccess[i];
  }
  dataTX[13] = UID[0];  dataTX[14] = UID[1];
  dataTX[15] = UID[2];  dataTX[16] = UID[3];
  dataTX[17] = 0x00;
  checkSum(dataTX);
  sendTX(dataTX , 18 ,14);


  if ((dataRX[9]== 0xD5) & (dataRX[10] == 0x41) & (dataRX[11] == 0x00)) {
  return 0;
  } else {
  return 1;
  }
}
//**********************************************************************
//!Write 16 bytes in address .
uint8_t writeData(uint8_t address, uint8_t *blockData)  //!Writing
{
  Serial.print("                ");
  dataTX[0] = 0x15;
  lengthCheckSum(dataTX); // Length Checksum
  dataTX[2] = 0xD4;
  dataTX[3] = 0x40;//inDataEchange CODE
  dataTX[4] = 0x01;//Number of targets
  dataTX[5] = 0xA0;//Write Command
  dataTX[6] = address; //Address


  for (int i = 0; i < 16; i++) {
  dataTX[i+7] = blockData[i];
  }


  dataTX[23] = 0x00;
  checkSum(dataTX);
  sendTX(dataTX , 24 ,14);


  if ((dataRX[9]== 0xD5) & (dataRX[10] == 0x41) & (dataRX[11] == 0x00)) {
  return 0;
  } else {
  return 1;
  }
}
//**********************************************************************
//!Read 16 bytes from  address .
uint8_t readData(uint8_t address, uint8_t *readData) //!Reading
{
  Serial.print("                ");


  dataTX[0] = 0x05;
  lengthCheckSum(dataTX); // Length Checksum
  dataTX[2] = 0xD4; // Code
  dataTX[3] = 0x40; // Code
  dataTX[4] = 0x01; // Number of targets
  dataTX[5] = 0x30; //ReadCode
  dataTX[6] = address;  //Read address
  dataTX[7] = 0x00;
  checkSum(dataTX);
  sendTX(dataTX , 8, 30);
  memset(readData, 0x00, 16);


  if ((dataRX[9]== 0xD5) & (dataRX[10] == 0x41) & (dataRX[11] == 0x00)) {
  for (int i = 12; i < 28; i++) {
  readData[i-12] = dataRX[i];
  }
  return 0;
  } else {
  return 1;
  }
}
//**********************************************************************
//!The PN532 sends back the version of the embedded firmware.
bool getFirmware(void)  //! It is needed to launch a simple command to sycnchronize
{
  Serial.print("                ");


  memset(dataTX, 0x00, 35);
  dataTX[0] = 0x02; // Length
  lengthCheckSum(dataTX); // Length Checksum
  dataTX[2] = 0xD4; // CODE
  dataTX[3] = 0x02; //TFI
  checkSum(dataTX); //0x2A; //Checksum


  sendTX(dataTX , 5 , 17);
  Serial.print("\n");
  Serial.print("Your Firmware version is : ");


  for (int i = 11; i < (15) ; i++){
  Serial.print(dataRX[i], HEX);
  Serial.print(" ");
  }
  Serial.print("\n");
}


//**********************************************************************
//!Print data stored in vectors .
void print(uint8_t * _data, uint8_t length)
{
  for (int i = 0; i < length ; i++){
  Serial.print(_data[i], HEX);
  Serial.print(" ");
  }
  Serial.print("\n");
}
//**********************************************************************
//!This command is used to set internal parameters of the PN532,
bool configureSAM(void)//! Configure the SAM
{
  Serial.print("              ");


  dataTX[0] = 0x05; //Length
  lengthCheckSum(dataTX); // Length Checksum
  dataTX[2] = 0xD4;
  dataTX[3] = 0x14;
  dataTX[4] = 0x01; // Normal mode
  dataTX[5] = 0x14; // TimeOUT
  dataTX[6] = 0x00; // IRQ
  dataTX[7] = 0x00; // Clean checkSum position
  checkSum(dataTX);


  sendTX(dataTX , 8, 13);
}
//**********************************************************************
//!Send data stored in dataTX
void sendTX(uint8_t *dataTX, uint8_t length, uint8_t outLength)
{
  Serial.print(char(0x00));
  Serial.print(char(0x00));
  Serial.print(char(0xFF));


  for (int i = 0; i < length; i++) {
  Serial.print(char(dataTX[i]));
  }


  Serial.print(char(0x00));
  getACK();
  waitResponse();// Receive response
  getData(outLength);
}
//**********************************************************************
//!Wait for ACK response and stores it in the dataRX buffer
void getACK(void)
{
  delay(5);
  waitResponse();
  for (int i = 0; i < 5 ; i++) {
  dataRX[i] = Serial.read();
  }
}
//**********************************************************************
//!Wait the response of the module
void waitResponse(void)
{
  int val = 0xFF;
  int cont = 0x00;
  while(val != 0x00) { //Wait for 0x00 response
  val = Serial.read();
  delay(5);
  cont ++;
  }
}
//**********************************************************************
//!Get data from the module
void getData(uint8_t outLength)
{
  for (int i=5; i < outLength; i++) {
  dataRX[i] = Serial.read();//read data from the module.
  }
}
//**********************************************************************
//!Calculates the checksum and stores it in dataTX buffer
void checkSum(uint8_t *dataTX)
{
  for (int i = 0; i < dataTX[0] ; i++) {
  dataTX[dataTX[0] + 2] += dataTX[i + 2];
  }
  byte(dataTX[dataTX[0] + 2]= - dataTX[dataTX[0] + 2]);
}
//**********************************************************************
//!Calculates the length checksum and sotres it in the buffer.
uint8_t lengthCheckSum(uint8_t *dataTX)
{
  dataTX[1] = byte(0x100 - dataTX[0]);
}

 

Regards

 

Rita

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to ritamüller +1 suggested
    you have one too many "}" in the main loop near the end actually } Serial.println(); } delay(2000); // wait 2 second in each loop } should be } Serial.println(); delay(2000); // wait 2 second in each loop…
Parents
  • dwinhold
    0 dwinhold over 10 years ago

    If I'm not mistaken, between lines 16 and 84 there is 1 too many "}", in the "void setup()".

     

    Dale

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • dwinhold
    0 dwinhold over 10 years ago

    If I'm not mistaken, between lines 16 and 84 there is 1 too many "}", in the "void setup()".

     

    Dale

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer