Arduino Forum Reading with Arduino
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
  • State Verified Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 393 subscribers
  • Views 341 views
  • Users 0 members are here
Related

Reading with Arduino

ritamüller
ritamüller over 10 years ago

Hello,

I have RFID 13.56 MHz / NFC Module for Arduino , I have tried to read 3 cards at the same time and at the serial monitor I have get the UID for the 3 cards .

 

is that reading at the same time or just the module has read one after the other ?


Thx


Rita

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 10 years ago in reply to clem57 +1 verified
    I covered some basics here. http://www.element14.com/community/community/designcenter/explorenfc/blog/2015/02/18/nfc-what-is-it How does it work. Contrary to popular belief the tags do not transmit. The…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    RFID, easpecially the once we get for use with Arduino etc can not read at the same time, it would be one after the other, if you present all three at the same time, you will be lucky if it reads just one of them as there all on the same frequency and encoding

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ritamüller
    0 ritamüller over 10 years ago in reply to Robert Peter Oakes

    So better to say detecting multiple tags at the same time in the same freq. band and reading one after the other ?

    that mean I should have an anti-collision method ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to ritamüller

    Or throw a message to user saying "too many cards, try one at a time"

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago in reply to ritamüller

    Or throw a message to user saying "too many cards, try one at a time"

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 10 years ago in reply to clem57

    I covered some basics here.

    http://www.element14.com/community/community/designcenter/explorenfc/blog/2015/02/18/nfc-what-is-it

     

     

     

    How does it work.

    Contrary to popular belief the tags do not transmit.

     

    The reader sends out a signal at the designed frequency (usually 125 KHz, 134 KHz, 13.5 MHz) and when a tag is within range it captures that energy.

    This provides sufficient energy to power the chip inside which then will short the antenna in a particular manner.

    The shorted antenna will detune the readers antenna, resulting in a difference. (a shorted antenna acts like a large metal object)

    The reader electronics will translate that pattern of 'shorts' and 'non-shorts' into data.

     

    How the reader handles the resultant data depends on the design of the system.

     

    These tags are referred to as 'passive', and for some inventory control an 'active' (powered) tag can be used.


    Because these tags are passive, you won;tbe able to read more than one at a time.

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer