Arduino
  • Products
  • More
Arduino
Arduino Forum RocketScream Reflow Oven Controller Error compiling
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 417 subscribers
  • Views 543 views
  • Users 0 members are here
Related

RocketScream Reflow Oven Controller Error compiling

kf9cm
kf9cm over 12 years ago

Hi Everyone,

 

I have tried several different IDE's in order to get this sketch to compile, Arduino 1.0, 1.0.5r2 and even .023 and I always get the same error message. I have checked all the line numbers in the error message and they seem to be right.

 

Error compiling

 

In file included from PID_v1.cpp:14:
C:\Arduino\libraries\examples/PID_v1.h:1:1: error: unterminated #ifndef

 

I have tried a lot of Forums, but no one seem to know. I have attached the program file and libraries to this post. If anyone could at least run it on there computer and see if they get the same error message I would be most appreciative. The files has been scanned with Avast and are clean.

 

 

Thank You

 

Gary

Attachments:
Reflow_Oven_Controller.ino.zip
PID_v1.h.zip
  • Sign in to reply
  • Cancel
Parents
  • kf9cm
    kf9cm over 12 years ago

    Lim over at RocketScream sent me in the right direction.
    It seems that the problem is in the sketch and library. The library file groups  (.h & .cpp) have to be in separate folders labeled MAX31855 and PID_v1.  Then be put in the IDEs main library folder. 
    The INCLUDES in the sketch need  the < > characters  on the *.h files, NOT the " " characters.

     

     

     

    // DO THIS!

     

    // ***** INCLUDES *****
    #include <LiquidCrystal.h>
    #ifdef    USE_MAX31855
        #include <MAX31855.h>
    #else
        #include <max6675.h>
    #endif
    #include  <PID_v1.h>

     

    // NOT THIS!

     

    // ***** INCLUDES *****
    #include <LiquidCrystal.h>
    #ifdef    USE_MAX31855
        #include  "MAX31855.h"
    #else
        #include  "max6675.h"

    #endif
    #include  <PID_v1.h>

     

    73 de Gary, KF9CM

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to kf9cm

    If it works then great, but I have always had the impression that you can put the library files in any folder as long as you include them in the right way, using the Library folder and sub folders is a nice and convent way of managing the code and keeping them separate for maintenance reasons. But if you want to have a project specific set of files and include they do not have to be separated like that as long as there are no conflicting names in the compiler search paths.

     

    But at the end of the day, if it works, who am I to argue

     

    Happy toasting image ( I mean re-flowing)

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to kf9cm

    If it works then great, but I have always had the impression that you can put the library files in any folder as long as you include them in the right way, using the Library folder and sub folders is a nice and convent way of managing the code and keeping them separate for maintenance reasons. But if you want to have a project specific set of files and include they do not have to be separated like that as long as there are no conflicting names in the compiler search paths.

     

    But at the end of the day, if it works, who am I to argue

     

    Happy toasting image ( I mean re-flowing)

     

    Peter