Arduino
  • Products
  • More
Arduino
Arduino Forum RocketScream Reflow Oven Controller Error compiling
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 417 subscribers
  • Views 542 views
  • Users 0 members are here
Related

RocketScream Reflow Oven Controller Error compiling

kf9cm
kf9cm over 12 years ago

Hi Everyone,

 

I have tried several different IDE's in order to get this sketch to compile, Arduino 1.0, 1.0.5r2 and even .023 and I always get the same error message. I have checked all the line numbers in the error message and they seem to be right.

 

Error compiling

 

In file included from PID_v1.cpp:14:
C:\Arduino\libraries\examples/PID_v1.h:1:1: error: unterminated #ifndef

 

I have tried a lot of Forums, but no one seem to know. I have attached the program file and libraries to this post. If anyone could at least run it on there computer and see if they get the same error message I would be most appreciative. The files has been scanned with Avast and are clean.

 

 

Thank You

 

Gary

Attachments:
Reflow_Oven_Controller.ino.zip
PID_v1.h.zip
  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago

    For that specific problem it looks like simply changing the end of PID_V1.h to this

     

    unsigned long SampleTime;

    double outMin, outMax;

    bool inAuto;

    };  // <-- change here

    #endif

     

    fixes the problem, it then on my computer highlights an issue with the MAX31855 lib but I may have parts missing , I was simply using your supplied code. The change was moving the ";" from after the #endif to the end of the preceding "}"

     

     

    Hope that helps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kf9cm
    kf9cm over 12 years ago in reply to Robert Peter Oakes

    Thanks Peter,

     

    I think I have a lot more wrong than just the sketch and libraries. The errors are taking the sketch away from the program folder.

     

    These are the errors:

     

    Reflow_Oven_Controller.cpp.o: In function `__static_initialization_and_destruction_0':
    C:\Users\GARYGI~1\AppData\Local\Temp\build452520561859438296.tmp/Reflow_Oven_Controller.cpp:253: undefined reference to `MAX31855::MAX31855(unsigned char, unsigned char, unsigned char)'
    Reflow_Oven_Controller.cpp.o: In function `loop':
    C:\Users\GARYGI~1\AppData\Local\Temp\build452520561859438296.tmp/Reflow_Oven_Controller.cpp:321: undefined reference to `MAX31855::readThermocouple(unit_t)'

     

    Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kf9cm
    kf9cm over 12 years ago in reply to Robert Peter Oakes

    Thanks Peter,

     

    I think I have a lot more wrong than just the sketch and libraries. The errors are taking the sketch away from the program folder.

     

    These are the errors:

     

    Reflow_Oven_Controller.cpp.o: In function `__static_initialization_and_destruction_0':
    C:\Users\GARYGI~1\AppData\Local\Temp\build452520561859438296.tmp/Reflow_Oven_Controller.cpp:253: undefined reference to `MAX31855::MAX31855(unsigned char, unsigned char, unsigned char)'
    Reflow_Oven_Controller.cpp.o: In function `loop':
    C:\Users\GARYGI~1\AppData\Local\Temp\build452520561859438296.tmp/Reflow_Oven_Controller.cpp:321: undefined reference to `MAX31855::readThermocouple(unit_t)'

     

    Gary