Arduino
  • Products
  • More
Arduino
Arduino Forum PID Program Code for Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 416 subscribers
  • Views 591 views
  • Users 0 members are here
  • industrial_automation
Related

PID Program Code for Arduino

e14 Contributor
e14 Contributor over 12 years ago

Respected Sir,

                     My self Rinkal padariya , I am stuided in Instrumentation & control Branch in BE

                          our project is "Development Of PID Controller for Temperature Control Using Arduino[ATmega238].

                              I attached some file which is PID Code .Please help me for error correction                                                                                                              

Attachments:
imageHow To Write PID control algorithm using C language _ TipsWell.pdf
PID Arduino.txt.zip
  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago

    A couple of things right away

     

    The code you have attached is measuring light, that's what photores do, it is a light dependent resistor..

     

    What is the source of the PID library (Where did you get it, please provide a link)

     

    what errors are you getting, please provide the errors as an image or written

     

    if you want High and Low temperature and could also want humidity too, as this is common on weather stations, you might want to look at this DHT22 temperature and Humidity Sensor with Arduino Uno and Ethernet Card (ENC or WizNet) (Instant weather Station)

     

    there is also the DS18B20 Arduino Playground - OneWire

     

    and a PID library from here Arduino Playground - PIDLibrary

     

    Armed with these libraries and the sample code you have you should be able to adapt the example to work with temperature.

     

    If you try and cant get too far then please come back , post the code you have and we can try to help more

     

    also in the sample code provided you had many instances where the comments continued on another line causing errors

     

    the attached is with this corrected and it compiles without errors but still working as a light sensor control, not a temperature

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago

    A couple of things right away

     

    The code you have attached is measuring light, that's what photores do, it is a light dependent resistor..

     

    What is the source of the PID library (Where did you get it, please provide a link)

     

    what errors are you getting, please provide the errors as an image or written

     

    if you want High and Low temperature and could also want humidity too, as this is common on weather stations, you might want to look at this DHT22 temperature and Humidity Sensor with Arduino Uno and Ethernet Card (ENC or WizNet) (Instant weather Station)

     

    there is also the DS18B20 Arduino Playground - OneWire

     

    and a PID library from here Arduino Playground - PIDLibrary

     

    Armed with these libraries and the sample code you have you should be able to adapt the example to work with temperature.

     

    If you try and cant get too far then please come back , post the code you have and we can try to help more

     

    also in the sample code provided you had many instances where the comments continued on another line causing errors

     

    the attached is with this corrected and it compiles without errors but still working as a light sensor control, not a temperature

     

    Peter