Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum 25 arduinos in same network
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 415 subscribers
  • Views 1265 views
  • Users 0 members are here
Related

25 arduinos in same network

Wiktor123
Wiktor123 over 4 years ago

Hello

Im in the start of a new project where i nead to connect at least 25 Arduinos in a network. I have first tried I2C but i going to be at the maximum 10 meters betwen them wher I2C have problems over 1 meter. What bus should i use? I prefer to use somthing thas bult in to the Arduinos and not any extra bords. 2 way communication is necessary. It would be nice if i can talk from the master to a slave and slave to slave. But i can be done whid Master to slave and slave to master.

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 4 years ago

    RS-485 is one way to do do this. It will require a $1 driver module at each node. There are many examples of arduino systems using RS-485. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 4 years ago

    RS-485 is one way to do do this. It will require a $1 driver module at each node. There are many examples of arduino systems using RS-485.