Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Turning on a machine automatically when another machine is turned on - using ad hoc ESP8266 network
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 43 replies
  • Subscribers 414 subscribers
  • Views 16638 views
  • Users 0 members are here
  • wifi
  • esp8266
  • relays
  • wireless
Related

Turning on a machine automatically when another machine is turned on - using ad hoc ESP8266 network

donnybahama
donnybahama over 4 years ago

I’m very new to microcontrollers and programming. I probably know just enough to be dangerous. I’m trying to devise a reasonably simple system for turning on the dust collector in my wood shop and positioning the sliding carriage (output side) of a blast gate manifold over the appropriate inlet for the tool that was just turned on. (The first 10 seconds of this video will clarify how the manifold works.)

The way I think I want to do this is using an ad hoc network of ESP8266 modules - 6 “sender” modules which send "Power ON” and [Machine ID] to the “receiver” module (mounted near the dust collector and blast gate manifold) when current is detected for the dust producing machine’s motor. The receiver module then triggers a relay which turns on a motor which turns a threaded rod which moves the manifold’s sliding carriage to position it over the inlet for the tool that was just turned on. Six reed switches - one each attached to the blast gate inlets - are connected to GPIO pins on the receiver module. A magnet mounted to the sliding carriage closes each reed switch as it travels. When the ESP8266 sees that the reed switch for the desired GPIO pin has been closed, it 1) deactivates the relay that’s supplying power (or ground) to the positioner motor, 2) activates a relay that turns on the dust collector, and 3) Turns on a green indicator that can be seen throughout the shop, indicating that the dust collector is on and the proper blast gate is open.

If that’s not the right way to do things, please let me know what the right way is.

Things I need guidance on:

  1. Because I have zero experience with microcontrollers and GPIO pins, I’m not exactly sure what the microcontroller expects to see on a GPIO pin in order to know that some trigger just occurred and some action must be taken. Does it want to see voltage? Ground? A particular frequency?
  2. The “sender modules send “Power ON” ad the machine ID to the receiver module when current is sensed. What’s the simplest/cheapest way to detect the current from a motor turning on and use that to trigger the GPIO pin?
  3. Again, because I have no experience programming a microcontroller, how do I tell the microcontroller to ignore the (momentarily) closed reed switches from the other manifold inlets as the carriage/magnet travels by reed switches 1, 2, and 3 to get to the desired (#4) position?
  4. Anything else I’m overlooking?

Thank you for your time and consideration.

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 4 years ago +5
    Hello donnybahama That is a relatively complex project for someone new to microcontrollers but doable with effort. The best advice I can give is to break it into pieces and prototype each step before…
  • beacon_dave
    beacon_dave over 4 years ago +5
    Perhaps best to start with Question 4... - Safety. Power tools, mains power and "new to microcontrollers and programming" can quickly result in injury. - Your 5th port (free hose) doesn't have a power…
  • dougw
    dougw over 4 years ago +4
    Nice manifold design. It might be better to use a pulley than a lead screw. A leadscrew wouldn't allow the magnets to align the ports.
Parents
  • beacon_dave
    beacon_dave over 4 years ago

    Perhaps best to start with Question 4...

    - Safety. Power tools, mains power and "new to microcontrollers and programming" can quickly result in injury.

    - Your 5th port (free hose) doesn't have a power line to sense in order to activate, so you will need some sort of override switch for that. Even if it is the default position when no tool is being used, then you still need to turn the shop vac on and off. 

    - Handling unplanned conditions - two machines are turned on at the same time. 

    - Manual over-ride - how do you operate the manifold manually when your microcontroller solution stops working and it is driven by a threaded rod.

    - Limit switches - if using a threaded rod then you may want separate hard-wired limit switches to stop the motor if your programming fails to detect the port reached sensor and keeps on going, which usually doesn't end well.

    - Power on states - your system could power up with the manifold position not on any sensor, so your initialisation routine will need to work out where it is so you may want soft limit sensors in case you end up past the outer ports.   

    - Motor controller - you will need a suitable motor controller between the microcontroller and the motor which can drive the threaded rod in either direction.

    - Mechanical switch de-bouncing - mechanical switches tend to bounce which can give unexpected behaviour in your programming.

    Question 3 I don't think is an issue, as if you turn machine 4 on you will likely be checking to see if machine 4 power sense is active AND port 4 sensor reached. Your program will likely be ignoring any activity on port sensors 1-3 as it passes them.

    Any reason that you have chosen the ESP8266 for this ? Sounds like you are perhaps planning on Wi-Fi connectivity ? However if you are already committed to running large vacuum hoses to each machine then a wired solution could be simpler / more reliable for starting out.    

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • donnybahama
    donnybahama over 4 years ago in reply to beacon_dave
    dougw said:
    It might be better to use a pulley than a lead screw

    I definitely want to consider alternate designs but I can’t envision how a pulley can move my carriage. Could you please elaborate?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • donnybahama
    donnybahama over 4 years ago in reply to beacon_dave
    dougw said:
    It might be better to use a pulley than a lead screw

    I definitely want to consider alternate designs but I can’t envision how a pulley can move my carriage. Could you please elaborate?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dougw
    dougw over 4 years ago in reply to donnybahama

    A pulley system would work exactly like the belt drive on most 3D printers that moves the print head across the bed. They use a stepper motor to drive one end of the belt while the other end just runs around an idler gear. It should be much faster than a leadscrew.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • donnybahama
    donnybahama over 4 years ago in reply to dougw

    Got it. Cool! Thanks for the clarification. I’m leaning more and more toward a stepper motor. Seems like it solves a lot of problems. And if I’m going to use a stepper motor, it seems logical to use a belt/pulley system. Seems like it would stand up better to the fine sawdust that will inevitably gum up the works over time, too. Now I just need to figure out a way to enclose the stepper motor, controller, and maybe even the belt (to keep sawdust off it entirely) without the motor or controller overheating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 4 years ago in reply to donnybahama

    Your drill idea could still work - they really have a lot more torque than a stepper motor, which you might need if you want to maintain a good seal. The vacuum side could use a funnel to reduce the need for accurate positioning - as long as you have a plate around the source hoses to seal the whole funnel mouth.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to donnybahama

    Might be worth taking a look at linear actuators:
    https://www.youtube.com/watch?v=zMfmlFcdgJ4

    which being enclosed should help keep most of the sawdust out. Some have built-in limit switches to protect against over-run along with encoders for positional feedback. Also can use a simple pin arrangement at the end of it to disengage it from the manifold carriage for revert to manual operation to keep the workshop running in the early prototyping phases.  

    DIY one using an Arduino for position and velocity control:
    https://youtu.be/WJkf264yxTU?t=176

    Probably can find low cost ones used in satellite dish positioners and gate openers.

    Pneumatic actuators could be another possibility if you already have compressed air available in the workshop.