Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Turning on a machine automatically when another machine is turned on - using ad hoc ESP8266 network
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 43 replies
  • Subscribers 414 subscribers
  • Views 16666 views
  • Users 0 members are here
  • wifi
  • esp8266
  • relays
  • wireless
Related

Turning on a machine automatically when another machine is turned on - using ad hoc ESP8266 network

donnybahama
donnybahama over 4 years ago

I’m very new to microcontrollers and programming. I probably know just enough to be dangerous. I’m trying to devise a reasonably simple system for turning on the dust collector in my wood shop and positioning the sliding carriage (output side) of a blast gate manifold over the appropriate inlet for the tool that was just turned on. (The first 10 seconds of this video will clarify how the manifold works.)

The way I think I want to do this is using an ad hoc network of ESP8266 modules - 6 “sender” modules which send "Power ON” and [Machine ID] to the “receiver” module (mounted near the dust collector and blast gate manifold) when current is detected for the dust producing machine’s motor. The receiver module then triggers a relay which turns on a motor which turns a threaded rod which moves the manifold’s sliding carriage to position it over the inlet for the tool that was just turned on. Six reed switches - one each attached to the blast gate inlets - are connected to GPIO pins on the receiver module. A magnet mounted to the sliding carriage closes each reed switch as it travels. When the ESP8266 sees that the reed switch for the desired GPIO pin has been closed, it 1) deactivates the relay that’s supplying power (or ground) to the positioner motor, 2) activates a relay that turns on the dust collector, and 3) Turns on a green indicator that can be seen throughout the shop, indicating that the dust collector is on and the proper blast gate is open.

If that’s not the right way to do things, please let me know what the right way is.

Things I need guidance on:

  1. Because I have zero experience with microcontrollers and GPIO pins, I’m not exactly sure what the microcontroller expects to see on a GPIO pin in order to know that some trigger just occurred and some action must be taken. Does it want to see voltage? Ground? A particular frequency?
  2. The “sender modules send “Power ON” ad the machine ID to the receiver module when current is sensed. What’s the simplest/cheapest way to detect the current from a motor turning on and use that to trigger the GPIO pin?
  3. Again, because I have no experience programming a microcontroller, how do I tell the microcontroller to ignore the (momentarily) closed reed switches from the other manifold inlets as the carriage/magnet travels by reed switches 1, 2, and 3 to get to the desired (#4) position?
  4. Anything else I’m overlooking?

Thank you for your time and consideration.

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 4 years ago +5
    Hello donnybahama That is a relatively complex project for someone new to microcontrollers but doable with effort. The best advice I can give is to break it into pieces and prototype each step before…
  • beacon_dave
    beacon_dave over 4 years ago +5
    Perhaps best to start with Question 4... - Safety. Power tools, mains power and "new to microcontrollers and programming" can quickly result in injury. - Your 5th port (free hose) doesn't have a power…
  • dougw
    dougw over 4 years ago +4
    Nice manifold design. It might be better to use a pulley than a lead screw. A leadscrew wouldn't allow the magnets to align the ports.
Parents
  • donnybahama
    donnybahama over 4 years ago
    fmilburn said:
    I'd probably look at a non-invasive current transformer sensor first, e.g. this one from Seeed.

    That looks perfect although it says, “used for measuring” which tells me it’s probably going to output a variety of values based on current flow whereas I just want to know if it’s zero or not zero. I guess I’d need to use an analog GPIO pin to handle this device’s non-digital output? Or is there a sensor out there that simply detects current/no current?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 4 years ago in reply to donnybahama

    Yes, it is an analog output.  There may be a sensor out there with digital high/low output but I've not looked.  However, it is easy to put a threshold value in your code and turn the analog output into high/low with an if statement.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to fmilburn

    The Arduino has a Comparator that you can use to trigger on level over/underrun.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to fmilburn

    The Arduino has a Comparator that you can use to trigger on level over/underrun.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • fmilburn
    fmilburn over 4 years ago in reply to Jan Cumps

    True - I don't know if the ESP8266 does though.  He could add an external comparator in any event.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to fmilburn

    It has: arduino.stackexchange.com/.../17967