Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Troubleshooting why Arduino logical operators doesn't compute
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 414 subscribers
  • Views 8864 views
  • Users 0 members are here
Related

Troubleshooting why Arduino logical operators doesn't compute

colporteur
colporteur over 4 years ago

image

How would you write the expression to test sensors Departure (A or B) HIGH AND Arrival (A or B) HIGH?

The first else if statement shown below doesn't work. Departure A OR Departure B HIgh AND Arrival A OR Arrival B High. The OR doesn't work. Only when both Departure A AND B are HIGH the serial print. The same applies to the third else if statement both Departure A and B have to be low for the statement to function. What am I coding wrong for the OR?

      if ((digitalRead(s1DeparturePinA) == LOW || digitalRead(s1DeparturePinB) == LOW) &&
          (digitalRead(s1ArrivalPinA) == HIGH || digitalRead(s1ArrivalPinB) == HIGH))
        {
         Serial.println(F("Train on siding 1 status DEPARTURE")); 
         delay(1);
        }
      else if ((digitalRead(s1DeparturePinA) == HIGH || digitalRead(s1DeparturePinB) == HIGH)&&
               (digitalRead(s1ArrivalPinA) == HIGH || digitalRead(s1ArrivalPinB) == HIGH))
        {
          Serial.println(F("Train on siding 1 status IN TRANSIT"));
          delay(1);
        }
      else if ((digitalRead(s1DeparturePinA) == HIGH || digitalRead(s1DeparturePinB) == HIGH) &&
               (digitalRead(s1ArrivalPinA) == LOW || digitalRead(s1ArrivalPinB) == LOW))
        {
          Serial.println(F("Train on siding 1 status ARRIVAL"));
          delay(1);
          s1ArrivalDetect = LOW;
        }
      else if ((digitalRead(s1DeparturePinA) == LOW || digitalRead(s1DeparturePinB) == LOW) && 
               (digitalRead(s1ArrivalPinA) == LOW || digitalRead(s1ArrivalPinB) == LOW) &&
                s1ArrivalDetect == LOW)
        {
          Serial.println(F("Train on siding 1 status STOP"));
          delay(1);       
        trainOneOut = LOW; //train selection flip_flop L=train on siding 2
        s1ArrivalDetect = HIGH;
        digitalWrite(l1_TurnoutL, LOW);  //unset departure and arrival turnouts for train1
        digitalWrite(s1_Power, LOW);        //unset power on for train1
        digitalWrite(l1_TurnoutR, HIGH);  //set departure and arrival turnouts for train2
        digitalWrite(s2_Power, HIGH);        //set power on for train2
        }

  • Sign in to reply
  • Cancel

Top Replies

  • javagoza
    javagoza over 4 years ago +5
    I would use some kind of linear encoder. If in your case you only have to detect the arrival and departure always in the same direction, the logic is reduced to detecting the rising edge of one sensor…
  • Jan Cumps
    Jan Cumps over 4 years ago +4
    First assign each pin's status to a variable' then print that variable to the serial monitor. You can then see if it's related to your logic, or to a pin not being correctly read. Added bonus: if you…
  • javagoza
    javagoza over 4 years ago in reply to colporteur +3
    For example In setup set the two ISRs // detect rising edge for switch A attachInterrupt(digitalPinToInterrupt(s1ArrivalPinA), isrArrivalSwitchRising, RISING); // detect falling edge for departure…
Parents
  • colporteur
    colporteur over 4 years ago

    Thanks for all the input. I examined the suggestions and then tried to envision a solution. I don't have the programming experience that would give me lots of options to draw solutions from. In the end, I worked my way out by shear testing.

    I followed the suggestion to read the sensor, assigning it to a variable and then evaluating the variable. Oh yeah, I displayed the variables also, that helped. Then I set about using the logical operators to achieve my end goal. I tried to incorporate the ISR concept but couldn't see a way to make it fit. Again that experience thing.

    The code definitely is not as concise as a seasoned programmer would have created but so far it appears to work. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colporteur
    colporteur over 4 years ago

    Thanks for all the input. I examined the suggestions and then tried to envision a solution. I don't have the programming experience that would give me lots of options to draw solutions from. In the end, I worked my way out by shear testing.

    I followed the suggestion to read the sensor, assigning it to a variable and then evaluating the variable. Oh yeah, I displayed the variables also, that helped. Then I set about using the logical operators to achieve my end goal. I tried to incorporate the ISR concept but couldn't see a way to make it fit. Again that experience thing.

    The code definitely is not as concise as a seasoned programmer would have created but so far it appears to work.