Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum SAMD21 and DMA: why do I have to give the end address of the DMA buffer, not the start address?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 414 subscribers
  • Views 1372 views
  • Users 0 members are here
  • mkr
  • samd21
  • arduino
Related

SAMD21 and DMA: why do I have to give the end address of the DMA buffer, not the start address?

Jan Cumps
Jan Cumps over 4 years ago

I'm checking out a few DMA ADC examples for the Arduino MKR with SAMD21 mcu.

Both examples I reviewed (1 and 2) set the destination buffer's end as the destination address:

#define SAMPLE_NO 8  // Define the number of ADC samples

uint16_t adcResult[SAMPLE_NO] = {};  // Store ADC values

// ..
  descriptor.dstaddr = (uint32_t)&adcResult[0] + sizeof(uint16_t) * SAMPLE_NO;  // Place it in the adcResult array

Most controllers I work with expect the start of the buffer. I'm reading the datasheet's DMA section, haven't found the explanation yet.
Anyone here in the know?

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 4 years ago +2
    Answering my own question: When destination address incrementation is configured (BTCTRL.DSTINC is one), SRCADDR must be set to the destination address of the last beat transfer in the block transfer…
  • Jan Cumps
    0 Jan Cumps over 4 years ago

    Answering my own question:

    When destination address incrementation is configured (BTCTRL.DSTINC is one), SRCADDR must be set to the destination address of the last beat transfer in the block transfer.