Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum What do I need for my arduino + current sensor to do data logging ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 415 subscribers
  • Views 1978 views
  • Users 0 members are here
Related

What do I need for my arduino + current sensor to do data logging ?

haoen456123
haoen456123 over 4 years ago

Hi all, 

I am currently working on an Arduino project which requires me to data log the current produced and study the current trend. 

Some requirements are : 

DC current up to 1A

1 - 5 seconds data logging of current data 

Resolution of 0.1mA

Power no limit 

Can anyone let me know which parts I need to form this set up to record the current produced ? 

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 4 years ago +6
    To resolve 0.1 mA and 1 Amp with the same sensor, you need a 16 bit A/D, which is beyond a normal Arduino. There are current sense chips that have a high-resolution built-in A/D converter that can interface…
  • Andrew J
    Andrew J over 4 years ago in reply to dougw +6
    And not just that. You need to check with the datasheet about the error rates because some can be quite high and all will have some impact on readings at 100uA. I think you may need to do some form of…
  • shabaz
    shabaz over 4 years ago +5
    That's non-trivial, and as Andrew mentions, there is the issue of noise that could swamp your lower readings, and you can try to remove some of that through filtering by say averaging, but then the speed…
Parents
  • Jan Cumps
    0 Jan Cumps over 4 years ago

    Is this a high or low voltage application?

    Do the test device (Arduino) and the system you are testing share the same ground?

    Where do you want to log to, and how?

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 4 years ago

    Is this a high or low voltage application?

    Do the test device (Arduino) and the system you are testing share the same ground?

    Where do you want to log to, and how?

    • Cancel
    • Vote Up +4 Vote Down