Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Need help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 414 subscribers
  • Views 5854 views
  • Users 0 members are here
  • help
  • prototyping
  • code
  • arduino
Related

Need help

masa98
masa98 over 4 years ago

hi

im working on a car seat controller and im using 2 arduino nano boards to controll the seat motors. but i ran into a problem with the code. i only get 1V from D2,D4,D5 if i use this code. but if i load another code the pins give 5V and my cirquit only draws 8.5 mA. can some body help.

 //B1-B6 Buttons 
 //D2-D7 output pins
 
int BI = 14;
int B2 = 15;
int B3 = 16;
int B4 = 17;
int B5 = 18;
int B6 = 19;

int D2 = 2;
int D3 = 3;
int D4 = 4;
int D5 = 5;
int D6 = 6;
int D7 = 7;

void setup() {
  
  pinMode(B1, INPUT);
  pinMode(B2, INPUT);
  pinMode(B3, INPUT);
  pinMode(B4, INPUT);
  pinMode(B5, INPUT);
  pinMode(B6, INPUT);

  pinMode(D2, OUTPUT);
  pinMode(D3, OUTPUT);
  pinMode(D4, OUTPUT);
  pinMode(D5, OUTPUT);
  pinMode(D6, OUTPUT);
  pinMode(D7, OUTPUT);
  
}

void loop() {
  
  if (digitalRead(BI) == HIGH && digitalRead(B2) == LOW) {
    
  digitalWrite(D2, HIGH);
  digitalWrite(D3, LOW);
}
  if (digitalRead(B2) == HIGH && digitalRead(BI) == LOW) {
    
  digitalWrite(D3, HIGH);
  digitalWrite(D2, LOW);
}
  else{
  digitalWrite(D2, LOW);
  digitalWrite(D3, LOW);
}

  if (digitalRead(B3) == HIGH && digitalRead(B4) == LOW) {
    
  digitalWrite(D4, HIGH);
  digitalWrite(D5, LOW);
}
  if (digitalRead(B4) == HIGH && digitalRead(B3) == LOW) {
    
  digitalWrite(D5, HIGH);
  digitalWrite(D4, LOW);
}
  else{
  digitalWrite(D4, LOW);
  digitalWrite(D5, LOW);
}

  
  if (digitalRead(B5) == HIGH && digitalRead(B6) == LOW) {
    
  digitalWrite(D6, HIGH);
  digitalWrite(D7, LOW);
}
  if (digitalRead(B6) == HIGH && digitalRead(B5) == LOW) {
    
  digitalWrite(D7, HIGH);
  digitalWrite(D6, LOW);
}
  else{
  digitalWrite(D6, LOW);
  digitalWrite(D7, LOW);
}
}

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 4 years ago +4
    It looks like the second 'if' should be an 'else if'. if else if else instead of if if else Otherwise the pin is being turned on by the first if and then immediately turned off by the else.
  • scottiebabe
    scottiebabe over 4 years ago +4
    'B1' versus 'BI' seems strange, not sure if it's related.
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps +4
    This is what happens: Condition: B1 : 0, B2 : 0 - D2: false ,D3: false ,D2: false ,D3: false , Condition: B1 : 0, B2 : 1 - D2: false ,D3: false ,D3: true ,D2: false , Condition: B1 : 1, B2 : 0 - D2:…
Parents
  • Jan Cumps
    Jan Cumps over 4 years ago

    Here's the loop() with indentation.

    void loop() {
    
    	if (digitalRead(B1) == HIGH && digitalRead(B2) == LOW) {
    		digitalWrite(D2, HIGH);
    		digitalWrite(D3, LOW);
    	}
    	else {
    		digitalWrite(D2, LOW);
    		digitalWrite(D3, LOW);
    		
    		if (digitalRead(B2) == HIGH && digitalRead(B1) == LOW) {
    			digitalWrite(D3, HIGH);
    			digitalWrite(D2, LOW);
    		}
    		else {
    			digitalWrite(D2, LOW);
    			digitalWrite(D3, LOW);
    		}
    	}
    }

    I'll try and write a testbed, and see what happens in the four scenarios:

    B1 B2
    0 0
    0 1
    1 0
    1 1
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    This is what happens:

    Condition: B1 : 0, B2 : 0 - D2: false ,D3: false ,D2: false ,D3: false ,
    Condition: B1 : 0, B2 : 1 - D2: false ,D3: false ,D3: true ,D2: false ,
    Condition: B1 : 1, B2 : 0 - D2: true ,D3: false ,
    Condition: B1 : 1, B2 : 1 - D2: false ,D3: false ,D2: false ,D3: false ,

    see how many times the same digitalWrite() is called, in  test 1, 2 and 4? 

    Test code. The testLoop() is the same logic as your loop():

    #include <iostream>
    #include <string>
    
    #define HIGH (true)
    #define LOW (false)
    #define D2 ("D2")
    #define D3 ("D3")
    
    bool digitalRead(bool value) {
    	return value;
    }
    
    void digitalWrite(std::string pin, bool value) {
    	std::cout << pin;
    	if (value) {
    		std::cout << ": true  ,";
    	} else {
    		std::cout << ": false ,";
    	}
    }
    
    void testLoop(bool B1, bool B2) {
    	std::cout << "Condition: B1 : ";
    	std::cout << B1;
    	std::cout << ", B2 : ";
    	std::cout << B2;
    	std::cout << " - ";
    
    
    	if (digitalRead(B1) == HIGH && digitalRead(B2) == LOW) {
    
    		digitalWrite(D2, HIGH);
    		digitalWrite(D3, LOW);
    	}
    	else{
    		digitalWrite(D2, LOW);
    		digitalWrite(D3, LOW);
    
    
    		if (digitalRead(B2) == HIGH && digitalRead(B1) == LOW) {
    
    			digitalWrite(D3, HIGH);
    			digitalWrite(D2, LOW);
    		}
    		else{
    			digitalWrite(D2, LOW);
    			digitalWrite(D3, LOW);
    		}
    	}
    	std::cout << std::endl;
    }
    
    int main() {
    	testLoop(false, false);
    	testLoop(false, true);
    	testLoop(true, false);
    	testLoop(true, true);
    	return 0;
    }
    

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    Now using beacon_dave's logic:

    result:

    Condition: B1 : 0, B2 : 0 - D2: false ,D3: false ,
    Condition: B1 : 0, B2 : 1 - D3: true ,D2: false ,
    Condition: B1 : 1, B2 : 0 - D2: true ,D3: false ,
    Condition: B1 : 1, B2 : 1 - D2: false ,D3: false ,

    Test code: The testLoop() is the same logic as Dave's loop():

    void testLoop(bool B1, bool B2) {
    	std::cout << "Condition: B1 : ";
    	std::cout << B1;
    	std::cout << ", B2 : ";
    	std::cout << B2;
    	std::cout << " - ";
    
    
    	if (digitalRead(B1) == HIGH && digitalRead(B2) == LOW)
    	{
    		digitalWrite(D2, HIGH);
    		digitalWrite(D3, LOW);
    	}
    	else if (digitalRead(B2) == HIGH && digitalRead(B1) == LOW)
    	{
    		digitalWrite(D3, HIGH);
    		digitalWrite(D2, LOW);
    	}
    	else
    	{
    		digitalWrite(D2, LOW);
    		digitalWrite(D3, LOW);
    	}
    
    	std::cout << std::endl;
    }

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • masa98
    masa98 over 4 years ago in reply to Jan Cumps

    that seamed to fix it. thanks for the help

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to masa98

    You will still have to work on debouncing the buttons. The loop is run many many times per second, and a mechanical switch doesn't nicely open or close at once. It bounces up many times very fast, before permanently open or close the contact.

    But the processor may be faster than those fast bounces, and your code would behave unstable because of that.

    One possible easy option is to:

    first digitalRead() all inputs at the begin of the loop in local variables. So that you don't poll the same pin several times in the same loop.
    In your if statements, you then use the variables, where you now use the repeated digitalRead() calls

    And put a delay(x) at the end of the loop, after all  the if statements.
    Experiment with the x value, so that you don't get bounce issues, and that the project is still reacting.

    delay(20)  would be a reasonable start point for experimenting.

    #define BUTTON_1 (14)
    #define BUTTON_2 (15)
    
    #define DEBOUNCE_DELAY (20)
    
    loop() {
      // poll input state at start of the loop
      bool btn1 = digitalRead(BUTTON_1);
      bool btn2 = digitalRead(BUTTON_2);
    
      // execute logic based on the gathered state
      if ((btn1 == HIGH) && (btn2 == LOW)) {
        // ...
      }
    
      // debounce delay (not the best debounce method, but may work)
      delay(DEBOUNCE_DELAY);
    }

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • masa98
    masa98 over 4 years ago in reply to Jan Cumps

    thanks the delay made my motors to start better

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 4 years ago in reply to masa98

    For debugging you could add big delays (like 5 seconds) at the bottom of each if/else block, so that after a button press it stays with the outputs you set, so then you have time to test them. Combined with the Serial.println, that should give you a fair bit of extra insight into what is happening.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ntewinkel
    ntewinkel over 4 years ago in reply to masa98

    For debugging you could add big delays (like 5 seconds) at the bottom of each if/else block, so that after a button press it stays with the outputs you set, so then you have time to test them. Combined with the Serial.println, that should give you a fair bit of extra insight into what is happening.