Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Need help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 414 subscribers
  • Views 5846 views
  • Users 0 members are here
  • help
  • prototyping
  • code
  • arduino
Related

Need help

masa98
masa98 over 4 years ago

hi

im working on a car seat controller and im using 2 arduino nano boards to controll the seat motors. but i ran into a problem with the code. i only get 1V from D2,D4,D5 if i use this code. but if i load another code the pins give 5V and my cirquit only draws 8.5 mA. can some body help.

 //B1-B6 Buttons 
 //D2-D7 output pins
 
int BI = 14;
int B2 = 15;
int B3 = 16;
int B4 = 17;
int B5 = 18;
int B6 = 19;

int D2 = 2;
int D3 = 3;
int D4 = 4;
int D5 = 5;
int D6 = 6;
int D7 = 7;

void setup() {
  
  pinMode(B1, INPUT);
  pinMode(B2, INPUT);
  pinMode(B3, INPUT);
  pinMode(B4, INPUT);
  pinMode(B5, INPUT);
  pinMode(B6, INPUT);

  pinMode(D2, OUTPUT);
  pinMode(D3, OUTPUT);
  pinMode(D4, OUTPUT);
  pinMode(D5, OUTPUT);
  pinMode(D6, OUTPUT);
  pinMode(D7, OUTPUT);
  
}

void loop() {
  
  if (digitalRead(BI) == HIGH && digitalRead(B2) == LOW) {
    
  digitalWrite(D2, HIGH);
  digitalWrite(D3, LOW);
}
  if (digitalRead(B2) == HIGH && digitalRead(BI) == LOW) {
    
  digitalWrite(D3, HIGH);
  digitalWrite(D2, LOW);
}
  else{
  digitalWrite(D2, LOW);
  digitalWrite(D3, LOW);
}

  if (digitalRead(B3) == HIGH && digitalRead(B4) == LOW) {
    
  digitalWrite(D4, HIGH);
  digitalWrite(D5, LOW);
}
  if (digitalRead(B4) == HIGH && digitalRead(B3) == LOW) {
    
  digitalWrite(D5, HIGH);
  digitalWrite(D4, LOW);
}
  else{
  digitalWrite(D4, LOW);
  digitalWrite(D5, LOW);
}

  
  if (digitalRead(B5) == HIGH && digitalRead(B6) == LOW) {
    
  digitalWrite(D6, HIGH);
  digitalWrite(D7, LOW);
}
  if (digitalRead(B6) == HIGH && digitalRead(B5) == LOW) {
    
  digitalWrite(D7, HIGH);
  digitalWrite(D6, LOW);
}
  else{
  digitalWrite(D6, LOW);
  digitalWrite(D7, LOW);
}
}

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 4 years ago +4
    It looks like the second 'if' should be an 'else if'. if else if else instead of if if else Otherwise the pin is being turned on by the first if and then immediately turned off by the else.
  • scottiebabe
    scottiebabe over 4 years ago +4
    'B1' versus 'BI' seems strange, not sure if it's related.
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps +4
    This is what happens: Condition: B1 : 0, B2 : 0 - D2: false ,D3: false ,D2: false ,D3: false , Condition: B1 : 0, B2 : 1 - D2: false ,D3: false ,D3: true ,D2: false , Condition: B1 : 1, B2 : 0 - D2:…
Parents
  • scottiebabe
    scottiebabe over 4 years ago

    'B1' versus 'BI' seems strange, not sure if it's related.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • masa98
    masa98 over 4 years ago in reply to scottiebabe

    i got somekind of error when i had it as B1 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 4 years ago in reply to masa98

    I'm not an Arduino expert but it appears to that Bx is defined as the binary equivalent   forum.arduino.cc/.../480156 interesting 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 4 years ago in reply to scottiebabe

    So make sure you stick to the BI variable as B1 would just be a constant 1

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to scottiebabe

    Yes. I wasn't aware of this (more info on where B1 is defined here).

    masa98, it would be good to not use B1 -> BX, but something that's not yet used by Arduino's API:

    #define BUTTON_1 14
    #define BUTTON_2 15
    // ...
    
    loop() {
      // poll all states at start of loop
      bool btn1 = digitalRead(BUTTON_1);
      bool btn2 = digitalRead(BUTTON_2);
    
      // execute logic based on state gathered above
      if ((btn1 == HIGH) && (btn2 == LOW)) {

    and if the buttons mean something (like left seat up, left seat down, right seat up, ...) :

    #define BUTTON_LEFT_UP    14
    #define BUTTON_LEFT_DOWN  15
    #define BUTTON_RIGHT_UP   16
    #define BUTTON_RIGHT_DOWN 17
    // ...
    

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 4 years ago in reply to Jan Cumps

    Even more interesting is technically binary literals are not defined in C https://www.iar.com/knowledge/support/technical-notes/compiler/any-binary-notation-in-c-source/

    But I use 0b01 etc all the time, so I guess most compilers support it anyways.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • scottiebabe
    scottiebabe over 4 years ago in reply to Jan Cumps

    Even more interesting is technically binary literals are not defined in C https://www.iar.com/knowledge/support/technical-notes/compiler/any-binary-notation-in-c-source/

    But I use 0b01 etc all the time, so I guess most compilers support it anyways.

    • Cancel
    • Vote Up +3 Vote Down