Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum need help with arduino code
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 414 subscribers
  • Views 1047 views
  • Users 0 members are here
Related

need help with arduino code

masa98
masa98 over 4 years ago

hi

im working on a car seat controller and im using 2 arduino nano boards to controll the seat motors. but i ran into a problem with the code. i only get 1V from D2,D4,D5 if i use this code. but if i load another code the pins give 5V and my cirquit only draws 8.5 mA. can some body help.

 //B1-B6 Buttons 
 //D2-D7 output pins
 
int BI = 14;
int B2 = 15;
int B3 = 16;
int B4 = 17;
int B5 = 18;
int B6 = 19;

int D2 = 2;
int D3 = 3;
int D4 = 4;
int D5 = 5;
int D6 = 6;
int D7 = 7;

void setup() {
  
  pinMode(B1, INPUT);
  pinMode(B2, INPUT);
  pinMode(B3, INPUT);
  pinMode(B4, INPUT);
  pinMode(B5, INPUT);
  pinMode(B6, INPUT);

  pinMode(D2, OUTPUT);
  pinMode(D3, OUTPUT);
  pinMode(D4, OUTPUT);
  pinMode(D5, OUTPUT);
  pinMode(D6, OUTPUT);
  pinMode(D7, OUTPUT);
  
}

void loop() {
  
  if (digitalRead(BI) == HIGH && digitalRead(B2) == LOW) {
    
  digitalWrite(D2, HIGH);
  digitalWrite(D3, LOW);
}
  if (digitalRead(B2) == HIGH && digitalRead(BI) == LOW) {
    
  digitalWrite(D3, HIGH);
  digitalWrite(D2, LOW);
}
  else{
  digitalWrite(D2, LOW);
  digitalWrite(D3, LOW);
}

  if (digitalRead(B3) == HIGH && digitalRead(B4) == LOW) {
    
  digitalWrite(D4, HIGH);
  digitalWrite(D5, LOW);
}
  if (digitalRead(B4) == HIGH && digitalRead(B3) == LOW) {
    
  digitalWrite(D5, HIGH);
  digitalWrite(D4, LOW);
}
  else{
  digitalWrite(D4, LOW);
  digitalWrite(D5, LOW);
}

  
  if (digitalRead(B5) == HIGH && digitalRead(B6) == LOW) {
    
  digitalWrite(D6, HIGH);
  digitalWrite(D7, LOW);
}
  if (digitalRead(B6) == HIGH && digitalRead(B5) == LOW) {
    
  digitalWrite(D7, HIGH);
  digitalWrite(D6, LOW);
}
  else{
  digitalWrite(D6, LOW);
  digitalWrite(D7, LOW);
}
}
  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 4 years ago +2
    What is connected to D2, D4, D5. Posting a complete schematic would help diagnose the issue.
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to ntewinkel +2
    There's a duplicate post, with more action: community.element14.com/.../
  • ntewinkel
    ntewinkel over 4 years ago in reply to Jan Cumps +1
    Thanks Jan Cumps ! I noticed that just after I posted it! I also noticed you were able to clear up the bugs there There's a bug in this forum, that doesn't allow me to reply using my iPhone, so I'm late…
Parents
  • ntewinkel
    0 ntewinkel over 4 years ago

    Line 4 declared BI (letter I), but line 20 uses B1 (digit 1)

    For debugging, I suggest using Serial.println within all of the "if" and "else" blocks, to see what is going on. Remember to set up Serial with a call to Serial.begin(...) (lots of examples available for that).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to ntewinkel

    There's a duplicate post, with more action: community.element14.com/.../

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 4 years ago in reply to Jan Cumps

    Thanks Jan Cumps! I noticed that just after I posted it!  I also noticed you were able to clear up the bugs there Slight smile

    There's a bug in this forum, that doesn't allow me to reply using my iPhone, so I'm late to the party again Laughing

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 4 years ago in reply to Jan Cumps

    Thanks Jan Cumps! I noticed that just after I posted it!  I also noticed you were able to clear up the bugs there Slight smile

    There's a bug in this forum, that doesn't allow me to reply using my iPhone, so I'm late to the party again Laughing