Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Rotating the Servo Using PID controller and SONAR
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 414 subscribers
  • Views 1941 views
  • Users 0 members are here
  • arduino-robot
  • help
  • servo_motor_control
Related

Rotating the Servo Using PID controller and SONAR

nafis
nafis over 4 years ago

I have to make a bot which has front wheel steering by one servo motor like real cars..and one driving motor to run the robot..by rotating the servo the bot will turn right and left..there is Two SONAR on the left and right side to detect the distance from left and right wall. By taking the distance from both sides of the wall the robot has to be moved continuously forward at the middle position by steering the front wheel with help of the Servo.
How can I rotate the servo with PID for smooth turning? At 118degree the servo is straight and the robot is entirely forward. that means at 118degree of servo the robot will be completely straight.
How can I code the PID algorithm to rotate the servo by taking the distimageance from two SONAR?image

  • Sign in to reply
  • Cancel

Top Replies

  • WumblingBorkeys
    WumblingBorkeys over 4 years ago +1
    I'd start by tackling the PID loop, once you understand the PID loop you can work to implement it. There are some great PID tuning and creation videos on youtube! What I did in a similar project was…
  • michaelkellett
    michaelkellett over 4 years ago +1
    What makes you think that PID is the best way to control the servo in this applicaton ? PID control doesn't care about offset (that's what the I term is for). Any real PID control system needs to be…
  • robogary
    robogary over 4 years ago in reply to nafis +1
    The Arduino IDE has example code for servos and the ping sensors, also a PID library.
Parents
  • WumblingBorkeys
    WumblingBorkeys over 4 years ago

    I'd start by tackling the PID loop, once you understand the PID loop you can work to implement it.

    There are some great PID tuning and creation videos on youtube!

    What I did in a similar project was 3 if/while commands, one for when the left side is closer,

    one for roughly center +- sensor error, and another for the right side closer.

    Then based on those statements get your difference and use that as your Porpotinal part of your PID loop. You might want to use the Map(int, int, int, int) command to change the distance from the wall to an appropriate steering angle.

    I don't have my code anymore unfortunately otherwise I'd send it over to you! I hope this helped a little bit.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • nafis
    nafis over 4 years ago in reply to WumblingBorkeys

    thanks for your reply...can you please give the code?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • nafis
    nafis over 4 years ago in reply to WumblingBorkeys

    thanks for your reply...can you please give the code?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • robogary
    robogary over 4 years ago in reply to nafis

    The Arduino IDE has example code for servos and the ping sensors, also a PID library.