Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum L293d motor driver
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 414 subscribers
  • Views 3377 views
  • Users 0 members are here
Related

L293d motor driver

Kaushik_ma
Kaushik_ma over 4 years ago

So guys I had setup of rc car .I am using 4 motors , l293d driver ,ardunio Uno board and an hc -06 Bluetooth module for connection. The problem is after setting all if I supply current through batteries the l293d driver and ardunio is working but Bluetooth module is not working , instead I am giving the supply from power Bank the Bluetooth module and ardunio are running but l293d driver is not working..please tell me an solution

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 4 years ago +2 verified
    Can you show a photo or drawing of how power is connected?
  • ralphjy
    ralphjy over 4 years ago +2
    Have you tried removing the shield power jumper and powering the Arduino and the motors separately? You mentioned using a Power Bank. If this is a USB Power Bank, it will not power the motors (except…
  • shabaz
    shabaz over 4 years ago +2
    You're brave, constructing a battery pack from three LiPo cells that are unprotected according to the peeled one, into a cheap spring holder with thin wires. If there's a stall on the motors then expect…
Parents
  • ralphjy
    0 ralphjy over 4 years ago

    Have you tried removing the shield power jumper and powering the Arduino and the motors separately?

    image

    You mentioned using a Power Bank.  If this is a USB Power Bank, it will not power the motors (except for servo motors).  So it would make sense that your motors did not work.

    Without a connection schematic it is difficult to determine why the HC-06 isn't working when the battery is the power source.  It would be good to try a separate power source for the Arduino and the the motors, but make sure you remove the power jumper first!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ralphjy
    0 ralphjy over 4 years ago

    Have you tried removing the shield power jumper and powering the Arduino and the motors separately?

    image

    You mentioned using a Power Bank.  If this is a USB Power Bank, it will not power the motors (except for servo motors).  So it would make sense that your motors did not work.

    Without a connection schematic it is difficult to determine why the HC-06 isn't working when the battery is the power source.  It would be good to try a separate power source for the Arduino and the the motors, but make sure you remove the power jumper first!