Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum When is the function delay() a delay?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 413 subscribers
  • Views 10529 views
  • Users 0 members are here
  • delay
  • arduino_code
Related

When is the function delay() a delay?

colporteur
colporteur over 3 years ago

else if (MainDepartureState == LOW && MainArrivalState == LOW) {
        if (startupMain == HIGH) {
          // pulse turnout for Main train
          digitalWrite(Main_Turnout, HIGH);
          relayDelay();//<-----1
          digitalWrite(Main_Turnout, LOW);
          if (deBug == HIGH) {
            Serial.println("The Main Turnout Activated");
          }
          // Engage Motor for Main
          motors.setSpeedB(minSpeedB);  // Start Motor for Main
          motors.forwardB();
          PowerMain = LOW;
          startupMain = LOW;
          delay(300000);//<----2
          if (deBug == HIGH) {
            Serial.println("Motor Delay Complete");
          }

According to what I have read “The delay() function allows you to pause the execution of your Arduino code for a specified period.”

Why are the delays I am using not working or the values are so extreme? How can I best accomplish a delay?

I tried using the delay() function at point <----1 in my code and it failed miserably. I wanted to activate a relay by turning it on, waiting for relay to engage (delay(2000), then turn it off. The delay(2000) two seconds didn’t work. I wrote a little relay routine that accomplish what I wanted but why did delay(2000) not give me two seconds?

I am using delay() function at <----2 in the code but the value doesn’t reflect the actual delay. I needed to generate some wait time for the motor to engage and trigger a sensor. My desire was a three second delay(3000) but the delay(300000) was a value that actually worked. That would be 300 seconds yes/no?

I'm a code resurrectionist and not an actual programmer. I will try and muddle through discussions 

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 3 years ago +6
    Based on GL shared insight, I used a different set of PWM pins so as not to muck with the delay() timer. I also took the BE suggestions and used subtraction in the millis routines. I am happy to report…
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur +5
    //user input variables int turnout_delay = 10000; //delay for relay contacts to engage int motor_delay = 900000; //delay for motor to move train unsigned long time_now = 0; int type cannot store outside…
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur +3
    I think that it helps if one can see names like "TCCR0B" and know inside that it is short for "Timer Control Counter Register" then that should immediately set-off alarm bells in one's head. Gough Lui…
Parents
  • ntewinkel
    ntewinkel over 3 years ago

    I would start by putting a serial.println before and after the delay just to make sure there’s no question of it being the right delay line you’re looking at.

     Also make sure you have selected the correct board for your sketch. There’s a good chance delay() just counts clock cycles, so a faster chip might whip through them faster than a standard old Uno might.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to ntewinkel

    This. Maybe use a digital output. Flip polarity before the delay. Flip polarity after delay. Use an oscilloscope to measure the time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to ntewinkel

    This. Maybe use a digital output. Flip polarity before the delay. Flip polarity after delay. Use an oscilloscope to measure the time.