Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum When is the function delay() a delay?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 413 subscribers
  • Views 10571 views
  • Users 0 members are here
  • delay
  • arduino_code
Related

When is the function delay() a delay?

colporteur
colporteur over 3 years ago

else if (MainDepartureState == LOW && MainArrivalState == LOW) {
        if (startupMain == HIGH) {
          // pulse turnout for Main train
          digitalWrite(Main_Turnout, HIGH);
          relayDelay();//<-----1
          digitalWrite(Main_Turnout, LOW);
          if (deBug == HIGH) {
            Serial.println("The Main Turnout Activated");
          }
          // Engage Motor for Main
          motors.setSpeedB(minSpeedB);  // Start Motor for Main
          motors.forwardB();
          PowerMain = LOW;
          startupMain = LOW;
          delay(300000);//<----2
          if (deBug == HIGH) {
            Serial.println("Motor Delay Complete");
          }

According to what I have read “The delay() function allows you to pause the execution of your Arduino code for a specified period.”

Why are the delays I am using not working or the values are so extreme? How can I best accomplish a delay?

I tried using the delay() function at point <----1 in my code and it failed miserably. I wanted to activate a relay by turning it on, waiting for relay to engage (delay(2000), then turn it off. The delay(2000) two seconds didn’t work. I wrote a little relay routine that accomplish what I wanted but why did delay(2000) not give me two seconds?

I am using delay() function at <----2 in the code but the value doesn’t reflect the actual delay. I needed to generate some wait time for the motor to engage and trigger a sensor. My desire was a three second delay(3000) but the delay(300000) was a value that actually worked. That would be 300 seconds yes/no?

I'm a code resurrectionist and not an actual programmer. I will try and muddle through discussions 

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 3 years ago +6
    Based on GL shared insight, I used a different set of PWM pins so as not to muck with the delay() timer. I also took the BE suggestions and used subtraction in the millis routines. I am happy to report…
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur +5
    //user input variables int turnout_delay = 10000; //delay for relay contacts to engage int motor_delay = 900000; //delay for motor to move train unsigned long time_now = 0; int type cannot store outside…
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur +3
    I think that it helps if one can see names like "TCCR0B" and know inside that it is short for "Timer Control Counter Register" then that should immediately set-off alarm bells in one's head. Gough Lui…
Parents
  • robogary
    robogary over 3 years ago

    Im a sw fumbler myself, Ill throw out a couple suggestions. variable relayDelay() wont be recognized as a Arduino delay command. The other delay(300000) should be too big a value, even tho it works. The delay value is an integer, 32767 max (or maybe 65535 if unsigned). There are some online articles that talk about some Arduino commands that interfere with the delay timer time accumulator in background. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to robogary

    I didn't explain myself well

    relayDelay() is  void function i created

    void relayDelay() {
      time_now = millis();
      while (millis() < time_now + turnout_delay) {
        //wait approx. [period] ms
      }
    }

    that I could use to test what amount of delay I would need in order to activate a relay so the contacts make. Currently turnout_delay = 10000 and I get about 1 second the relay is engaged. Now this throws a wrench in my understanding of delay() but the time duration works.

    Any reference links on Arduino commands that impact delay timer?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur

    What is the type of time_now variable? What is the type of turnout_delay? Are you sure you have enough free RAM?

    If you're not using unsigned long, then you are probably running into overflow issues as millis() reports unsigned long and if working as other data type, will not handle roll-over correctly.

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur

    What is the type of time_now variable? What is the type of turnout_delay? Are you sure you have enough free RAM?

    If you're not using unsigned long, then you are probably running into overflow issues as millis() reports unsigned long and if working as other data type, will not handle roll-over correctly.

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • colporteur
    colporteur over 3 years ago in reply to Gough Lui

    The code starts with 

    unsigned long time_now = 0;

    I assumed it stays unsigned long.

    My goal was a 3 second delay. Setting turnout_delay=10000, I get about 1 sec of delay. I tried replacing my function with just delay(3000) at it failed to engage the relay.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to colporteur

    There is something else wrong then.

    Can we please see your full code?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 3 years ago in reply to baldengineer

    I think the same, without seeing all the source code is a waste of time.
    A simple interrupt service routine may be the cause, or so simple that it is timing the data sent by the UART. From what I understand, he is debugging with the serial output through the UART. I advise against this method, it is very invasive and introduces new delays. It is much easier and more efficient to use a digital output to turn a LED on and off. On that digital output you can use a logic analyzer or an oscilloscope to measure times.