Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum When is the function delay() a delay?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 413 subscribers
  • Views 10571 views
  • Users 0 members are here
  • delay
  • arduino_code
Related

When is the function delay() a delay?

colporteur
colporteur over 3 years ago

else if (MainDepartureState == LOW && MainArrivalState == LOW) {
        if (startupMain == HIGH) {
          // pulse turnout for Main train
          digitalWrite(Main_Turnout, HIGH);
          relayDelay();//<-----1
          digitalWrite(Main_Turnout, LOW);
          if (deBug == HIGH) {
            Serial.println("The Main Turnout Activated");
          }
          // Engage Motor for Main
          motors.setSpeedB(minSpeedB);  // Start Motor for Main
          motors.forwardB();
          PowerMain = LOW;
          startupMain = LOW;
          delay(300000);//<----2
          if (deBug == HIGH) {
            Serial.println("Motor Delay Complete");
          }

According to what I have read “The delay() function allows you to pause the execution of your Arduino code for a specified period.”

Why are the delays I am using not working or the values are so extreme? How can I best accomplish a delay?

I tried using the delay() function at point <----1 in my code and it failed miserably. I wanted to activate a relay by turning it on, waiting for relay to engage (delay(2000), then turn it off. The delay(2000) two seconds didn’t work. I wrote a little relay routine that accomplish what I wanted but why did delay(2000) not give me two seconds?

I am using delay() function at <----2 in the code but the value doesn’t reflect the actual delay. I needed to generate some wait time for the motor to engage and trigger a sensor. My desire was a three second delay(3000) but the delay(300000) was a value that actually worked. That would be 300 seconds yes/no?

I'm a code resurrectionist and not an actual programmer. I will try and muddle through discussions 

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 3 years ago +6
    Based on GL shared insight, I used a different set of PWM pins so as not to muck with the delay() timer. I also took the BE suggestions and used subtraction in the millis routines. I am happy to report…
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur +5
    //user input variables int turnout_delay = 10000; //delay for relay contacts to engage int motor_delay = 900000; //delay for motor to move train unsigned long time_now = 0; int type cannot store outside…
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur +3
    I think that it helps if one can see names like "TCCR0B" and know inside that it is short for "Timer Control Counter Register" then that should immediately set-off alarm bells in one's head. Gough Lui…
Parents
  • robogary
    robogary over 3 years ago

    Im a sw fumbler myself, Ill throw out a couple suggestions. variable relayDelay() wont be recognized as a Arduino delay command. The other delay(300000) should be too big a value, even tho it works. The delay value is an integer, 32767 max (or maybe 65535 if unsigned). There are some online articles that talk about some Arduino commands that interfere with the delay timer time accumulator in background. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to robogary

    The standard Arduino library defines the millisecond value as a (32-bit) unsigned long. So you can use values considerably larger than 32767/65535.

    The issue people tend to run into is when they multiply two integers. For example, delay(3000 * 1000); Since both values fit inside of a 16-bit data value, the complier treats the operation entirely as 16-bit even though the result overflows. All of that happens despite the (correctly) result fitting inside of a 32-bit value which would work if explicitly written. (or if the math is casted.)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to baldengineer

    Thanks for clarifying my bad info on the integer value. Good point on the multiplier.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • robogary
    robogary over 3 years ago in reply to baldengineer

    Thanks for clarifying my bad info on the integer value. Good point on the multiplier.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ntewinkel
    ntewinkel over 3 years ago in reply to robogary

    I’ve been caught on that number sizing thing so many times, usually due to defining small constants that automatically get tucked into small types. That’s one thing newer languages do more nicely. C is happy to just let you suffer Laughing